MISUMI Aluminum Extrusion Search Tool (BETA)

This page will help you see the different aluminum extrusion options that MISUMI has and also help you select the extrusions, brackets, and hardware you might need.

To use this page, simply apply a filter on the left by making a selection in one of the comboboxes. The results shown will correspond to all filters you select (in other words, you can apply as many filters as you need and the results shown will have all of the selected filters applied). To remove a filter, simply click on the "X" for that filter.

If you have any questions, or run into any issues, please contact us at engineering@misumiusa.com.

To continue, click: , or apply a filter.

Extrusion Series

Extrusion Series is the main way that MISUMI extrusions are grouped. The Series refers to the extrusion's groove shape. When selecting extrusions, brackets, and hardware, be sure to select parts from the same series. For example, while a Series 8 extrusion and a Series 8-45 extrusion both have a 10mm slot width, the groove is shaped differently. Because of this, for example, a Series 8 t-nut will NOT work in a Series 8-45 extrusion, and vice versa.

You may notice that the Series number seems closly related to the Slot Width. The reason for this is that the Series number represents the largest diameter of the mounting bolt used for the extrusion's mounting brackets. For example, a Series 5 extrusion will use a M5 bolt when mounting a bracket.

Extrusion Base Size

Base size is the minimum size that the particular extrusion is derrived from. For example, the part illustrated above is an HFS6-606030. The overall width and height of this extrusion is 60mm. But, the base size of this extrusion is 30mm as this extrusion is "made up" of three 30mm by 30mm extrusions. This also means that the distance between the two slots on a side will be 30mm.

Slot Width

The Slot Width is the width of the slot of the groove on an extrusion. Please note that extrusions with the same slot width may not have the same groove shape (Series). For example, while a Series 8 extrusion and a Series 8-45 extrusion both have a 10mm Slot Width, they do NOT have the same groove shape.

Extrusion Width

The overall width of the part.

Extrusion Height

The overall height of the part

Material

The material of the part.

Surface Finish

You can search for extrusions and brackets based on surface treatement

Most extrusion and hardware are offered with clear anodized coating

Some can also be obtained with black anodizing, clear acrilic coat over clear anodized finish or yellow powder coating

This last option is a new MISUMI offering and we do not have cad data for these parts available

All you need to do is to remove the "Y" from the part number and you can download clear anodized version

you can use the model since all dimensions are the same, but remember to add "Y" back when ordering

Extrusions, brackets and nuts

The following slot series are available:

3 (3.4mm slot width designed for 15mm base extrusion)

5 (6mm slot width)

6 (8 mm slot width)

8 (10mm slot width designed for 40mm base extrusion)

8-45 (10mm slot width designed for 45, 50 and 60mm base extrusion)

Special (In some cases extrusions have two slot styles or an unusual design)

Please, remember to pay special attention to extrusions and brackets with 8 and 8-45 series

8-45 series brackets will only work with 8-45 series extrusions

Most 8 series brackets will also work with only 8 series extrusions with some exceptions