Empowering Engineers with

Configurable Components

News

MISUMI'S 3D CAD CD-ROM OFFERS THOUSANDS OF NATIVE CAD MODELS

MISUMI Factory Automation Components

December 9, 2009

MISUMI'S 3D CAD CD-ROM OFFERS THOUSANDS OF
NATIVE CAD MODELS FOR FAST, CONVENIENT DOWNLOAD

Now available free upon request, popular CD-ROM saves time, simplifies design engineering,
and eliminates the need to create in-house drawings.

 

Misumi USA, Inc., a subsidiary of Misumi Corporation, part of Misumi Group, Inc. (Tokyo: 9962) announces that the Misumi 3D CAD Model library in CD-ROM format is now available upon request, free of charge, to machine builders, automation system designers and product design engineers.

The compact disks contain native CAD drawings of literally thousands of mechanical components offered in Misumi's 2009 Catalog.  This FREE two CD set provides users with a fast and convenient way to download native CAD drawings of Misumi components right to their PC and import them into various CAD applications, without the need to register on Misumi's Website.  Easy to use and access, the CAD drawings eliminate the time and labor that would otherwise be required to generate engineering drawings in-house.

Misumi's powerful on-line 3D CAD Configurator is at the heart of Misumi's unique business model.  It has long been highly popular among design engineers who regularly source Misumi's configurable and custom-designed components for their projects. 

With this powerful tool, engineers gain the ability to configure a part to precise tolerances and specifications − including critical dimensions, material and surface treatments − and download the native CAD file of the component into the assembly model. Once finalized, they can enter the order using Misumi's Web Ordering system (with no minimum order required), and input a part number, which will then become a purchased item and stored by that part number for future orders.    

According to Frank Bowman, engineer and designer for Betz Contracting & Machining, a Misumi machine builder customer, "Receiving a custom-ordered part from a vendor and being able to integrate it into our equipment without having to do any in-house work or modification on it is quite unusual.  With Misumi, we don't have to worry about that − we get exactly what we order, every time."  

Daniel Shirkey, business development manager of Orbitform Group, a manufacturer of standard and custom forming, fastening and assembly machinery, notes: "The time we save by downloading the model helps to shorten the overall duration of the design process. We estimate these downloads typically result in cost savings amounting to 15 to 40 percent, and time savings in the 50 percent range."

Those interested in ordering the Misumi 3D CAD CD's can enter a request at the Misumi USA website, http://www.misumiusa.com/Catalogs/request.aspx?Catalog=3844

 

About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of Misumi Corporation, a part of the Misumi Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as single-axis actuators, linear shafts, aluminum extrusions, linear guides, XY stages and other components for factory automation and various machine builds.  For a complete list of available components, please visit www.misumiusa.com.  


MEDIA CONTACT

COMPANY CONTACT
MISUMI USA, Inc.
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E.
pesposito@misumiusa.com