MISUMI Factory Automation Components
July 15, 2010
MISUMI
AND NEW STAINLESS STEEL PIPE FRAME SYSTEMS FOR FAST, EASY
ASSEMBLY
Versatile,
convenient and cost-effective, Factory Frame and Pipe Frame Systems include all
components required to assemble strong, durable storage racks and shelves,
mobile carts, in-plant pallets, and more.
Misumi USA, Inc., a subsidiary of Misumi Corporation, part of Misumi Group, Inc. (Tokyo: 9962) and a leading provider of fixed and configurable mechanical components for machine building and factory automation systems, recently introduced its new line of Factory Frame Systems, and has added a Stainless Steel Pipe System to its existing family of versatile metal pipe systems.
Both systems are fully configurable, offering users a convenient, cost-effective option for creating a wide array of temporary and permanent storage units, mobile conveyors and other equipment suitable for use in industrial, retail and commercial environments. Misumi's innovative system-based approach to its Factory Frame and Pipe Systems allows users to design, configure and assemble units to meet their exact application requirements, with all components included in a single purchase order and deliverable within a short period of time.
Aluminum Factory Frame Systems
Compared with conventional pipe frames, Misumi's aluminum alloy Factory Frames are designed to offer improved squareness at assembly by setting the frame dents securely in the joint tabs. So there is no need to "fix" several frames at a time, which enables easier assembly without the various parts twisting out of alignment. In addition, assemblers can make fine adjustments to each separate frame without disturbing adjacent or completed frames.
Misumi's new Factory Frame pipes include:
·
FFA (length
dimension configurable from 60 to 4000 mm)
· FFAKS (4000 mm fixed length, 5 pieces per pack)
Both products feature Aluminum Alloy construction with a Clear Anodized surface finish. For assembly, Misumi offers a wide range of Aluminum Alloy Joints in various configurations. Accessory parts for the Aluminum Factory Frame System include saddles, inner caps, pipe stand, adjusting bolt sets and casters. Shipping time for the Factory Frame Pipes is three (3) days.
Stainless Steel Pipe Frame Systems
A new line of Stainless Steel Pipe Frames, Joints and
Accessory Parts has been added to Misumi's comprehensive family of metal pipe
systems. The new Stainless Steel Pipe
products include:
·
PFSUS (length
dimension configurable from 60 to 2400 mm)
· PFSUSKS (4000 mm fixed length, 5 pieces per set)
Both products feature 430 Stainless Steel construction. For assembly, Misumi offers a wide range of Structural Steel Joints (Product Number PBLSS) in various configurations, including Orthogonal, 4 Directional Orthogonal, 4 Directional Parallel, 5 and 6 Direction Joints, Cross Type, and Free Joints. Additional accessory parts for the Stainless Steel Pipe Frame System include inner caps, insert nuts, adjusting bolt set and casters. Shipping time for the Stainless Steel Pipe Frames is six (6) days.
Clear directions for calculating frame dimensions are
provided in Misumi's print or E-Catalog.
For complete technical specifications, product types, sizes, materials, pricing
and ordering information on Misumi's selection of Factory Frame and Stainless
Steel Pipe Frame Systems, please visit http://us.misumi-ec.com
About MISUMI USA, Inc.
Located
in Schaumburg,
MEDIA
CONTACT
COMPANY CONTACT
MISUMI USA, Inc.
Patrick J. Esposito
Marketing Communications
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com
While we are not able to respond directly to comments submitted in this form, the information will be reviewed for future improvement.
Please use the inquiry form.
Customer Privacy Policy