Empowering Engineers with

Configurable Components

News

MISUMI'S STANDARD PRECISION POSITIONING STAGES OFFER EASY ALIGNMENT

MISUMI Factory Automation Components

April 14, 2011

MISUMI'S STANDARD PRECISION POSITIONING STAGES OFFER EASY
ALIGNMENT AND ADJUSTMENT, WHILE REDUCING OVERALL COSTS

With 22 new and legacy models in the line, users can select the right solution for
their applications - at prices 20 to 40 percent lower than conventional stages.

 

April 14, 2011 (Schaumburg, IL) MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (TOKYO: 9962), recently announced the addition of several new products to its family of Standard Precision Positioning Stages. 

These versatile devices are designed to meet a wide and diverse range of positioning application requirements. When compared with conventional high precision positioning stages, either purchased or produced in-house, the Standard Precision Positioning Stages offer excellent value - delivering a cost savings of 20 to 45 percent.  All styles are shipped in three days.

Standard Precision Positioning Stages are used by industrial companies to perform various positioning tasks in tooling jigs, manufacturing, assembly, testing and inspection, nesting, sensor adjustment.  Now with 22 different styles available in MISUMI's 2011 lineup, users can select from among a broad range of products, depending on specific application requirements such as: moving axes, positioning accuracy, load capacity, feed mechanism (rapid or fine), linear guidance structure (Dovetail, Cross Roller, or Linear Balls), and type of clamping mechanism.

All of MISUMI's Standard Precision Positioning Stages are quickly and easily adjustable without the use of tools.  Their simple, compact design and rugged construction provides long-term reliability, as well as ease of alignment and positioning repeatability. 

The new additions to the line include:

         Cross Roller X Axis (Right or left hand drive) Stages

         Low Profile Cross Roller XY Stages

         Dovetail Feed Screw Stages

         Low Profile Dovetail Rack & Pinion Stages, and Long Stages

         Rotary Stages

To assist design engineers in the selection process, MISUMI offers full technical information and mounting instructions in its 2011 print and eCatalog, where a detailed Precision Comparison Table is also available.  A Quick Reference Guide to Standard Position Stages is available on-line. Once the desired stage is selected, engineers can quickly download a native CAD data file into their project plan, saving design time and costs and eliminating the need for additional engineering drawings.  Pricing and ship times can be found online and orders can be placed through the Web Ordering System (WOS).

For more information about MISUMI's line of Standard Positioning Stages, visit http://us.misumi-ec.com/contents/mech/campaign/stage20110124/ or http://us.misumi-ec.com/contents/mech/product/ts/.

 

About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as leader pins, single-axis actuators, linear shafts, slotted keys, aluminum extrusions, parting locks, linear guides, XY stages and other components for factory automation, plastic mold and press die industries.  For a complete list of available components, please visit http://us.misumi-ec.com

MEDIA CONTACT
COMPANY CONTACT
MISUMI USA, Inc
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. 
pesposito@misumiusa.com