10 Products to Add to Your Wish List Bill of Materials

Treat your bill of materials for any application with MISUMI and MISUMI partner components. We have so much to choose from. Here’s a snapshot of a few of our favorites.

1. R-DLC NAAMS Locating Pin

R-DLC or Rainbow diamond-like carbon is just as pretty as it sounds. This coating can increase cycle rate and reduce replacement downtime because of its high wear resistance plus it’s easily identifiable.

2. THK Cut-to-Length Linear Guides

MISUMI has partnered with THK to provide linear guides to your length specifications.

3. Manual Positioning Stage

The accuracy! Stages come in the clutch when needing that minor movement. Visit our spotlight page to help select yours.

4. NAAMS Derived Custom NC Block

Your NC Block the way you need it for your fixture. Simply upload your 3D CAD Model to our dedicated website and receive a quote on your custom NC Block. Be the best on the block!

5. Cut-to-Length Cables

MISUMI cutting service can cut cable length up to 1m increments.

6. Linear Shafts

MISUMI’s shafts configurations are endless! Choose your material, surface treatment, tolerance, length, diameter, thread size, thread length, etc. We’ve reduced lead times too!

7. Pneumatic Fittings

One can never have too many pneumatic fittings! We’ve just partnered with PARKER HANNIFIN to provide the best in pneumatics. Choose your port size and material on our website.

8. MISUMI GV Conveyors

Everyone loves a good conveyor. There’s always something to move with them. Our fresh GV conveyors are lightweight and low maintenance. Check out our spotlight page for more features.

9. Dayton Lamina’s New Guided Retainers

These retainers are much better than the standard. Experience the space savings and cost savings in your die!

10. Dayton Lamina’s DAYLube

A nano-ceramic lubricating grease that is versatile and Food Grade! Add life to your components!

No more wishing, add any of these products to your Bill of Materials and explore our breadth of products at misumiusa.com.

Share this Story
Load More Related Articles
Load More By Carlicia Layosa
Load More In Featured Articles

4 Comments


  1. William Barker

    December 13, 2019 at 9:57 pm

    Carlicia,

    My name is William Barker, a mentor of FIRST FTC team 7244, Out of the Box Robotics. We are using your linear slides due to their improved performance as compared to rev robotics for our robot competing this year for Skystone. I would like to see if there are sponsorship opportunities for our team this year!

    Reply

    • Carlicia Layosa

      December 16, 2019 at 7:53 am

      Hi William!
      I will email you regarding FIRST Sponsorships!
      Thanks,
      Carlicia

      Reply

  2. simon laker000000000000

    January 3, 2020 at 7:05 pm

    hi my name is Simon Laker.
    i have a inquiry about ball screws .
    ive been attempting to design a 3d printer with ball screws on all axis.
    ive purchased several sfe 1616 type and have not been happy with the performance.
    1 x 600 mm long .
    1 x 550 mm long.
    with ends machined to suit bearings.
    could you advise me of the smallest diameter screw for fast travel .
    i’m interested in 40 mm lead pitch if possible .
    ground not rolled.if this is not possible please point me in the right direction.
    these are light load. have to with stand constant change of direction.
    zero back lash .
    kind regards simon laker.

    Reply

    • Carlicia Layosa

      January 6, 2020 at 7:42 am

      Hi Simon,

      Thanks for your inquiry! I have forwarded your application to our engineering team and they will get back to you w/ a recommendation.

      Thanks!
      Carlicia

      Reply

Leave a Reply to William Barker Cancel reply

Your email address will not be published. Required fields are marked *

*

Check Also

President Nobuyuki Ashida Wins Best CEO and Best CEO for Diversity from Comparably

There’s a buzz going around both virtually and ...

Subscribe to the Mech Lab!

Like us on Facebook

Follow us on Twitter @usa_misumi

Subscribe to our Channel