Part I: Comparing Rolled Ball Screws and Ground Ball Screws

At a high level, ground and rolled ball screws appear to function nearly identically within a wide range of mechanical applications.  However, the raceway surfaces, which are very similar to traditional machine screw threads found in a typical screw/nut system, are differentiated by the manufacturing process used to create these features.   Apart from the hardened ball bearings that make rotational motion possible, a ball screw system consists of two basic components: the leadscrew which possesses external threads and the ball nut which possesses internal threads.  A grasp of the two distinct manufacturing processes used to fabricate these components is the key to understanding both the strengths and limitations of rolled and ground ball screws.

Rolling and Grinding

Rolled ball screw threads are created by pushing each uncut bar stock blank through rotating tool dies in a single operation.  The driving principle behind this process is a cold work deformation process where the blank material is literally shaped by rolling tooling dies which are designed to form both the internal and external threads of the lead screw and ball nut.  Although the rolling dies come in a wide variety of shapes and sizes as required to roll various thread sizes, the deformation principle is the same for both internal and external threads.  The rolling process is highly efficient because no material is physically removed from the cut blanks, as would be the case in any cutting or grinding process.  The process is widely used throughout the industry because it can be easily automated to achieve high rates of production.

rolled screw method

Rolled ball screw threads are created by pushing each uncut bar stock blank through rotating tool dies in a single operation.

Conversely, ground screw threads are fabricated through an abrasion process that typically occurs in a horizontal setup where the material blanks rotate on their long axis between two machining centers while extremely hard abrasive cutters that are designed to cut a few threads at a time, carve out the threads from the cut blanks.  A similar process is employed for both internal and external thread cutting of the lead screw and ball nut.   This progressive abrasive machining process requires the material blanks to be cut to final length before grinding.  Varying cutter sizes and styles are used to grind the internal vs external threads, but the conceptual process is the same.

ground ball screw

Ground screw threads are fabricated through an abrasion process that typically occurs in a horizontal setup where the material blanks rotate on their long axis between two machining centers.

Strengths and Limitations

Rolled screw threads generally possess more strength than ground screw threads due to the significant material strengthening that is achieved as a result of the large plastic deformation induced in the material to create the threads during the rolling process.  Rolled threads are the more cost effective option because they can be quickly fabricated in automated rolling machine setups.  Because the rolling process is a considered to be a “one shot” process, any fabrication errors in the rolled screw threads are nearly impossible to fix.  Rolled threads also tend to possess rougher surface finishes than ground threads, and this can be especially problematic because rough surface threads can lead to reduced mechanical efficiency due to the higher rolling friction encountered in the rolling ball bearings.  A rough surface finish can also contribute to an overall decrease in the wear resistance of the ball screw system.

Finally, rolled ball screw systems are especially vulnerable to dimensional distortions as a result of die tooling wear. These sources of error can lead to a ball/nut system that possesses excessive backlash, which occurs due to a mismatch between the bearing diameter and screw shaft threads, and it also sharply decreases the positional accuracy that can be achieved.

Conversely, the thread grinding process is inherently more time intensive than the rolling process, partly because of the specialized grinding tools required for the cutting operation.  This translates into a significantly higher “off the shelf” price tag for ground ball screws compared to rolled ball screws.  However, there is a significant benefit achieved for the higher cost process because the ground threads can be held to tighter tolerances in relation to the centerline of the material blank because each thread is ground one at a time.  For these reasons, ground ball screws are almost exclusively employed in applications where high degrees of precision and repeatability are required.

Ballscrews

Profiles of rolled (left) and ground (right) ball screws

Finally, there is one last note that needs to be mentioned related to the heat treating and/or case hardening methods typically employed for the two types of ball screws.  In ground screw threads, the material blanks typically undergo case hardening before the threads are ground onto the blanks. Rolled screw threads undergo a similar case hardening process only after the threads have been rolled due to the fact that case hardened surfaces are too hard to go through the rolling operation.  The primary disadvantage to this type of post-rolling heat treatment is that it can lead to distortion in the rolled threads due to the intrinsically unpredictable material expansion rates in the thread geometry.

Conclusion

Rolled ball screw systems will generally cost significantly less than ground ball screws, and should be more than serviceable for use in most applications.  Both rolled and ground balls screws are available in a wide variety of lengths, diameters, and load capacities to fit a broad range of applications.  However, if very high degrees positional accuracy is required, to a high degree of repeatability, it may be more than worth the cost to opt for a precision ground ball screw system.  The engineer must carefully consider these distinctions when tasked with selecting between the two for any given machine application.

Share this Story
Load More Related Articles
Load More By Carlicia Layosa
Load More In Tips & Tricks

12 Comments


  1. Landon Solomon

    July 16, 2015 at 2:31 pm

    So….. Why not split the difference? It seems like a middle ground would be rolled, post-hardened threads that are then finish-ground for accuracy. Does the setup expense of the grinding operation preclude any savings from such an option?

    Reply

    • Dan

      July 16, 2015 at 3:04 pm

      I was thinking the same thing. The only answer that I could think of would be that the grinding process must be an active process that measures the cut dimension as the cuts are taking place. that would be the only way to compensate for grinding surface wear as the cuts progress. If that is the case, then it would take about the same amount of time to grind the pre-rolled screws as it would to grind the blanks. Rolling the screws would just become an added step that takes the place of the roughing cuts and requires another piece of equipment.

      Reply

    • misumiusa

      July 17, 2015 at 10:08 am

      The suggested option is possible for sure, sounds like a hybrid screw, which would likely wind up in the middle of both for accuracy, but need to go through both processes. Grinding or rolling are the industry standards for quite some time now, but there are other less common procedures out there depending on the manufacturer. Currently Misumi offers only the choice of roller or ground, but as the industry changes it’s not say that we might not offer other options in the future.

      Reply

  2. Dinesh Bramhapurkar

    July 16, 2015 at 11:34 pm

    Do we have possibility to create Hybrid Screw manufacturing process which will have initially Rolled threads little bit oversized & then grounding off the oversize to actual. This can add advantages of both processes like Strength from Rolling & tighter tolerances from Grounding operation. please let me know I gave any dumb idea 😉 🙂

    Reply

    • misumiusa

      July 17, 2015 at 10:08 am

      Dinesh, you’ve hit it spot on. A hybrid screw would likely wind up in the middle of both for accuracy, but need to go through both processes. Grinding or rolling are the industry standards and more common options, but there are other less common procedures out there depending on the manufacturer. MISUMI offers only the choice of rolled or ground as of now, but as the industry changes it’s not say that we might not offer other options in the future.

      Reply

  3. Ball Screw Applications | MISUMI USA Blog

    July 21, 2015 at 11:03 am

    […] The main function of a ball screw system is the efficient transfer of rotational motion to linear motion, sometimes to extremely high degrees of precision, accuracy, and repeatability.  Ball screws are typically differentiated by the manner in which the bearing threads were fabricated, either by a bulk deformation process called rolling, or by a precision grinding process.  For a more detailed discussion about the differences between these two types ball screw systems as general principles useful for selecting between the two types, see the previous blog entry Comparing Rolled and Ground Ball Screws. […]

    Reply

  4. Joe Humpamonkey

    August 5, 2015 at 12:06 am

    I’m waiting for the article where the roll form the nut…

    Reply

  5. Anjana Anand

    August 17, 2019 at 1:34 am

    Very Informative Blog On Rolled Ball Screw

    Reply

  6. Wesley Allen

    October 8, 2019 at 11:18 pm

    I’m building a triangular platform lift for an elevator in a small Log Cabin. I need three ball screw jacks 96 in Long. I will also need the hardware that goes with them 1 rolled ball screw (flanged) and the bearing supports for each 3/4″ rod.

    I do not have a lot of money I need to keep the cost down

    Reply

  7. Austin Saunders

    January 16, 2020 at 8:01 am

    It’s cool that ground screw threads are made with an abrasion process. My brother has been telling me about how he needs some new fasteners for a project that he’s starting soon. I’ll share this information with him so that he can find ones with the right threading.

    Reply

    • Carlicia Layosa

      January 16, 2020 at 8:22 am

      Hi Austin,

      That’s great! IF you or your brother has any questions regarding our products, feel free to reach out to our Engineering team at engineering@misumiusa.com

      Thank you!
      -Carlicia

      Reply

  8. Asif Shaik

    October 20, 2020 at 4:58 am

    The concept is very easy to understand with great visual images.

    Reply

Leave a Reply to Dan Cancel reply

Your email address will not be published. Required fields are marked *

*

Check Also

How Electric Vehicle Battery Packs are Manufactured

While most people know what components comprise a ...

Subscribe to the Mech Lab!

Like us on Facebook

Follow us on Twitter @usa_misumi

Subscribe to our Channel