Rotary Bearing Fits and Tolerancing

Rotary bearings are machine elements that support rotating shafts accurately while providing low friction conditions. In order to maintain a stable bearing performance over a prolonged duration, appropriate bearing fit design considerations are required to avoid any negative effects ([Chart 1]) that may arise from bearings‘ rotary operation.

[Chart 1] Common Issues & Solutions

Issue Side Effect Proposed Solution
Significant temperature increase due to high speed rotation. Shaft diameter may expand causing moment loads, resulting in bearing seizure, and uneven wear. Choose fitting dimensions with the anticipation of shaft expansion.
Thrust and radial direction clearance variations occurring from applied loads. Degradation of rotational accuracy. Abnormal noises. Choose fitting dimensions with anticipation of reformed clearances under load.

Design Examples of Rotary Bearing Applications

The example seen in [Fig. 1] is based on “Inner race rotation/Outer race retained”.

[Fig.1] Example - Inner race rotation : Outer race retained (loading in one direction)

Selection of Bearing Fits Based on Shaft Diameter

Transition fit or interference fit is selected to ensure the shaft and the inner ring will always rotate together.

[Chart 2] Selection Example of Fits (Radial Bearings)

Shaft/Bearing Fits Applicable For: Fit Standards
Transition Fit For light or varying loads h5, js6, k6, etc.
Interference Fit For general applications js5, k5, m5, m6, etc.

Selection of Fits For Bearing Holder Bores

Clearance fit should be chosen for ease of assembly while preventing any deformation of bearings‘ outer/inner races. In general, a Clearance fit (H7) is used. In case of light loading applications (H8) can be used, or (G7) when large temperature variations are to be expected.

[Chart 3] Fit Selection Examples For Bores (Radial Bearings)

Bore Fit Selection Applicable For: Fitting Standards
Clearance Fit General rotation applications H7
Clearance Fit Light loads H8 (wider tolerance than H7)
Clearance Fit Significant temperature increase G7 (large clearance)
Share this Story
  • Tips & Tricks

    Rotary Bearing Fits and Tolerancing

    Rotary bearings are machine elements that support rotating shafts accurately while providing low friction conditions. In order to maintain a stable bearing ...
  • lubricating rotary bearings
    Tips & Tricks

    Easy Maintenance Tips for Your Rotary Bearings

    Most production facilities have some kind of rotary bearings, and while they are working, no one gives them much thought. But as ...
Load More Related Articles
Load More By Carlicia Layosa
Load More In Tips & Tricks

Leave a Reply

Your email address will not be published. Required fields are marked *

*

Check Also

How Electric Vehicle Battery Packs are Manufactured

While most people know what components comprise a ...

Subscribe to the Mech Lab!

Like us on Facebook

Follow us on Twitter @usa_misumi

Subscribe to our Channel