The Issues that Occur with Soldering, Crimping, and Press Contact

Today’s electrical cable connectors are quite complicated to get it right for the do it your- self assembler unless they are well trained in several aspects of skilled assembly. Proper connections must be made between components for an item to function as engineers designed it to work. This post will discuss several areas of failures that occur when attempting to build a cable set without the necessary backgrounds in proper soldering or crimping and to a lesser degree – press-fit contacts.

Soldering

Soldering could be viewed as the most difficult skill to master. In fact, in the field of electronics manufacturers who assemble circuit boards, employers very often either hire personnel who are certified in soldering or train them internally to properly solder/re-solder as in wave soldering of entire boards. The art of soldering involves making sure the connection doesn’t result in numerous conditions that can cause failures now or sometime down the road.

The issues that can affect wire to connector pins are a connection that is made without proper flux cleaning of the metal surfaces. The right balance of heat and timing is required to allow soldering flux to fuse/weld the surfaces either a lead base solder or one that is lead-free – if required. Lead-free soldering is more difficult to get proper and long-lasting results. Soldering that allows too much heat will result in melted wire insulation and melting of the plastic connector body. Too little heat applied causes poor flux cleaning action and melting of the solder resulting in what many call “cold solder joint”. The solder will appear darker and less shiny than normal. Cold solder can break apart from the connection entirely.

Proper Soldering Tools

Other defects include excessive amounts of solder, too little amounts used, soldering wire at an angle rather than parallel to the pin and not removing flux buildup when necessary (conductive properties to adjacent contacts). Having a precision temperature-controlled soldering station is invaluable along with frequent tip cleanings, not to mention the correct tip for the job. Another defect that includes all wire connection types is too long an area of striped off insulation. Great hand /eye coordination, judgment skills, and patience are needed especially for soldering.

Soldering Issue Examples

Crimping

Crimping is another form of attaching wires. In this manner, expensive tools or machines are needed to physically bend the terminal end making strong electrical contact with the stripped wire end. And the number of terminal sizes available makes for an expensive outlay of capital to cover more than 1 or 2 sizes of manufacturing specialized tools of machines. Afterward, the crimped terminal is inserted into the connector but not fully completing the process.

Press Contact

The least labor-intensive electrical connection outside of purchasing cable assemblies is press contact. The wire end is stripped to the desired bare conductor and from there it is pushed into the terminal block where it is firmly held by specially designed metal “springs”. These connectors require proper stripping of the wires – neither too little bare wire or removing too much of the insulation can possibly lead to short-circuiting if wires touch or arching over of current.

Before the cable can be placed into use, a visual inspection must be performed to check for any missing parts, no damage exists, and the assembly needs to be tested for issues like being improperly wired (multiple wires misrouted) – this is checked by continuity testing which can also find the regular open connection. 

MISUMI Solution

MISUMI offers cable assembly services to create quality cables which are produced using manufactured tools and equipment. They are also soldered by certified soldering operators along with the cables passing the following quality tests:        

MISUMI’s Cable Product Certification


Share this Story
Load More Related Articles
Load More By Patrick Teagues
Load More In Featured Articles

4 Comments


  1. Betty Hunt

    March 16, 2020 at 7:30 am

    Glad to read this informative blog. Thanks for sharing the issue in the soldering crimping.

    Reply

  2. Alex Show

    April 27, 2020 at 12:55 am

    While I was searching for information for hardware tools here I found an informative blog on soldering crimping. Hardware tools are a necessity of the daily routine without it we can not solve hardware issues . Thank you for sharing such a piece of valuable information here.

    Reply

  3. John Shaw

    November 3, 2020 at 6:26 am

    yes, I go with you hand soldering is not easy task to perform. We should perform hand soldering in the presence of hand soldering master.

    Reply

  4. Ronald Smith

    November 17, 2020 at 5:11 am

    Found this post interesting where I got to know the issue occurring while we work on soldering , Crimping & Press Contact. This is a helpful post through which people will be aware of the methods mostly used in electronics industries.

    Reply

Leave a Reply

Your email address will not be published. Required fields are marked *

*

Check Also

Get it Twisted: Twisted Pair vs. Non-Twisted Pair Cables

How should I appeal to you, the reader?  ...

Subscribe to the Mech Lab!

Like us on Facebook

Follow us on Twitter @usa_misumi

Subscribe to our Channel