Skip to content

Loading...

News

AUGUST 2007 MISUMI NEWSLETTER

MISUMI Factory Automation Components

August 1, 2007

MISUMI
Empowering Engineers with Configurable ComponentsAugust 2007 - www.misumiusa.com
Refer New Customers, Get a $25 Best Buy™ Gift Card

Special Offers

Take advantage of the MISUMI Referrals = Rewards program today. Hurry to www.misumiusa.com/referrals and secure your $25 Best Buy Gift Card. This offer may not last for long so be sure to act now before it is too late. Simply refer three engineers to MISUMI and you could receive a $25 Best Buy Gift Card! 

Remember, there's never a minimum order requirement or a set up charge when you order from MISUMI. And the more customers we get means we can continue to offer you regular price reductions. 

Click Here to submit your referrals and take advantage of this offer!

New Single Axis Actuator from MISUMI

Single Axis ActuatorThrough October 31, 2007 customers that include promotion code KUA5PO when placing an order for the Single Axis Actuator will receive 5% off list price. 

Manufactured in 11 days with 208 possible configurations and a $1,073 starting price, the new Single Axis Actuator from MISUMI is the reliable way to bring linear motion to the machine that's quick, easy and affordable. Why build it yourself when you can configure it and buy it from MISUMI. The diameter and lead for the rolled ball screw are selectable as is the width and length for the aluminum base, making this one of the most configurable Single Axis Actuators available in the market today. 

Click here for more information on the new MISUMI Single Axis Actuator.

Product Spotlights

Here are some helpful products that offer a wide variety of materials and configurations, perfect for when material and configurability matter most.

Linear Shafts

Linear ShaftsWith materials ranging from Steel to Bearing Steel and Stainless Steel, MISUMI Linear Shafts can be configured in one-millimeter length increments. In addition, no drawings are required because engineers can use the MISUMI online CAD Configurator to design shafts to their specifications. The best part is engineers have a variety of shaft end configurations to choose from and all MISUMI Linear Shafts feature a standard manufacturing time of three days with same day or next day shipping available on some configured shafts. 

Click Here for more information on our entire line of Linear Shafts. 

Technical Guide: To help choose the right shaft, click here to view the Shapes and Material Selection Table.

Linear Guides

Linear GuidesFrom Carbon Steel to Aluminum, MISUMI offers an extensive line of materials for its linear guides. Configurable in 1mm length increments, MISUMI Linear Guides are available in regular and high grade for both standard and heavy load applications In addition, some MISUMI Linear Guides feature interchangeable blocks and rails with the ability to add additional blocks depending on the length of the rail and application. 

Click Here for more information on our entire line of Linear Guides. 

Technical Guide: For help in choosing the right guide for the right application, click here to view the Linear Guides Selection Guide.

Rods

RodsAvailable in Steel, Stainless Steel, Alloy Steel, Aluminum, Brass and Titanium, MISUMI Rods offer configurability in 1mm length increments as well as a selectable outer diameter. Perfect for multiple uses in factory automation, MISUMI Rods are ready to ship in 6 to 8 days and are priced to meet the design budget. 

Click here for more information on our entire line of Rods. 

Technical Guide: click here to view an example of how MISUMI Rods can also be used as posts.

Hexagonal Posts / Circular Posts / Square Posts

PostsOffering mostly Steel and Stainless Steel, with Aluminum as an option for select types, MISUMI Posts meet the needs of demanding applications where strength and rigidity play crucial roles in the performance of the machine. With configurable lengths in 1mm increments and an array of threaded and tapped end configurations, MISUMI Posts feature a variety of shapes, sizes and types as well as a host of surface treatments including Black Oxide, Electroless Nickel Plating, Black Chrome and Clear Anodizing. Configurability options are also available for the thread length and thread diameter for some types. 

Click here for more information on our entire line of Posts. 

Technical Guide: To help choose the right posts, click here to view the Shape and Material Selection Table.

Steel Plates / Stainless Steel Plates / Aluminum Plates / Copper Plates

PlatesWhy machine custom plates when you can configure plates from MISUMI and save valuable time and money? MISUMI Plates offer configurable dimensions in 1mm increments and arrive machined and ready to install. Available are a variety of steel, stainless steel, aluminum and copper materials so exact application needs can be met. 

Click here for more information on our entire line of Plates. 

Technical Guide: For help in choosing the right class of steel, click here to view the Steel Plates Reference Guide.