Skip to content

Loading...

News

MISUMI EXPANDS ITS LINE OF HEXAGONAL POSTS

MISUMI Factory Automation Components

September 11, 2008

MISUMI EXPANDS ITS LINE OF HEXAGONAL POSTS
FOR FASTENING, STANDOFF

More sizes, materials, finishes and configurable options

Hexagonal Posts - Small Web.jpg

Misumi USA, Inc. announces a major expansion in its popular lines of RoHS compliant hexagonal posts, used for mechanical fastening, standoff and general assembly of small devices and finished products, especially in electronics and general machine building.  

New small diameter (4-5.5mm) hex posts, in 303 stainless with one end tapped and one end threaded or both ends tapped, ideal for printed circuit board assembly.  Available in lengths from 5-20mm, configurable in 1mm increments, which allows for the ideal dimensional standoff for a particular design.  There are no set-up charges and standard shipping is three days. 

New hexagonal posts with configurable pilot diameter and length.  Available with one end threaded and one end tapped or both ends tapped, length configurable in 1mm increments from 20 to 800mm.  Also available are new hexagonal posts with side tapped holes for temporary positioning with both ends threaded, length is configurable in 1mm increments from 25 to 800mm.  Choices of materials are 1018 carbon steel, 304 or 316 stainless steel.  The 1018 carbon steel is available with black oxide or EN plating. There are no set-up charges, standard shipment is six days, and an express shipping option is available.

Many threaded configurations of Misumi hex posts can now be specified with a fine
thread option.   In addition to these hex post lines, Misumi also offers circular and square configurable post designs, plus a full range of stands, clamps, mounting brackets and strut bases to complement these posts. 

For more information and pricing on these products, please visit our website at www.misumiusa.com. 


About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a subsidiary of Japan based MISUMI Corporation. MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as, single axis actuators, linear shafts, aluminum extrusions, linear guides, XY stages and other components for factory automation.  For a complete list of available components, please visit www.misumiusa.com

MEDIA CONTACT

COMPANY CONTACT
MISUMI USA, Inc.
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E.
pesposito@misumiusa.com