MISUMI Factory Automation Components
January 1, 2009
MISUMI
INTRODUCES
MAGNETIC
Ideal design option for ultra low dust generating applications on assembly or transfer mechanisms

Misumi USA, Inc., a subsidiary of Misumi
Corporation, part of Misumi Group, Inc. (TYO:9962) announces a new line of magnetic transmission
drive components, ideally suited for design applications where the
non-contacting components result in ultra low dust generation. These applications include many cleanroom
assembly operations in the semiconductor, circuit board, business appliance and
consumer electronics markets. Additional
applications include those where the low noise and minimal vibration caused by
these components are critical to the assembly or transfer mechanism
performance.
These magnetic drive components from Misumi
operate on the principle of attractive force and thus function without
contact. Depending on the transmission
direction desired, Type MDQ allows perpendicular alignment, while Type MDY
allows parallel alignment. All
components are housed in 5056 aluminum with a gas emission prevention
treatment. Outside diameters from
16-35mm and inside diameters from 6-20mm are offered, with unit prices starting
at $34.00. Standard delivery is eight
days.
Once the alignment configuration is known, a
designer can calculate the required quantity needed, based on the size and
distance of the workload to be carried.
Then, a calculation of the required torque can be made, based on the
weight of the workload and specified quantity ordered.
Misumi magnetic transmission drive components
are ordered in pairs and should not be used with other manufacturers' magnets
or components.
All flux rate by temperature, torque rate by
distance change and magnetic flux density by distance from the drive
specifications are included in the new Misumi catalog, which can be ordered in
print or accessed online.
For more information and full pricing on these unique products, please visit our website at www.misumiusa.com. Application assistance is always available from Misumi engineers.
About MISUMI USA, Inc.- Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of Misumi Corporation, a part of the Misumi Group (TYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as single-axis actuators, linear shafts, aluminum extrusions, linear guides, XY stages and other components for factory automation and various machine builds. For a complete list of available components, please visit www.misumiusa.com.
MEDIA
CONTACT
COMPANY CONTACT
MISUMI USA, Inc.
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com
Your comments help us improve our website. Give feedback