MISUMI Factory Automation Components
February 10, 2009
MISUMI OFFERS
COMPREHENSIVE LINE OF
FIXED AND CONFIGURABLE METAL PLATES
Wide range of material,
configuration and finishing options to fit applications in
machine-building,
metalworking, factory automation, motion system design
Misumi USA, Inc., a subsidiary of Misumi
Corporation, part of Misumi Group, Inc. (TYO: 9962) provides an exceptionally wide range of fixed
and configurable Metal Plates in various sizes, thicknesses, materials and finishes. The product line is designed to meet the
diverse application needs of design engineers, manufacturing and assembly engineers,
and system designers/integrators in the machine-building, metalworking, industrial
automation and motion control industries.
Misumi offers its Standard Dimension Fixed
and Configurable Metal Plates in a broad array of materials, including structural
carbon steel, carbon steel, tool steel, pre-hardened steel, and stainless
steel, as well as aluminum alloys and rolled copper.
Precision Class Metal Plates are available for
users requiring exceptionally tight tolerances in plate length, width and
thickness. Misumi also provides Irregular Shape Plates, which include L, U and
T Shaped and Inclined Blocks, and Machined Circular Plates, in a variety of
sizes.
Applications for Misumi's carbon steel Metal Plates
include general machining (e.g., surface milling, surface and blanchard grinding). Applications for the stainless steel Metal Plates
include machine components requiring anti-rusting properties, such as machinery
designed for use in sanitary environments and in high moisture environments.
Material selection for Metal Plates will
depend on the user's specific application requirements, taking into account
such factors as: strength, hardness, brittleness, temperature range, weight, machinability,
weldability, ferrous characteristics, resistance to wear and corrosion.
With no minimum order requirements or set up charges on a product portfolio of more than 500,000 metric and inch mechanical components, Misumi has built its reputation as the premier global supplier of high quality factory automation components. At the heart of the Misumi business model is the unique CAD configurator and web ordering system. This unique business model offers customers an effective strategy for reducing costs and gaining competitive advantage through streamlined production and assembly processes and faster time-to-market. ll pricing information and delivery times are published in the catalog and website. For more information on Misumi's comprehensive selection of Aluminum Extrusions and Accessories, please visit our website at www.misumiusa.com.
About MISUMI USA,
Inc.
Located
in Schaumburg,
MEDIA
CONTACT
COMPANY CONTACT
MISUMI USA, Inc.
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com
Your comments help us improve our website. Give feedback