Skip to content

Loading...

News

NEW COUPLINGS FROM MISUMI USA

MISUMI Factory Automation Components

August 12, 2010

NEW COUPLINGS FROM MISUMI USA INCLUDE DOUBLE DISC CLAMPING TYPES,
PLUS HIGH RIGID, AND SUPER SHORT OLDHAM TYPES

MISUMI's comprehensive line of Couplings offers a wide choice of products, sizes and configurations for use with servo motors, and in other industrial machinery and motion control applications.

New_Couplings_235 x 235.jpg

MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (Tokyo: 9962) and a leading provider of fixed and configurable mechanical components for machine building and factory automation systems, has added new product designs to its comprehensive selection of Couplings - one of the largest and most diverse in the industry today.

MISUMI Coupling types include high precision Single Disc and Double Disc Clamping models, many of which are ideally suited for use with servo motors.  Also offered are Oldham, Slit and N Couplings, as well as Jaw, Sleeved, Bellows, and Resin types, in a variety of sizes and configurations.  Coupling components are typically used in the manufacture and assembly of industrial machines, as well as automation and motion control equipment and devices.

The new MISUMI Couplings products include:

 

  • SCXW, a Double Disc Type High-Precision Disc Clamping Coupling offering high torque with no backlash.  Ideal for connection to servo motors, its torsional rigidity is up to 26 percent higher than conventional (standard) disc clamping couplings.  Excellent for applications requiring faster positioning precision.  All the bolts are Trivalent Chromate plated and suitable for use in clean environments.
  • MFJGWK, a High Rigid Oldham Coupling, Set Screw Type, and MFJCGWK, a High Rigid Oldham Coupling, Clamping Type.  Both products feature an aluminum bronze spacer and have a keyed bore.  These couplings have allowable torque 2X higher compared to resin spacers. 
  • SCOC, a Super Short Oldham Coupling, Clamping/Spacer Type, a space-saving version suitable for use with miniature devices because it is 17 percent shorter than conventional types.

Most MISUMI Couplings ship in six (6) days, with the exception of the new High Rigid Oldham Couplings, which ship in eight (8) days.  Some Couplings offer optional express shipping for faster delivery.

Complete instructions for proper alignment adjustment of couplings, as well as specifications for allowable misalignment, can be found in MISUMI's print and online catalog.  Proper alignment adjustment of couplings is very important because the repeated use of couplings over their allowable misalignment's can rapidly shorten their life span or cause premature failure.  To prolong a coupler's life span, it is recommended to keep each misalignment within one-third (1/3) of the stated allowable value.

For complete technical information, product types and specifications, a detailed selection guide, pricing and ordering information on MISUMI Couplings, please visit http://us.misumi-ec.com

 About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as leader pins, single-axis actuators, linear shafts, slotted keys, aluminum extrusions, parting locks, linear guides, XY stages and other components for factory automation, plastic mold and press die industries.  For a complete list of available components, please visit https://us.misumi-ec.com/


MEDIA CONTACT

COMPANY CONTACT
MISUMI USA, Inc.
Patrick J. Esposito
Marketing Communications
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com