Skip to content

Loading...

News

MISUMI TO ATTEND ATX WEST

MISUMI Factory Automation Components

February 8, 2011

MISUMI USA UNVEILS NEW CONFIGURABLE COMPONENTS
AT 2011 AUTOMATION TECHNOLOGY EXPO WEST

New products include LX and KU Linear Actuator line extensions, Mini Conveyors, automotive style locating pins, factory frame joints, and more.

MISUMI also offers same day shipment option for in-stock components!

 

February 8, 2011 (Schaumburg, IL) MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (TOKYO: 9962), will highlight a host of new mechanical components for motion control, assembly and factory automation applications at this year's Automation Technology Expo West in Anaheim CA.  Machine building OEMs and automation system design engineers can learn more about the new products at MISUMI Booth Number 4121.

A sampling of the new MISUMI components include:

�         LX Series Linear Actuator line extensions, to include Actuators with Reverse Parallel Motor or Motor Wrap (for space-saving requirements).  No design time required - can be configured to precise specifications and standardized for fast, easy reordering.

�         KU Series Actuator line extensions, including nine new standardized types of Precision Class Single Axis KU Actuators.

�         Miniature Conveyors,  including a new, space-saving Flat Belt Single Track Mini Conveyor (70mm) with built-in motor drive, and a Dual Track Mini Conveyor (57mm), End Shaft Driven, which features a rugged carbon steel sprocket and Polyacetal plastic chain for ease of maintenance.

�         Configurable Automotive Style Locating Pins and Holders, in six different styles, developed specifically for leading automotive industry OEMs.

�         Gates PowerGrip GT Belt Series has been added to MISUMI's line of Timing Pulleys and Belts.  Offers shaft bore machining and surface treating options, yet ships in only six days!

�         Compact and cost-saving On-Off Switchable Magnet Blocks with Three-Sided Attraction.  Used primarily in assembly applications, the Magnet Blocks are about one-third the size of competitive units - at a fraction of the price.   

�         Factory Frame Joints in five new styles, a significant line expansion for easy assembly of MISUMI's highly popular Aluminum Extrusions, which are available in large array of profiles, styles and sizes.

�         New accessories designed for use in assembling factory floor carts, pallets and/or shelving built with MISUMI Aluminum Extrusions, include Adjustable Height Floor Stoppers and Skidproof Nuts.

Most MISUMI components are configurable, with downloadable CAD files and full specs and pricing available at the company's website at https://us.misumi-ec.com/.  The new products are also highlighted in the MISUMI 2011 Catalog of Mechanical Components for Factory Automation.

 

About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as leader pins, single-axis actuators, linear shafts, slotted keys, aluminum extrusions, parting locks, linear guides, XY stages and other components for factory automation, plastic mold and press die industries.  For a complete list of available components, please visit https://us.misumi-ec.com/

MEDIA CONTACT
COMPANY CONTACT
MISUMI USA, Inc
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. 
pesposito@misumiusa.com