MISUMI Factory Automation Components
March 24, 2011
MISUMI'S Z AXIS SIMPLIFIED ADJUSTMENT UNITS FEATURE RACK AND
PINION MECHANISM FOR EASY ALIGNMENT AND QUICK ADJUSTMENTS
The long-stroke, scaled post adjustment units clamp securely to
prevent misalignment due to shaft rotation ‒ they provide an economical choice
for less demanding positioning and adjustment of jig fixtures and other devices.
March 24,
2011 (Schaumburg, IL) MISUMI USA, Inc., a
subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (TOKYO: 9962), has
announced the addition of a new Z Axis Simplified Adjustment Unit to its diverse
selection of Simplified Adjustment Units designed for use in a variety of industrial
applications.
The
MISUMI Z Axis Simplified Adjustment Unit
(Part Number ZKB20)
is a long-stroke, scaled post, vertical travel positioning device commonly used
in manufacturing and assembly plants to make up-and-down height adjustments as
needed in positioning devices such as jig fixtures, cameras, sensors, spray
nozzles and the like. The units can also
be used for slotted hole adjustments and setup changes.
The
new Z Axis Simplified Adjustment units provide secure clamping to prevent shaft
rotation, and they feature an easy to read scaled post, and a rack and pinion
feed mechanism that allows for fast, easy adjustments with a simple rotation of
the handle. The result is more accurate alignment during setup and improved
stability in maintaining the proper position during operation.
Available
in various lengths to accommodate travel distances ranging from 70mm to 170mm,
the Z Axis Simplified Adjustment Units are ruggedly constructed to withstand
repetitive long-term use. The post
material is 304 Stainless Steel. The block is made of 6063 Aluminum Alloy with
a clear anodized finish and the handle is 5067 Aluminum Alloy. The rack and pinion gears are formed of 1045
Carbon Steel.
Brackets
for the ZKB20 Z Axis Scaled Post Simplified
Adjustment Units are sold separately so that users can select bracket types
that fit each installation surface (e.g., tabletop mounts, wall mounts).
In
addition to the new Z Axis Unit, MISUMI offers a comprehensive family of
Simplified Adjustment Units, designed for manual adjustment in less demanding
positioning applications. The simplified
units provide an economical alternative to building or purchasing the more
complex and costly precision stages often required in automated positioning
applications. The MISUMI line includes
Feed Screw, Push Screw and Rack & Pinion feed mechanisms, and the products are
offered in a variety of axis styles.
For more information about MISUMI's new Z Axis Rack & Pinion Simplified Adjustment Unit, as well as the company's entire product line, visit https://us.misumi-ec.com/.
About MISUMI USA, Inc.
Located
in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a
Subsidiary of MISUMI Corporation, a part of the MISUMI Group
(TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and
configurable components such as leader pins, single-axis actuators, linear
shafts, slotted keys, aluminum extrusions, parting locks, linear guides, XY
stages and other components for factory automation, plastic mold and press die
industries. For a complete list of available components, please visit https://us.misumi-ec.com/
MEDIA CONTACT
COMPANY CONTACT
MISUMI USA, Inc
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com
Your comments help us improve our website. Give feedback