Skip to content

Loading...

News

MISUMI TO ATTEND ATX CANADA

MISUMI Factory Automation Components

May 16, 2011

MISUMI USA TO PRESENT NEW CONFIGURABLE COMPONENTS AT
2011 AUTOMATION TECHNOLOGY EXPO CANADA

New products include low cost Positioning Components, LX and KU Linear Actuator line extensions, Mini Conveyors, Automotive Style Locating Pins, Factory Frame Joints, and more.


May 16, 2011 (Schaumburg, IL
) MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc.(TOKYO:9962),will highlight a host of new mechanical components for motion control, assembly and factory automation applications at this year's Automation Technology Expo Canada, June 21-23, inToronto.  Machine building OEMs and automation system design engineers can learn more about thenew products at MISUMI Booth Number 939.

Samplings of the new MISUMI components include:

�         New Low Cost positioning solutions includingStandard Precision Positioning Stages and Simplified Adjustment Units.

�         LX Series Linear Actuator line extensions, to include Actuators with Reverse Parallel Motor or Motor Wrap (for space-saving requirements).  No design time required - can be configured to precise specifications and standardized for fast, easy reordering.

�         KU Series Actuator line extensions, including nine new standardized types of Precision ClassSingle Axis KU Actuators.

�         Miniature Conveyors,including a new space-saving Flat Belt Single Track Mini Conveyor (70mm) with built-in motor drive, and a Dual Track Mini Conveyor (57mm), End Shaft Driven, which features a rugged carbon steel sprocket and Polyacetal plastic chain for ease of maintenance.

�         ConfigurableAutomotive Style Locating Pins and Holders, in six different styles, developed specifically for leading automotive industry OEMs.

�         Gates PowerGrip GT Belt Series, an additionto MISUMI's line of Timing Pulleys and Belts.  Offers shaft bore machining and surface treating options, yet ships in only six days!

�         Compact and cost-saving On-Off Switchable Magnet Blocks with Three-Sided Attraction.Used primarily in assembly applications, the Magnet Blocks are about one-third the size of competitive units - at a fraction of the price. 

�         Factory Frame Joints in five new styles, a significant line expansion for easy assembly of MISUMI's highly popular Aluminum Extrusions, which are available in large array of profiles, styles and sizes.

�         New accessories designed for use in assemblingfactory floor carts, pallets and/or shelving built with MISUMI Aluminum Extrusions, include Adjustable Height Floor Stoppers and Skidproof Nuts.

Most MISUMI components are configurable, with downloadable CAD files and full specs and pricing available at the company's website at https://us.misumi-ec.com/.  The new products are also highlighted in the MISUMI 2011 Catalog of Mechanical Components for Factory Automation.

For more information, customers can contact their MISUMI USA Account Manager, call Customer Service at 800-681-7475 or visit https://us.misumi-ec.com/

  

About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as leader pins, single-axis actuators, linear shafts, slotted keys, aluminum extrusions, parting locks, linear guides, XY stages and other components for factory automation, plastic mold and press die industries.  For a complete list of available components, please visit https://us.misumi-ec.com/

MEDIA CONTACT
COMPANY CONTACT
MISUMI USA, Inc
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. 
pesposito@misumiusa.com