Skip to content

Loading...

News

MISUMI ADDS NEW POSITIONING STAGES

MISUMI Factory Automation Components

July 7, 2011

MISUMI ADDS NEW POSITIONING STAGES TO LINE OF
LOW-COST STANDARD PRECISION POSITIONING SOLUTIONS
 

New Dovetail Slide Feed Screw, Low Profile Cross-Roller, and Rotary Standard Precision Stages
offer users more affordable choices, greater design flexibility.

 

PR_Stage-XYCRSC-200 X 200.jpg

July 7, 2011 (Schaumburg, IL) ― MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (Tokyo: 9962), has announced the addition of three new Standard Precision Positioning Stages to its comprehensive selection of low-cost positioning solutions. 

MISUMI's Standard Precision Positioning Stages combine streamlined functionality with precision levels acceptable for a great many automation-related applications - at prices 20 to 50 percent lower than typical high precision positioning devices.  Standard Precision Stages provide adequate levels of precision relative to straightness, parallelism, and parallelism of motion. They are ideal for use as adjustment units in assembly, inspection and processing instruments and jigs used by discrete and process OEMs across a wide range of industries.

The three new Positioning Stages include:

·         Standard Precision Dovetail Slide Feed Screw - a positioning mechanism consisting of two precision ground flat surfaces sliding against each other. The new models feature fine-feed dovetail slide stages with 0.5 mm travel per rotation. Product versions include: X-Axis Stages (XFEX), XY-Axis Stages (XYFES) and Z-Axis Stages (ZFES), with each offered in a choice of models based on clamping position, travel distance and allowable load with straightness accuracy of 50um.

·         Standard Precision Cross-Roller, Low Profile (XYCRSC) - An accurate, low profile positioning guide incorporating two cross-rollers connecting upper and lower plate. The device can perform finely tuned adjustments in 0.01 mm increments, with selectable micrometer head (head positions include center, standard and reversed).

·         Standard Position Rotary Stages (RTRS) - a rotary stage that provides simple 360˚ wide angle adjustments, as well as fine-tuned +/- 5˚ adjustment with standard or reversed position micrometer head.

All three of the new products ship in just three (3) days. For more detailed information about the new, low-cost Standard Precision Positioning Stages and MISUMI's entire line of positioning solutions, including technical information, application examples, pricing and delivery times, go to http://us.misumi-ec.com.

About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as leader pins, single-axis actuators, linear shafts, slotted keys, aluminum extrusions, parting locks, linear guides, XY stages and other components for factory automation, plastic mold and press die industries.  For a complete list of available components, please visit MISUMI USA.

MEDIA CONTACT

COMPANY CONTACT 
MISUMI USA, Inc.
Patrick J. Esposito 
Marketing Manager 
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com