MISUMI Factory Automation Components
September 22, 2011
MISUMI UNVEILS DOUBLE SPEED CHAINS
AND SPROCKETS IN MATCHED SETS,
OFFERING A COMPLETE SOLUTION FOR ASSEMBLY OF FREE
FLOW CONVEYORS
Mixed structure small and large
diameter rollers enable the chain to convey
work parts and products 2.5 times
faster than the chain speed.
September 22, 2011 (Schaumburg, IL) ― MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (Tokyo: 9962), has unveiled a complete line of Double Speed Chains and Sprockets, which can be used to assemble and install free flow conveyor lines in industrial settings. Also included in the matched product line are Extruded Aluminum Frames and Return Guides for the Double Speed Chains. Free flow conveyors are used to transport parts, work pieces or finished goods from area to area within manufacturing, processing and assembly plants.
MISUMI's new Double Speed Chains and Sprockets product line-up includes:
· Double Speed Chains (WCHE) featuring a mixed construction of small and large diameter roller wheels, which allows conveyed items to move along at 2.5 times the speed of the actual chain speed. The chains are ruggedly constructed of carbon steel plates and engineered plastic rollers to provide durability and long service life. They are available in a range of sizes and configurations to accommodate user requirements.
· Sprockets for Double Speed Chains (WESP) are equally durable, offering 1045 carbon steel construction, precisely machined teeth, and shaft bore specification options.
· Extruded Aluminum Frames (WCF) and Return Guides (RNG) are available to complete the matched conveyor belt assembly package. The frames are made of 6063-TS Aluminum Alloy with a High Density Polyethylene (HDPE) top cover.
The Double Speed Chains, Sprockets, Frames
and Return Guides all ship in 6 days. A
complete guide to product sizes, specifications and pricing can be found in
MISUMI's 2011 Catalog and eCatalog.
With no minimum order requirements or set-up
charges on a product portfolio of more than 1,000,000 metric and inch mechanical
components, MISUMI has built its reputation as the premier global supplier of
high quality factory automation components.
At the heart of the MISUMI business model is the unique CAD Configurator
and convenient Web Ordering System.
Exclusive to MISUMI, this business model offers customers an effective
strategy for reducing costs and gaining competitive advantage through
streamlined production and assembly processes and faster time-to-market.
About MISUMI USA, Inc.
Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as leader pins, single-axis actuators, linear shafts, slotted keys, aluminum extrusions, parting locks, linear guides, XY stages and other components for factory automation, plastic mold and press die industries. For a complete list of available components, please visit MISUMI USA.
MEDIA
CONTACT
COMPANY CONTACT
MISUMI USA, Inc.
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com
Your comments help us improve our website. Give feedback