MISUMI Factory Automation Components
September 21, 2011
MISUMI NOW OFFERS MX
LUBRICATION OPTION FOR LX SERIES ACTUATORS
AND LINEAR GUIDES TO OPTIMIZE
SERVICE LIFE
Polyurethane
micro-particle self-lubricating agent improves component performance and
service life, while reducing maintenance time and costs.
September 21, 2011 (Schaumburg, IL) ― MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (Tokyo: 9962), has announced that it will now offer its exclusive MX Lubrication option for the company's LX Linear Actuator Series and comprehensive line of Linear Guides.
The MX Lubrication option refers to the addition of a special polyurethane lubricating agent containing interconnected micro-particles that enable it to supply an optimal amount of lubrication on the track surface over the life of the actuators and guides, resulting in extended, maintenance-free operation. And, by providing a continuous lubrication between the rolling elements and their races, the MX self-lubricating system also acts as an effective seal, protecting the ball-nut and the linear rail from contamination. In the LX Actuators, the MX self-lubrication cartridges are mounted on both sides of the LX bearing block, lubricating both the ball screw and the integrated linear bearing rails with every motion of the actuator.
In addition to reducing maintenance time and costs, MISUMI's newly available MX Lubrication option also improves the efficiency and friction-free performance of all sizes of LX Linear Actuators and Linear Guides.
MISUMI'S LX Actuators and Linear Guides
MISUMI's popular LX Series Linear Actuators
offer optimal versatility for designers of motion control machinery and
devices. For example, the selection
includes:
·
Thousands of configurations designed for a
broad and diverse range of applications, such as servo press machines,
precision conveyance of parts, measuring devices, painting units, and more
·
Five different profiles, ranging in length
from 75 mm to 500 mm, including styles with or without covers
·
High precision, high speed types, and
actuators designed for heavy load capacity, all available at competitive prices
and with short lead times
· Motorized versions with both metric and NEMA motor mounts (prices include standardized motors)
MISUMI also offers an extensive line of Linear Guides, including miniature guides and guides designed for light, medium and heavy loads.
MISUMI
Offers One-to-One Technical Assistance
There are many factors for engineers to consider and numerous calculations to make in specifying linear motion components - from precise rail length sizing to load, speed and positioning accuracy. MISUMI offers one-to-one technical assistance to help design engineers configure, select and specify exactly the right linear motion components for their industrial automation machinery and motion control systems. This personalized service is provided by the company's team of experienced engineers and is available online or over the phone.
For
more information on these and all of MISUMI's products and services, visit Booth
Number 2108 at Design & Manufacturing Midwest, or visit https://us.misumi-ec.com/.
About MISUMI USA, Inc.
Located
in Schaumburg,
MEDIA CONTACT
COMPANY CONTACT
MISUMI USA, Inc
Patrick J. Esposito
Marketing Manager
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.com
Your comments help us improve our website. Give feedback