Business Benefits of Standardizing on Configurable vs. Custom Components Purchasing configurable components from a reliable outside source can not only reduce production costs, but can also save significant time and effort at the front end, in the design and procurement processes. The fact is that automation machine builders and integrators...More>> |
Customer Service TEL: 1-800-681-7475 / 847-843-9105 Email:inquire@misumiusa.com Monday - Friday 8:00AM - 7:00PM (CST) |
| | | Featured Case Study: NISSIN BRAKE OHIO'S MODULAR DESIGN STRATEGY USES CONFIGURABLE COMPONENTS TO GAIN TIME AND COST SAVINGS Nissin Brake Ohio, Inc., in Findlay, Ohio, is a Tier 1 supplier of brake and control system parts and assemblies for automotive and non-automotive applications. Established in 1988 by Japanese manufacturer, Nissin Kogyo Co. Ltd., Nissin Brake serves numerous high-profile automotive OEMs, such as Honda, Harley-Davidson and GM to name a few. With its primary manufacturing plant in Findlay, Nissin Brake also supports production in Rock Spring, GA, and research and development facilities... More>> |
MISUMI'S SIMPLIFIED SLIDE RAILS PROVIDE VERSATILE, COST EFFECTIVE SOLUTIONS FOR LINEAR MOTION DEVICES AND APPLICATIONS The Simplified Slide Rails are suitable for use in a host of non precision positioning functions; for example, platform mounted inspection and detection devices, parts feeding devices, and linear guides used to transfer items from one process area to the next and they can be used effectively in both manual or automated linear motion operations. Compared with conventional high precision positioning products, they are more compact and lighter in weight. Product offerings include standard and specialized product versions, optional features and configurable lengths, with selection depending on each user's application needs relative... More>> |
100,000 ADDITIONAL MACHINED TO ORDER PARTS NOW SHIP IN 4 DAYS.
MISUMI has shortened the lead time for more than 100,000 components, this allows machine and automation system OEMs to build products faster and more efficiently. More>> |
|
|