MISUMI Factory Automation Components
October 31, 2012
MISUMI
ANNOUNCES WEST COAST AVAILABLITY OF ALUMINUM EXTRUSIONS
Locally stocked product will lead to
significantly reduced ship times for aluminum extrusions and accessories to West
Coast customers

Schaumburg, IL - October 31, 2012 - MISUMI
USA,
Inc., a subsidiary of MISUMI Corporation, part of MISUMI
Group, Inc. (Tokyo:
9962),
announced today the addition of its expansive line Aluminum Extrusions and
accessories to its West Coast Distribution Center.
Typical applications for aluminum extrusions include:
safety guarding, enclosures, work stations, light machine bases,
shutters, robotic jigs and fixtures, as well as many other applications
suitable for use in a variety of industries.
With the addition of the aluminum
extrusions to
the West Coast facility, over 80 percent of Misumi's most popular aluminum
extrusions will be available locally.
Additional key advantages of using MISUMI Aluminum
Extrusion
Machining
alterations:
Selection of Misumi Aluminum
Extrusions and Accessories will depend on the user's specific
application requirements, taking into account such factors as: load-bearing
strength, hardness, rigidity, tensile strength, finished product dimensions and
desired finish.
With no minimum order requirements or set-up charges on a
product portfolio of more than 1,000,000 metric and inch mechanical
components, MISUMI has built its reputation as the premier global
supplier of high quality factory automation components. At the heart of
the MISUMI business model is the unique on-demand
CAD
Configurator and convenient electronic commerce on the one-stop Web.
Exclusive to MISUMI, this business model offers customers an effective strategy
for reducing costs and gaining competitive advantage through streamlined
production and assembly processes and faster time-to-market.
About MISUMI USA, Inc.
Located in
Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary
of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI
USA, Inc. is a leading supplier
of fixed and configurable
components such as bearings, leader pins, single
axis actuators, linear
shafts,
slotted keys, aluminum
extrusions,
parting locks, locating
pins,
linear
guides, XY
Stages and other components for factory automation, plastic mold and
press die industries. For a complete list of available components, please
visit MISUMI USA.
MISUMI USA, Inc.
COMPANY CONTACT
Patrick J. Esposito
Marketing Communications
P. 847-843-9105
F. 847-592-5922
E. pesposito@misumiusa.comYour comments help us improve our website. Give feedback