News

MISUMI USA SHOWCASES LINEAR GUIDES AT ATX CANADA

MISUMI Factory Automation Components

May 14, 2013

Linear_Guides_448 x 258.jpg

Exceptionally wide variety of product models and rapid delivery times allow design engineers to select the right linear motion solution for small, medium, heavy and ultra-heavy loads.

MISUMI USA, Inc., a subsidiary of MISUMI Corporation, part of MISUMI Group, Inc. (Tokyo: 9962), will display its extensive portfolio of Linear Guides at ATX Canada, Booth #939.  Demonstrations will be available for machine and automation system design engineers seeking rugged and reliable linear motion solutions. In addition, shipping time for 95 percent of MISUMI Linear Guides is just six (6) days or less.

MISUMI's Linear Guide product line-up includes:

·         Interchangeable types in which the block and rail are sold separately and non-interchangeable types in which the block and rail are sold as a matched set.

·         Miniature Guides in a variety of styles designed for lighter loads.  These have two rows of contacting steel balls in a 4-point raceway contact design.

·         Medium and Heavy Load styles designed for heavier loads, including Ultra- and Extra Super Heavy loads. These have four rows of contacting steel balls in a 2-point raceway contact design. 

·         Low Temperature Black Chrome Plated types, featuring a 5 µm fluoropolymer layer chemically deposited as a black film on rails and blocks.  This protective coating results in a durable finish that resists corrosion and is immune to cracking and flaking, even under repeated bending.

·         A wide range of standard and customized design options, including short blocks, long blocks, wide blocks, blocks with dowel holes, and dust-resistant versions for use where dust and machining chips pose a hazard to smooth operation.

·         Accessories, such as clamp, bolt and plate stoppers, height adjusting blocks, locking units and cross roller tables.

The Linear Guides utilize steel balls rolling on precisely ground raceways, with the balls being recirculated by plastic return caps.  In selecting linear guides, design engineers must consider various specifications, such as allowable load and clearance requirements. Product experts will be available at the booth to provide engineering assistance using MISUMI's easy-to-use online CAD Configurator. 

To ensure proper installation, MISUMI's Linear Guides feature a datum surface―a surface with a straight groove―on both the rail and the block to help users align the units correctly.

With no minimum order requirement or set-up charges, MISUMI has built its reputation as the premier global supplier of high quality factory automation configurable components. At the heart of the MISUMI business model is the unique on-demand CAD Configurator and easy to navigate website. This unique business model offers customers an effective strategy for reducing costs and gaining competitive advantage through streamlined production and assembly processes and faster time-to-market.   

About MISUMI USA, Inc.

Located in Schaumburg, Illinois, MISUMI USA, Inc. was established in 1988 as a Subsidiary of MISUMI Corporation, a part of the MISUMI Group (TOKYO: 9962). MISUMI USA, Inc. is a leading supplier of fixed and configurable components such as Bearings, leader pins, single axis actuators, linear shafts, slotted keys, aluminum extrusions, locating pins, linear guides, XY Stages and other components for factory automation, plastic mold and press die industries.  For a complete list of available components, please visit MISUMI USA.


COMPANY CONTACT    

MISUMI USA, Inc.        

Patrick J. Esposito         

Marketing Communications

P. 847-843-9105

F. 847-592-5922

E. pesposito@misumiusa.com