6061 and 6063 Aluminum Alloy Products

Aluminum Alloy 6061 vs 6063

Aluminum 6061 and 6063 are often compared because they share many of the same advantages, but they are designed for different strengths. Both offer good corrosion resistance and versatility, yet they differ in mechanical properties, finish quality, and the types of applications they are best suited for. In practice, choosing between them usually comes down to whether the job calls for greater structural strength (6061) or better extrudability and appearance (6063).

What is Aluminum 6061?

Aluminum 6061 is a heat-treatable alloy in the 6xxx series, meaning its primary alloying elements are magnesium and silicon. That combination gives it a useful mix of mechanical strength, corrosion resistance, and general manufacturability. One of the defining characteristics of 6061 is its versatility. It can be machined, welded, formed, and finished without the material becoming overly specialized for just one type of use. In practical terms, that makes it a dependable choice for components that need to perform well across more than one requirement, such as strength, weight reduction, weather resistance, and fabrication efficiency. It is frequently used for structural parts, frames, plates, brackets, supports, and machined components where a balance of durability and manageable weight is important.

What is Aluminum 6063?

Aluminum 6063 is widely used when a part needs to be produced in a precise cross-sectional shape with clean lines, consistent geometry, and a refined finished appearance. Because of that, 6063 is commonly seen in products made from extruded profiles rather than heavier plate- or bar-based components. It is well suited for creating complex or detailed shapes, including profiles with thin walls, rounded edges, channels, and other design features that would be more difficult to produce efficiently in many other alloys.

6061 vs 6063 Mechanical Properties

Property Aluminum 6061-T6 Aluminum 6063-T6
Density 0.0975 lb/in³ (2.70 g/cm³) 0.0975 lb/in³ (2.70 g/cm³)
Ultimate Tensile Strength 45,000 psi (310 MPa) 35,000 psi (241 MPa)
Yield Strength 40,000 psi (276 MPa) 31,000 psi (214 MPa)
Elongation at Break 12% 12%
Brinell Hardness 95 73
Elastic Modulus 10,000 ksi (68.9 GPa) 10,000 ksi (68.9 GPa)
Shear Modulus 3,760 ksi (25.9 GPa) 3,770 ksi (26.0 GPa)
Shear Strength 30,000 psi (207 MPa) 22,000 psi (152 MPa)
Fatigue Strength 14,000 psi (96.5 MPa) 8,000 psi (55.2 MPa)
Melting Range 1,080–1,205°F (582–652°C) 1,130–1,210°F (610–655°C)
Thermal Conductivity 1167 BTU-in/hr-ft²-°F (167 W/m·K) 1390 BTU-in/hr-ft²-°F (200 W/m·K)
Electrical Conductivity 40% IACS 53% IACS
Mechanical properties shown are typical reference values for 6061-T6 and 6063-T6. Actual values can vary by product form, manufacturing method, and supplier specification.

6061 vs 6063 Strength Comparison

  • 6061 is generally the stronger alloy. In most standard tempers, it offers higher tensile and yield strength than 6063.
  • When a component must resist bending, distortion, or service stress, 6061 usually provides more margin without requiring the profile to be oversized.
  • 6063 strength is ok for many applications, but it is more often used in parts where the design is shaped around profile requirements rather than maximum load-bearing performance.
  • A nicely designed 6063 profile can still perform effectively in lighter-duty applications, but matching the performance of 6061 may require a larger or more optimized cross section.
  • The exact strength of both 6061 and 6063 depends on condition and heat treatment, so the most accurate comparison is always between equivalent tempers rather than alloy numbers alone.

Applications of 6061 vs 6063

Application Area Aluminum 6061 Aluminum 6063
Structural Components Commonly used for frames, supports, brackets, base plates, and load-bearing assemblies where higher strength is needed. Used less often for structural duty; more suitable for lighter-duty shapes where appearance and profile consistency matter more than strength.
Machined Parts Widely used for machined components such as fixtures, mounts, couplings, and equipment parts. Less commonly selected for machining-heavy parts; usually chosen when the final shape is primarily produced by extrusion.
Architectural Profiles Can be used, but is not typically the first choice when surface finish and intricate profile design are the main priorities. Very common for window frames, door frames, railings, trim, curtain wall components, and decorative profiles.
Industrial Framing Frequently used in machine bases, workstations, guards, and custom structural assemblies that benefit from added rigidity. Also common in extruded framing systems, especially where clean geometry and lighter-duty performance are sufficient.
Transportation Equipment Often used in truck bodies, marine fittings, bicycle components, and automotive or trailer parts. Used in trim, rails, and appearance-oriented transportation components rather than more demanding structural parts.
Electrical and Thermal Applications Used where a balance of strength and conductivity is needed, including housings and support structures. Common for heat sinks, conduit shapes, and enclosure profiles where formability and conductivity are beneficial.
Anodized Components Can be anodized successfully, though finish uniformity is not always the main reason it is selected. Frequently chosen for anodized parts because it tends to produce a cleaner, more uniform finished appearance.
Piping and Tubing Used for tubing and pipe in applications where mechanical performance is important. Often used for extruded tubing and hollow profiles where shape quality and finish are key considerations.
Custom Extrusions Suitable for custom extrusions that must balance shape complexity with stronger end-use performance. Preferred for complex, thin-wall, or appearance-sensitive custom extrusions.
Application tendencies shown here reflect common industry use patterns. Final material selection still depends on strength requirements, extrusion complexity, finishing needs, and the demands of the specific design.

Parting Thoughts

MISUMI USA carries a wide range of industrial manufacturing components – including Metal Plates & Blocks, and Metal Cylinders & Rods – for your next project or machine fix. If you have any questions about measurement or sizing for your Aluminum Alloy needs, feel free to connect with our product experts, and engineers. Also, if you are looking for more insights be sure to check out our other blog articles, including: Aluminum Alloy – Uses in Manfacturing, Mechanical Properties of Aluminum Alloys, and more.

Author: Scott Bredemann | Updated: 3/19/2026

Disclaimer:
The content on this webpage is for informational purposes only. MISUMI makes no guarantees, expressed or implied, regarding the accuracy, completeness, or validity of the information. Performance parameters, tolerances, designs, materials, or processes should not be assumed to reflect third-party suppliers’ or manufacturers’ deliverables within MISUMI’s network. Buyers are responsible for specifying their part requirements.