Polymer Pellets,Masterbatch, Polymer,Raw Material, Industry

7 Types of Nylon | Key Variants and Their Applications Within Manufacturing & Industry

Author: Scott Bredemann | Updated: 02/7/2025

Nylon is one of the most versatile and widely used materials in modern manufacturing, playing a pivotal role in industries ranging from textiles to automotive engineering. Its durability, flexibility, and performance make it indispensable—but did you know that nylon comes in multiple specialized variants, each tailored for specific applications? In this article, we’ll explore seven key types of nylon, uncovering their unique properties and the critical roles they play across industries.

The Origins of Nylon

We can trace nylon’s story back to the pioneering work of Wallace Carothers at DuPont in the 1930s. Seeking a new synthetic fiber, Carothers’ team stumbled upon a revolutionary material with exceptional properties. This marked the birth of nylon, forever changing the landscape of textiles and beyond.

7 Types of Nylon

1. Nylon 6: The MVP of nylons, Nylon 6 is known for its well-rounded characteristics, making it a popular choice for textiles (think carpeting and activewear), packaging films, and even automotive parts. Its affordability and versatility are undeniable, but it can absorb moisture, affecting dimensional stability.

2. Nylon 6,6: Renowned for its robust molecular structure, Nylon 6,6 offers superior strength and durability. It thrives in engineering applications like gears and bearings, finds its way into industrial components, and even forms the backbone of some clothing items. While highly dependable, its production process demands slightly higher costs.

3. Nylon 6,10: This unique variant boasts a different chemical makeup, translating to exceptional processing properties and high melting points. The oil and gas industry relies on Nylon 6,10 for its pipelines, but it’s also used in automotive parts and various consumer goods. It can be more expensive than Nylon 6, but its specific properties often justify the cost.

4. Nylon 4,6: Standing out from the crowd, Nylon 4,6 shines in high-temperature environments. Its exceptional thermal stability makes it ideal for electrical components and demanding industrial applications. However, its production is less common compared to other nylons, potentially affecting availability.

5. Nylon 11: Embracing sustainability, Nylon 11 is derived from castor beans, a renewable resource. This eco-friendly twist doesn’t compromise on performance – Nylon 11 offers impressive flexibility and resilience. It finds applications in gas and oil pipelines, tubing, and even as protective coatings. While its eco-credentials are a plus, production costs can be higher than traditional nylons.

6. Nylon 12: When it comes to chemical resistance, Nylon 12 reigns supreme. This durable variant is a favorite for automotive fuel lines, hydraulic hoses, and cable sheathing, where withstanding harsh chemicals is crucial. Its exceptional performance comes at a price, as Nylon 12 can be more expensive than some of its counterparts.

7. Bio-Based Nylon: The future is green! Bio-based nylon represents an exciting sustainable alternative. Derived from renewable resources like plant-based materials, it offers a lower environmental footprint while maintaining many of the desirable properties of traditional nylon. This eco-friendly option is making waves in sustainable textiles, packaging, and even automotive parts. However, bio-based nylon production is still evolving, and widespread availability might take some time.

Nylon Granuales
Nylon Granuales

How Is the Quality of Nylon Determined?

Determining nylon quality isn’t a one-size-fits-all approach. Instead, manufacturers use a multi-pronged attack with various tests. They examine the nylon’s mechanical properties under different stresses, including how it handles heat and repeated strain. Electrical properties are measured for specific applications. Physically, the nylon is inspected for consistency and checked for how well it resists chemicals it might encounter in use. Finally, they assess how well the nylon maintains its size and shape under varying conditions. By analyzing this data, manufacturers ensure the nylon meets the specific demands of its intended purpose.

Factors for Selection

Choosing the right nylon variant depends on a three-pronged approach:

  • Performance: Consider the mechanical properties, chemical resistance, and thermal stability required for your application.
  • Cost: Balancing performance with cost-effectiveness is key.
  • Application: The specific needs of your project will dictate the most suitable nylon type.

Can Nylon be Injection Molded?

Nylon is a champion of injection molding for a reason. It melts smoothly due to its good flow properties and low melt viscosity, filling molds with ease. The resulting parts are tough and long-lasting, ideal for applications requiring strength and wear resistance. But nylon isn’t without its quirks. Since it absorbs moisture from the air, proper drying is essential before molding to avoid impacting the final product. Additionally, the high temperatures required for melting necessitate specialized injection molding equipment. Despite these considerations, nylon’s overall strengths and diverse variants make it a popular and reliable choice for creating injection molded parts across many industries.

PropertyAdvantage for Injection MoldingDisadvantage/Consideration
Flow PropertiesGood flow at high temperatures, fills mold cavity easily
Strength & DurabilityMolded parts are strong and wear-resistant
VersatilityDifferent nylon types offer a range of properties for specific applications
Moisture AbsorptionYes, can absorb moisture from the environmentRequires proper drying before molding to avoid affecting final properties
Processing TemperatureHigh melting temperatureRequires specialized injection molding equipment
Injection Molding Process
Injection Molding Process

Best Types for Injection Molding

While many can be molded, some offer distinct advantages. Nylons 6 and 6,6 are particularly favored due to their excellent flow properties, allowing them to fill molds with ease. These nylons also solidify into strong and durable parts. For applications requiring high-heat resistance, Nylon 4,6 becomes a strong candidate. Ultimately, the “best” type of nylon depends on the specific needs of the project. Factors like chemical resistance, dimensional stability, and cost will influence the final selection process.

Parting Thoughts

At MISUMI USA, we offer a wide selection of configurable and standard nylon components tailored to meet the needs of modern industrial manufacturing. Whether you require nylon bushings, spacers, or other machine parts, MISUMI’s extensive catalog provides high-quality solutions designed for precision and performance. Explore our range of industrial nylon parts and discover how our customizable options can streamline your production processes. Contact us today to learn more or request a quote, and experience why MISUMI is a trusted partner for engineers and manufacturers worldwide.