Author: Scott Bredemann
Updated: 04/29/2024
Teflon© is a brand name for a synthetic material scientifically known as polytetrafluoroethylene (PTFE). This mouthful of a term refers to the complex chemical structure that grants Teflon its unique properties.
What is Teflon?
At its core, PTFE is a fluoropolymer, meaning its backbone is made of carbon atoms strung together, with fluorine atoms attached to each carbon. This unique arrangement creates a remarkably slick and non-stick surface.

History of Teflon
Teflon’s journey began in the late 1930s when Dr. Roy Plunkett, a chemist at DuPont, stumbled upon it accidentally while researching refrigerants. In 1938, Plunkett discovered that a gas called tetrafluoroethylene had polymerized into a waxy white substance inside a pressurized container. This serendipitous discovery laid the foundation for what would become Teflon.
In 1945, DuPont patented PTFE under the name Teflon, derived from its remarkable non-stick properties. Initially used in military applications during World War II, Teflon soon found its way into various civilian uses, from cookware to industrial machinery, revolutionizing countless industries along the way.
Applications of Teflon
- Industrial Machinery: Bearings and bushings benefit from Teflon’s low friction properties, reducing wear and improving efficiency in machinery.
- Seals and Gaskets: Teflon’s chemical resistance and durability make it ideal for sealing applications in automotive, aerospace, and manufacturing industries.
- Electrical Components: Teflon’s electrical insulation properties make it suitable for coating wires, cables, and connectors in electronics and telecommunications.
- Conveyor Belts: Teflon coatings on conveyor belts reduce friction, improve material flow, and increase belt longevity in manufacturing and food processing industries.
- Medical Devices: Teflon is used in medical implants, catheters, and surgical instruments due to its biocompatibility and chemical inertness.
- Cookware: Teflon coatings on pots, pans, and bakeware provide non-stick surfaces, making cooking and cleaning easier.
- Automotive Parts: Teflon coatings on engine components reduce friction, improve fuel efficiency, and enhance durability in automotive applications.
- Aerospace Components: Teflon coatings on aircraft parts provide corrosion resistance, reduce ice formation, and improve aerodynamics.

Types of Teflon
- Fine Powder PTFE: Fine powder PTFE is commonly used as a lubricant additive in greases, oils, and other lubricants to reduce friction and wear. Its versatile applications in various industries make it the most common type of PTFE.
- Granular PTFE: Granular PTFE is widely utilized as a raw material for manufacturing various PTFE products such as rods, tubes, and sheets. Its versatility and ease of processing contribute to its common usage in the industry.
- Film PTFE: Film PTFE is frequently employed as a non-stick surface covering for cookware, heat sealing membranes, release liners, and electrical insulation tapes. Its widespread use in consumer and industrial applications makes it a common type of PTFE.
- Micro Powder PTFE: Micro powder PTFE is commonly used as a lubricant additive, filler, or surface modifier in various applications to improve wear resistance, reduce friction, and enhance surface properties. Its specialized applications make it less common compared to fine powder PTFE.
- Dispersion PTFE: Dispersion PTFE, while versatile, is less common than other forms of PTFE. It is often used as a coating or impregnating agent for fabrics, papers, and various substrates, as well as in formulations for paints, coatings, and lubricants.
- Expanded PTFE (ePTFE): Expanded PTFE, though highly specialized and valuable in certain applications, is the least common type of PTFE. It is primarily used in gasketing applications for sealing fluids and gases in demanding environments due to its unique porous structure and properties.
- Filled PTFE: Filled PTFE consists of PTFE resin blended with fillers such as glass fibers, carbon, bronze, or graphite. These fillers enhance specific properties of PTFE, such as wear resistance, thermal conductivity, or dimensional stability. Filled PTFE is commonly used in applications where improved mechanical properties are required.
- Modified PTFE: Modified PTFE refers to PTFE formulations that undergo chemical modifications to improve certain characteristics such as adhesion, surface roughness, or thermal stability for specific applications. Modified PTFE variants are engineered to meet the requirements of specialized industries like aerospace, automotive, and electronics.
Mechanical Properties
Teflon, also known as PTFE, boasts impressive properties that make it a versatile material for various applications. Here’s a quick look at some of its key mechanical characteristics:
This table provides a snapshot of the typical values for each property. Remember that specific properties may vary depending on the type of Teflon and its processing methods.
| Property | Value | Units |
| Tensile Strength | 6.90 – 23.00 | MPa |
| Elongation at Break | 300 – 550 | % |
| Flexural Modulus | 0.5 – 1.0 | GPa |
| Compressive Strength | 10 – 20 | MPa |
| Impact Strength | 2.5 – 5.0 | J/m |
| Hardness (Shore D) | 55 – 60 | Shore D |
| Coefficient of Friction (Static) | 0.04 – 0.08 | – |
| Coefficient of Friction (Dynamic) | 0.02 – 0.06 | – |
| Density | 2.10 – 2.30 | g/cm³ |
Electrical Properties
Teflon’s exceptional electrical properties make it a valuable material for applications requiring insulation and low conductivity. Here’s a table outlining some key characteristics:
| Property | Value | Units |
| Volume Resistivity | 1.0 x 10^16 – 1.0 x 10^18 | Ω⋅cm |
| Surface Resistivity | 1.0 x 10^18 – 1.0 x 10^19 | Ω |
| Dielectric Constant | 2.0 – 2.1 | – |
| Dielectric Strength | 30 – 60 | kV/mm |
| Arc Resistance | 165 | Seconds |
Advantages
- Non-Stick: Teflon’s most well-known property is its exceptional non-stick characteristic. This makes it ideal for applications where materials need to flow freely without sticking, reducing friction and cleaning requirements.
- Low Friction: Closely linked to its non-stick nature, Teflon offers a very low coefficient of friction. This translates to smooth movement of parts, reduced wear and tear, and improved machine efficiency.
- Chemical Resistance: Teflon exhibits exceptional resistance to a wide range of chemicals. This makes it suitable for use in harsh environments where exposure to corrosive materials is a concern.
- Heat Resistant: Teflon boasts a high melting point and can withstand a wide range of temperatures, from very low to moderately high. This allows it to function effectively in applications with significant temperature fluctuations.
- Electrical Insulation: Teflon is an excellent electrical insulator due to its high dielectric strength and volume resistivity. This makes it valuable for applications requiring electrical components to be protected from current leakage.
- Water and Weather Resistant: Teflon is hydrophobic, meaning it repels water. Additionally, it is resistant to UV rays, oxidation, and other environmental factors. This ensures its durability and functionality in various conditions.
Disadvantages
- Limited Temperature Range for High-Heat Applications: While Teflon offers good heat resistance, it can’t handle extremely high temperatures. At temperatures exceeding its limit (around 327°C or 621°F), Teflon can begin to degrade and release harmful fumes.
- Susceptibility to Scratches and Wear: Though known for its non-stick properties, Teflon can be scratched or abraded, especially with forceful use or contact with sharp objects. This can damage the non-stick surface and potentially impact performance.
- Cost Factor: Compared to some other materials, Teflon can be more expensive. This can be a deciding factor depending on the application and budget constraints.
- Off-Gassing Potential: At very high temperatures exceeding its recommended limits, Teflon can off-gas harmful fumes. Proper ventilation is crucial to avoid inhaling these fumes.
- Limited Strength: While suitable for many applications, Teflon is not known for its high strength or rigidity. This might limit its use in situations requiring high load-bearing components.
Is Teflon Biodegradable?
Teflon products take hundreds or even thousands of years to break down in landfills, contributing significantly to plastic waste. Furthermore, the historical use of PFOA, a harmful chemical, in some Teflon manufacturing processes raises environmental and health risks. The potential release of microplastics from Teflon wear and tear adds another layer of concern.
However, there are reasons for optimism. Major manufacturers have phased out PFOA usage, and research is ongoing to develop eco-friendly manufacturing methods for Teflon. Additionally, efforts to create recycling techniques for Teflon waste offer a promising step towards a more sustainable future for this material. While the environmental impact of Teflon requires careful consideration, advancements are being made to address these concerns.
Summary
Explore the possibilities of Teflon/PTFE for your manufacturing needs – visit us.misumi-ec.com to discover a wide range of Teflon parts and components tailored to your specifications. With MISUMI USA’s vast selection and customizable options, you can find the perfect Teflon solution for your application. Experience the quality, reliability, and performance of Teflon/PTFE products at us.misumi-ec.com today!