Author: Scott Bredemann
Updated: 03/05/2025 | Read Time: 4mins
TIG welding, or Tungsten Inert Gas welding, is renowned for producing clean, precise, and high-quality welds. This makes it the method of choice in industries where both strength and appearance are critical—such as aerospace, automotive, and medical equipment manufacturing. What sets TIG welding apart is its ability to weld a wide range of metals, including aluminum, stainless steel, and copper alloys, with minimal spatter and distortion.
In this guide, we’ll cover everything you need to know about TIG welding, from the basic process to the equipment required. We’ll also dive into the advantages and disadvantages of TIG welding, comparing it to other common methods like MIG and stick welding.
What is TIG Welding?
TIG welding (Tungsten Inert Gas welding), is a welding method that uses a non-consumable tungsten electrode to create the weld. The process involves generating an arc between the tungsten electrode and the workpiece, which is shielded by an inert gas, typically argon or helium. This shielding gas prevents contamination from the air, ensuring that the weld is clean and strong.
One of the key advantages of TIG welding is the control it offers. The welder manually feeds filler metal into the weld pool, allowing for greater precision and flexibility, especially on thinner materials. This makes it ideal for applications where high-quality, aesthetically pleasing welds are required, such as in aerospace, medical device manufacturing, and even fine art metalworking.
TIG welding is also known for its ability to weld a variety of metals, including steel, aluminum, and titanium. The process can be used on both thin and thick materials, but it excels in producing strong, clean welds on thinner gauges. However, it does require skill and experience from the welder, as the process involves precise control of heat, filler material, and arc length. While TIG welding tends to be slower compared to other methods like MIG or stick welding, the results are often worth the extra time and effort, providing welds that are both visually appealing and structurally sound.

Equipment need for TIG Welding
- TIG Welder Machine: The core of TIG welding, available in AC (for aluminum) and DC (for steel) models. It controls amperage to suit different materials and thicknesses.
- Tungsten Electrode: A non-consumable electrode with a high melting point that creates the welding arc. Options like pure, thoriated, and ceriated tungsten are used for different materials.
- Filler Rods: Used to add material to the weld pool, with rods specific to the material being welded (e.g., stainless steel for stainless steel, aluminum for aluminum).
- Shielding Gas: Typically argon or a mix of argon and helium, it protects the weld from atmospheric contamination. Proper gas flow is essential for a clean weld.
- Welding Torch: Holds the tungsten electrode and directs the shielding gas. Air-cooled torches are common for lighter work, while water-cooled torches are used for heavier-duty welding.
- Personal Protective Equipment (PPE): Includes a welding helmet, heat-resistant gloves, flame-resistant clothing, and a welding jacket to protect from UV radiation and burns.
- Work Surface and Clamps: A stable, clean work surface and clamps are needed to hold materials in place, ensuring consistent and precise welds.
How to TIG Weld
- Prepare the Workpiece: Start by cleaning the metal to remove any dirt, grease, or oxidation. Use a wire brush or grinder to ensure a clean surface, as contaminants can weaken the weld.
- Set Up the Welder: Choose the appropriate settings on your TIG welder. Adjust the amperage based on the material and thickness. Select AC or DC depending on whether you’re welding aluminum or steel.
- Insert the Tungsten Electrode: Attach the tungsten electrode to the torch. Make sure it’s properly sharpened to a point for a stable arc.
- Choose Your Filler Rod: Select the correct filler rod based on the material being welded. Make sure the rod is clean and free of contaminants.
- Set Up Shielding Gas: Connect the gas line to the welder and set the flow rate. Argon is most commonly used, but if you’re welding aluminum, you may want to mix in some helium for better heat control.
- Strike the Arc: Hold the torch at a slight angle, about 15 to 20 degrees, and initiate the arc. You can start the arc by either scratching the tungsten electrode on the metal or using a high-frequency start, depending on your machine.
- Control the Weld Pool: Once the arc is established, move the torch steadily along the seam. Add filler rod as needed by dipping it into the weld pool. Maintain a consistent speed to avoid undercutting or excessive heat.
- Finish the Weld: Once you’ve completed the seam, slowly pull the torch away to let the weld cool. Allow the weld to solidify before touching it, ensuring a clean finish.
Pro Tip: Practice your hand control by running short test beads. This helps you get a feel for the right speed and torch angle, which is crucial for producing smooth, consistent welds.
Comparison to Other Welding Methods
| Feature | TIG Welding (Tungsten Inert Gas) | MIG Welding (Metal Inert Gas) | Stick Welding (Shielded Metal Arc Welding) |
|---|---|---|---|
| Precision | High precision and clean welds | Less precise, more spatter | Least precise, with more spatter and slag |
| Materials | Works on steel, aluminum, stainless steel, titanium | Works on steel, aluminum, and some alloys | Works on steel, iron, and other ferrous metals |
| Welding Speed | Slower, as it requires more control | Faster, continuous feed of wire | Moderate, with some speed variations depending on material |
| Ease of Use | Requires skill and experience | Easier for beginners | Easy to use, good for outdoor applications |
| Weld Quality | High-quality, smooth, aesthetically pleasing | Moderate quality, more post-weld cleanup | Strong welds but rougher finish, often requiring cleanup |
| Portability | Medium (requires gas tanks and cooler for water-cooled torches) | High (portable machines and easy to set up) | High (simple equipment, no gas needed) |
| Cost | High initial cost for equipment | Moderate cost for equipment | Low initial cost for equipment |
| Applications | Precision work like aerospace, medical devices, art | General fabrication, automotive, and construction | Heavy-duty outdoor work, pipelines, and structural welding |
| Weld Strength | High strength, minimal distortion | Moderate strength, more prone to distortion | Strong welds, good for thick materials but less clean finish |
Each welding method has its strengths, and the choice depends on the project needs, material, and desired outcome. TIG welding offers the highest precision, while MIG and stick welding are generally faster and easier for large-scale projects.

Top 3 Applications in Industrial Manufacturing
Aerospace Manufacturing
It is the top pick for aerospace applications due to its precision and ability to create strong, lightweight welds on high-performance materials like titanium and aluminum. Aircraft parts, such as fuselages and engine components, require exceptional weld quality to ensure safety and durability under extreme conditions.
Medical Device Production
In the medical field, it is used to fabricate critical components such as surgical tools, implants, and prosthetics. Stainless steel, a material often used in medical devices, requires a clean, strong weld to meet strict hygiene and performance standards.
Automotive Manufacturing
It is used in automotive manufacturing for applications that demand both strength and appearance, such as exhaust systems, roll cages, and custom parts. The ability to weld thin metals without warping or burning through is particularly valuable in high-performance cars,. TIG welding also helps in creating aesthetically pleasing welds, which is important for parts that are visible or exposed.
Parting Thoughts
We hope you found this article informative and valuable as you continue to expand your TIG welding knowledge. At MISUMI USA, we are committed to providing you with resources to support your business and projects. Be sure to explore our other articles for more insights into the manufacturing world. Additionally, take a look at MISUMI USA’s extensive online catalog of standard and configurable parts designed to meet your welding needs. Examples include:
If you have any questions about TIG welding or other industrial manufacturing needs, don’t hesitate to reach out to our product experts for assistance.