How to Select the Right Bearing Pt 6

Bearing Lubrication

This post is a continuation of the Koyo Bearings series, you can find the original post on their website here.

In Part 5, we explained about the preload and rigidity of a bearing.

To catch up on the previous Bearing Selection blog posts, read each one below:

How to Select the Right Bearing Part 1: The Order of Priority for Selecting Bearings and the Types of Bearings

How to Select the Right Bearing Part 2: Selecting Bearing Arrangement

How to Select the Right Bearing Part 3: Bearing Dimensions and Service Life

How to Select the Right Bearing Part 4: Bearing limiting speed, running accuracy, and fits

How to Select the Right Bearing Part 5: Bearing Preload and Rigidity

In Part 6, we will explain about bearing lubrication as a measure for whether the bearing type you chose was appropriate. The surfaces of bearing rolling elements and rings (inner ring and outer ring) are finished extremely smooth. But however smooth they are their surfaces still have unevenness.

When a bearing rotates, the convex regions of the bearing rings and the rolling elements come in contact with each other. This contact between the convex regions leads to friction and wear, inhibiting the smooth rotation of the bearing. (See Figure 1.)

Fig. 1: Contact between a bearing ring and a rolling element (with no lubricant)

In order to prevent this friction and wear, oil or some other substance is applied between the contact regions. This is called “lubrication.” With the appropriate lubrication, an oil film makes it so that the rolling elements and bearing rings do not come in direct contact. This results in less friction and a massive decrease in wear. (See Figure 2.)

Fig. 2: No contact between a bearing ring and a rolling element (with lubrication)

For stable and smooth rotation of the bearing, it is necessary to reduce the friction caused by the rolling motion and prevent the wear of the bearing components. “Lubrication” plays a major role in this process.

Table 1: Bearing selection checklist

Below is an explanation of the lubricating methods used to allow the bearing to rotate stably over a long period of time.

  • Purpose of lubrication
  • Types of lubrication
  • Features of grease lubrication
  • Features of oil lubrication

1. Purpose of lubrication

The primary purpose of lubrication is to reduce friction and wear, but there are also other reasons for lubrication (see Table 2).

Table 2: Purposes of lubrication

This lubrication brings about various positive effects for the bearing.

2. Types of lubrication

The major types of bearing lubrication are grease lubrication, which uses semi-solid (i.e., like cream) grease; and oil lubrication, which uses lubricating oil.

Because grease is semi-solid, it tends not to leak out and can be easily affixed to the inside of the bearing. Since this makes it convenient as a sealing device, grease lubrication is widely applied for bearings.

On the other hand, oil lubrication is more effective as a lubricant than grease lubrication, and so is used in situations where such factors as high-speed rotation, a large cooling effect, or dirt filtering are required (see Table 3).

Table 3: Comparison between grease and oil lubrication

3. Grease lubrication

1) What is grease?

The main components of grease are base oil (lubricating oil), thickeners, and additives, and the components and amounts of these are adjusted and blended according to the purpose of use (see Table 4).

Table 4: The components of grease and their roles

The lubricating oil used for the base oil is explained in “4. Oil lubrication” further down this column.

The thickener disperses throughout the base oil (lubricating oil) and makes it semi-solid, preventing the base oil from spilling out.
The additives complement the performance needed for the purpose of use.
With grease lubrication, when the bearing rotates the base oil gradually oozes out and lubricates the bearing.

2) How to select the right grease

We should select the appropriate grease with the characteristics needed for the purpose of use (see Table 5).

Table 5: Examples of characteristics of grease

Engineer’s Note: Greases of different brands should not be mixed. The grease’s characteristics may change and cause damage to the bearing.

3) Grease lubrication method

As the primary methods of grease lubrication, allow us now to look at grease-packed bearings (wherein grease is filled inside the bearing in advance) and the feeding method.

a) Grease-packed bearings

Grease-packed bearings are bearings that are sealed by the bearing manufacturer using a shield or seal after inserting the necessary grease into the inside of the bearing (see Figure 3).

Fig. 3: Grease-packed bearings with seals

b) The grease feeding method

After mounting a non-greased bearing into the machine, grease is filled onto the bearing (see Figure 2). Grease supplied through the grease nipple is filled into the grease sector inside the housing, flowing into the inside of the bearing. Used grease is pumped out of the bearing and ejected out of the housing by the centrifugal force of the rotary disc attached to the grease valve.

Fig. 4: An example of the grease feeding method

The grease feeding interval can be determined by the type, size, and rotation speed of the bearing.

4. Oil lubrication

1) What is lubricating oil?

Generally, mineral oil–which is a refined crude oil and suitable for lubrication–is used as lubricating oil.
However, mineral oil has the disadvantages that it oxidizes at high temperatures and its lubricating function deteriorates, and that at low temperatures its viscosity increases and the force required to stir the lubricating oil (the “stirring resistance”) increases.
For this reason, we use synthetic oil that has excellent lubricating function in high temperature or low temperature (see Table 6).
Additives are added to the lubricating oil to improve certain characteristics (preventing oxidation, rust, foam, and so on).

Table 6: Characteristics of the various types of lubricating oil

2) How to select the right lubricating oil

Select the lubricating oil with the appropriate viscosity for the operating temperature of the bearing. First we select the lubricating oil with the proper kinematic viscosity for the type of bearing (see Table 7).

Table 7: Proper kinematic viscosity by bearing type

Next we select the proper kinematic viscosity for the bearing operating condition (see Table 8).

Table 8: Proper kinematic viscosity by bearing operating conditions

Lubricating oil with low kinematic viscosity is smooth, the lubricating oil having little resistance. It is used in bearings that rotate at high speed. However, if the kinematic viscosity is too low, there will be insufficient formation of the lubricating oil film, and the lubricating effectiveness will be decreased.

On the other hand, lubricating oil with high kinematic viscosity is thick, the lubricating oil film being strong. It is used in bearings to which a heavy load is applied. However, if the kinematic viscosity is too high, the viscosity resistance of the lubricating oil will cause a large amount of heat to be generated.

The kinematic viscosity of lubricating oil changes depending on the temperature (see Figure 6). For this reason, consider the temperature during operation when you select the lubricating oil.

Fig. 6: The relationship between oil viscosity and temperature

3) Oil lubrication method

In order to select the most appropriate lubricating method from among the many methods of oil lubrication, consider the operating condition, usage criteria, and cost.
Allow us to explain the four most common methods of oil lubrication.

a) Oil bath

This is a method of operating the machine by immersing the bearing in lubricating oil. It is suitable for low- to medium-speed rotation.

Fig. 7: Oil bath

b) Oil drip

Lubricating oil is dripped from the oiling device and the effect of the rotating part causes the lubricating oil to mist and fill the housing. This has a cooling effect. This method can be applied at relatively high speeds and mid-level loads.

Fig. 8: Oil drip

c) Oil splash

This is a method in which gears, etc. are attached to the shaft, the lubricating oil is splashed, and it is made into droplets for oil supply. This method can be applied at relatively high speeds.

Fig. 9: Oil splash

d) Forced oil circulation

This is a lubrication method in which the lubricating oil is inserted inside the bearing, then cooled, and then circulated again. It is most commonly applied in high-speed rotation or high-temperature conditions.

Fig. 10 Forced oil circulation

Conclusion

Bearings aim for stable and smooth rotation, and to do that the friction with rolling motion needs to be reduced and the abrasion of the various components needs to be prevented. “Lubrication” plays a major role in this process. It is important to choose the appropriate lubricant and lubricating method in order to allow the bearing to rotate stably over a long period of time.

  1. The major types of bearing lubrication are grease lubrication, which uses semi-solid (i.e., like cream) grease; and oil lubrication, which uses lubricating oil.
  2. Most bearings use grease lubrication, which is convenient as a sealing device.
  3. For situations where such factors as high-speed rotation, a large cooling effect, or waste filtering are required, oil lubrication is used.
  4. In order to select the most appropriate lubricant (grease or lubricating oil) and lubricating method, consider the operating condition, usage criteria, and cost.

Explore the MISUMI collection of Koyo Bearings here.

Works Cited

Koyo Bearings. (2020, July 30). Bearing Trivia. Retrieved from Koyo Bearings: https://koyo.jtekt.co.jp/en/2020/07/column02-06.html

Share this Story
Load More Related Articles
Load More By Carlicia Layosa
Load More In Mechanical Design

Leave a Reply

Your email address will not be published. Required fields are marked *

*

Check Also

Consumer Product Packaging Part 2: Filling

To catch up on part 1 of our ...

Subscribe to the Mech Lab!

Like us on Facebook

Follow us on Twitter @usa_misumi

Subscribe to our Channel