Author: Scott Bredemann
Updated: 04/15/2024
Polystyrene is a versatile and widely used material in the manufacturing industry, known for its lightweight, durable, and cost-effective nature. Whether you’re designing packaging, insulation, or custom components, polystyrene plays a crucial role in delivering high-quality products across various sectors. In this article, we’ll explore what polystyrene is, its key features, the production process, and its diverse applications in manufacturing.
What is Polystyrene?
Polystyrene is a lightweight plastic polymer commonly abbreviated as PS. It’s characterized by its rigid structure and excellent insulation properties, making it a popular choice in manufacturing. This polymer is derived from styrene, a clear liquid hydrocarbon obtained from petroleum.
Polystyrene exists in various forms, including expanded polystyrene (EPS) and extruded polystyrene (XPS), each tailored for specific applications. Its chemical composition and molecular structure contribute to its durability and versatility, allowing for easy shaping and molding into different products.
Production Process of Polystyrene
The production of polystyrene involves several stages, starting from the polymerization of styrene monomer to the formation of the final products. Raw materials such as styrene monomer are polymerized to create the polymer chains characteristic of polystyrene. These chains are then processed into sheets, foams, and other forms using specialized manufacturing techniques.

Polystyrene Uses in Manufacturing
Several features make polystyrene a popular choice in manufacturing. It offers a high strength-to-weight ratio, ideal for applications where weight reduction is crucial. This light weight also translates to reduced transportation costs. Polystyrene’s low thermal conductivity makes it a great insulator, optimizing temperature control in packaging and construction. The material can be easily molded and shaped into various forms, catering to diverse manufacturing needs, allowing for the creation of a wide range of products. Additionally, polystyrene exhibits resistance to moisture and some chemicals, ensuring product protection during storage and transport.
| Industry | Application | Properties Used |
| Packaging | Protective packaging (packing peanuts, trays) | Lightweight, shock-absorbing, moisture resistant |
| Construction | Insulation boards | Thermal insulation, moisture resistance (XPS) |
| Automotive | Car parts (dashboards, interior components) | Lightweight, moldable |
| Consumer Products | Electronics packaging, disposable cups, toys | Cost-effective, moldable, clarity (for some applications) |
| Medical & Laboratory Equipment | Sterilized devices, laboratory equipment | Sterility, clarity |
| Injection Molding | Mass-produced plastic parts | Moldable, cost-effective (compared to other materials for injection molding) |
Advantages of Polystyrene in Manufacturing
One of the key advantages of polystyrene in manufacturing is its cost-effectiveness, making it a viable option for mass production. Its lightweight nature also contributes to reduced transportation costs, further enhancing its appeal to manufacturers. Moreover, polystyrene offers ample opportunities for customization to meet specific requirements.
| Advantage | Description | Benefit |
| Cost-effectiveness | Polystyrene is a relatively inexpensive material. | Lowers production costs for manufacturers. |
| Lightweight | Polystyrene has a high strength-to-weight ratio. | Reduces transportation costs and makes products easier to handle. |
| Versatility | Polystyrene can be easily molded and shaped into various forms. | Allows for the creation of a wide range of products with diverse designs. |
| Thermal Insulation | Polystyrene has low thermal conductivity. | Improves temperature control in packaging and construction, leading to energy efficiency. |
| Moisture Resistance | Polystyrene exhibits resistance to moisture. | Protects products from water damage during storage and transport. |
| Chemical Resistance (Limited) | Polystyrene resists some chemicals. | Protects products from certain chemical interactions. |
| Moldability in Injection Molding | Polystyrene serves as a cost-effective feedstock for injection molding. | Enables mass production of complex plastic parts at a lower cost compared to some materials. |
| Clarity (Some grades) | Certain types of polystyrene offer good clarity. | Makes them suitable for applications requiring product visibility, such as medical equipment packaging. |
Polystyrene in Injection Molding
One of the primary methods of utilizing polystyrene in manufacturing is through injection molding. This process involves melting polystyrene pellets and injecting the molten material into a mold cavity under high pressure. Once cooled and solidified, the mold is opened to reveal the final product. Injection molding offers numerous advantages for polystyrene applications, including high production efficiency, intricate design capabilities, and cost-effectiveness for large-scale production runs. It’s commonly employed in producing a wide range of items, including packaging components, household appliances, automotive parts, and medical devices. The versatility and reliability of polystyrene in injection molding make it a go-to choice for manufacturers seeking efficient and precise fabrication of complex components.
Polystyrene vs Polypropylene
Polystyrene often finds itself compared to another versatile plastic, polypropylene (PP). While both offer advantages, key differences exist. Polypropylene boasts superior strength and heat resistance, making it ideal for applications like reusable containers and automotive parts that endure high temperatures. Polystyrene, on the other hand, excels in lightweight applications and cost-effectiveness. It’s the go-to for disposable items and insulation needs. Additionally, polystyrene offers superior clarity, a factor valued in medical equipment and packaging requiring product visibility. When choosing between these two materials, the specific application and desired properties take center stage.
| Feature | Polystyrene (PS) | Polypropylene (PP) |
| Chemical Structure | Aromatic | Aliphatic |
| Strength | Lower | Higher |
| Heat Resistance | Lower melting point, less suitable for high temperatures | Higher melting point, suitable for high temperatures |
| Weight | Lightweight | Lightweight |
| Moisture Resistance | Moderately resistant | Highly resistant |
| Chemical Resistance | Resistant to some chemicals | Resistant to a wider range of chemicals |
| Cost | Generally less expensive | Can be slightly more expensive |
Polystyrene vs Styrofoam
The terms “polystyrene” and “Styrofoam” are often used interchangeably, leading to some confusion. While closely related, they’re not the same. Polystyrene is the broader term, encompassing a variety of plastic with specific chemical structures. Expanded polystyrene (EPS) is one type of polystyrene, and “Styrofoam” is actually a trademarked brand name specifically referring to a form of EPS produced by The Dow Chemical Company. This trademarked EPS is known for its blue tint and is commonly used in building insulation boards. So, all Styrofoam is a type of EPS (polystyrene), but not all polystyrene is Styrofoam.
Conclusion
For all your configurable industrial manufacturing needs, including products made from polystyrene and a variety of other materials, visit MISUMI USA. Explore our wide selection of customizable components designed to meet your specific project requirements. Also, be sure to check out more articles from our blog for helpful support in your manufacturing journey!