Q & A: Single & Double Type Stroke Bushings

Published on
October 8, 2014

1 min read

Question:

Dear MISUMI Engineering Team,

What is the difference in the single and double type? Why is the “Maximum Stroke” so much different between the two types?

Thank you,

Eric

Answer:

Hello Eric,

I assume you are referring to Stroke bushings. Typically our linear bushings are designed with a return mechanism, where balls recirculate back into the system which allows limitless stroke.

Single and double
MISUMI Linear Ball Bushings

The advantage of using double bushings is having more ball bearings (double amount) in contact with shaft. This allows for great improvement of static and dynamic load, drastically increases your moment load ratings and system’s stability.

The construction of a Stroke Bushing is very different.

There is no ball return mechanism. The balls are embedded into a sleeve and they roll on the shaft’s outside diameter and the housing’s inside diameter while the sleeve is suspended between the two, providing solid lubrication to the ball bearing .

Sleeve
Strocke Bushing sleeve structure

So if the shaft is stationary, while moving the housing, the sleeve with bearing balls will also move, but at different (slower) rate in relation to the shaft, but the sleeve’s travel  will be limited by surface length of the housing’s Inside Diameter.

Please, see the single and double Stroke Bushings:

single and double large
Single/Double visual Stroke explanation

Again, by having double amount of ball bearings  you will still benefit from better load ratings, but it will limit your stroke. I hope I answered your questions, but feel free to comment below or contact us at engineering@misumiusa.com with any additional questions!

Thank you,

Chris Blaszcyk

Product Development Manager
Standard Mechanical Components Team

About the Author

Carlicia Layosa

Carlicia is the Marketing Automation Manager at MISUMI. She holds a bachelor's degree in Mechanical Engineering and a master's degree in Energy Engineering from the University of Illinois at Chicago. She is a Certified SOLIDWORKS Associate, Marketo Certified Expert, and is passionate about education and training.

You may also like these