Continuing with our warning lights series, we will discuss tips for selecting the right one for your application. Be sure to read the selection tips for stack lights here.
Differences Between Rotating Warning Lights and Stack Lights
First, what is the difference between rotating warning lights and stack lights? In a production setting, rotating lights and stacked signal lights are typically used for different purposes.
Rotating warning lights are often used to indicate that a particular machine or area is temporarily out of service, or that a potentially hazardous situation is present. For example, if a machine needs maintenance or repair, a rotating light may be used to signal that the area should be avoided until the issue is resolved.
Stack lights are often used to show the status of a particular machine or process. For example, a green light may indicate that a machine is running smoothly, while a red light may indicate that there is a problem that needs to be addressed.
Stack lights are often used to show the status of a particular machine or process. For example, a green light may indicate that a machine is running smoothly, while a red light may indicate that there is a problem that needs to be addressed.
Choosing the Right Rotating Light
Then, how to choose the right rotating light? When choosing a rotating light, it is important to consider the following factors:
1 – Color
Rotating warning lights come in various colors such as red, yellow, green, blue, etc. It is important to choose the appropriate color depending on the purpose. For example, red is suitable for warning signals, yellow for caution, and green for indicating work in progress.
2 – Flashing Pattern
The flashing pattern of the rotating light is important for drawing attention to it. If there are different flashing patterns available, it is recommended to choose one that can attract more attention.
3 – Light Source
Whether the Light Source is LED or light bulbs has a significant impact on short- or long-term costs. In general, LEDs tend to be more expensive, but their long life means fewer replacements and less time spent replacing them.
4 – Buzzer
Some rotating warning lights have a buzzer. It helps to communicate an abnormality or warning to the surroundings more quickly.
5 – Size
The size of the rotating light should be chosen to suit the location where it will be installed. In particular, for narrow spaces, it is important to choose a compact product.
Considering these factors, it is important to choose the right rotating light that suits your purpose. MISUMI offers a vast selection of rotating warning lights, including Patlite with many products in stock. Explore them all here.