From the wheels on a skateboard to the fan in your fridge, there are a variety of environments where bearings are used in our daily lives. But what about when your application requires much more resilience due to extreme conditions?
Here’s what to consider when selecting a bearing to be used in harsh environments.
Corrosion and Contaminants
Bearings are able to spin smoothly due to using round balls or rollers that have a small area of contact with the inner and outer rings, which greatly reduces friction. Applications such as mining or machining can have contaminants that are able to fall into the track and are likely to not only create more friction but also damage the bearing.
The best way to protect your bearings in an environment that could have dust, debris, metal chips, and more is to add shields or seals to block particles from getting inside. If your application requires higher operating speeds and you still need to have some protection against contaminants, using shielded bearings will accomplish what you need but will not protect against any liquids.
If you need a high level of protection from all contaminants, liquids included, seals will be the better option and bring the added benefit of less maintenance due to holding lubrication better.
When water or corrosive chemicals are involved, stainless steel bearings with seals or full ceramic bearings are the best option to prevent any rusting or corrosion from occurring. Stainless steel bearings are capable of withstanding heavy loads and are easy to maintain, while ceramic bearings have a higher tolerance against corrosion and temperature.
Temperature Range and Lubrication
Depending on the temperature of the environment, caused by the weather or the application itself, key items to consider would be thermal expansion and lubrication.
Thermal expansion can cause a variety of issues, such as higher friction, misalignment, and reduced bearing life. To prevent issues, you could:
- Choose a bearing with greater clearance in anticipation of higher fluctuations in temperature
- Or use similar materials for the shaft or housing
This allows the bearing to expand and contract without binding and have a better fit on shafts or in housings. These benefits do come with the tradeoffs of increased vibration and reduced precision.
Choosing the right lubrication for your environment can prevent lubricant breakdown and increased friction. Grease is widely used because it stays in place and carries different characteristics depending on the base oil and thickening agent but requires more work to clean and reapply.
An example for a high-temperature environment would be to use a mineral oil base with a lithium soap thickener. Oil is easy to apply and has higher heat dissipation, but it leaks easier and requires more sealing.
Vibration and Shock
When dealing with the vibration and shock encountered with construction equipment and heavy-duty machinery, choosing the right bearing for the job will reduce fatigue and stress points that would otherwise occur.
Applications with consistent vibration can reduce the lifespan of a bearing by causing fatigue cracks and pitting on the raceways. Spherical roller bearings, like the TRITAN line offered through MISUMI, are an ideal option that can handle extreme speeds and are self-aligning to better manage chaotic loads caused by vibrations.
If you’re dealing with applications that have high shock loads, you could see premature failures coming from plastic deformation of the raceways. This can cause uneven rotation and increased friction in operation.
A way to combat high shock is to use tapered roller bearings, such as the NTN line offered through MISUMI. Tapered roller bearings are capable of handling heavier radial and thrust loads in applications where durability is required.
For more information on material selection and bearing fits, read “Ball Bearing Materials: Benefits & Shortfalls” and “Rotary Bearing Fits and Tolerances”.
Don’t forget to take a look at the wide range of bearings from brands like TRITAN, NTN, SKF, and more offered by MISUMI.