Industry Insights Warehouse Automation

Warehouse Automation Part 1: Pick-to-Light Systems

Pick-to-Light Systems: How They Work & Benefits | MISUMI

Pick-to-light systems use LED displays and confirm buttons at storage locations to guide operators through paperless order picking, cutting search time and picking errors. As part of our warehouse automation series on the Internet of Things (IoT) era, this guide explains how the technology works and which mechanical components you need to build one.

Pick-to-light display module with alphanumeric readout and confirm button mounted at a storage location
Pick-to-light display. Image: KBS Industrieelektronik GmbH, CC BY-SA.

What Are Pick-to-Light Systems?

Pick-to-light systems are simple but robust order-fulfillment technology designed to streamline picking, improve accuracy, and lower labor costs. They are paperless: alphanumeric displays and buttons are installed at storage locations and guide employees through light-aided manual picking, putting, and sorting of packages or products.

Quick definition: A pick-to-light system lights the exact storage location, shows the quantity to pick, and waits for the operator to press a button to confirm. Nothing is printed, and the operator never has to search for a location.

How Does Pick-to-Light Work?

Here is a step-by-step description of how a typical pick-to-light system operates.

1
Scan the container.

The operator scans the barcode on a temporary or reusable holding container, such as a shipping carton. This links the container to a specific order.

2
Follow the light.

The alphanumeric display, typically LED, lights up to guide the operator to the indicated storage location. The display then shows which item and how many to pick.

3
Pick and confirm.

The operator picks the items, places them in the holding container, and presses the button to confirm the pick.

4
Repeat until complete.

The system illuminates each location in turn until every item on the order has been picked and placed in its holding container.

5
Use optional features.

Depending on the system, the LED display can be paired with an acknowledgment button and a digital readout for more detailed instructions and options.

Pick-to-light system installed on warehouse shelving with lighted displays at each bin
Pick-to-light system installed on shelving. Image: Ingenieria-logistica, CC BY-SA.

Engineering note: The confirm-button press is the data point that makes the system valuable. Each press records which location was picked, how many units, and when, which is what feeds pick-rate reports and inventory updates when the system is linked to a WMS.

Pick-to-Light vs. Put-to-Light

Put-to-light systems are essentially the opposite of pick-to-light: they reverse the flow. Instead of directing an operator to take items from storage to fill an order, a put-to-light system guides the operator to place incoming goods where they belong, whether that is a retail store order, a customer order, or any other organizational grouping.

Pick-to-light
  • Flow: from storage locations into an order container
  • Light shows: where to pick and how many
  • Typical goal: fulfill customer orders accurately
Put-to-light
  • Flow: from incoming goods into order or destination locations
  • Light shows: where to put each item and how many
  • Typical goal: sort and distribute by order, store, or customer

Benefits of Pick-to-Light Systems

Ease of use

Training operators in traditional picking can take hours or more, depending on warehouse size and complexity. With an efficient pick-to-light system, companies can cut training down to 30-45 minutes.

System integration

A pick-to-light system can be installed standalone or integrated with an existing warehouse management system (WMS), enterprise resource planning (ERP), supply chain management, or other host systems. Advanced systems can produce pick-rate reports, analyze productivity, and allow the size of work zones to vary to match labor to order volume.

Increased efficiency

Systems are usually organized by your existing work zones, which minimizes walking. If an order must pass through multiple zones, the system follows the order and reduces idle time. Some systems mount onto mobile carts or conveyor systems so one operator can fulfill an entire order across many zones.

Paperless operation

Operators save time by eliminating traditional paper-based record keeping.

Improved order accuracy

From a customer-service standpoint, the greatest benefit is fewer picking errors, which improves order-fulfillment performance.

Lower labor costs

Picking is one of the biggest expenses in warehouse operations. Less walking, shorter fulfillment time, and greater accuracy combine to reduce labor cost.

Building a pick-to-light station, cart, or shelving line?

Shop Factory Frames Browse Aluminum Extrusion

Pick-to-Light vs. Other Picking Methods

Pick-to-light is one of several ways to direct manual picking. The table below compares the approaches on the factors that most often drive the decision.

MethodOperator guidanceHands and eyesFixed infrastructure at locationsBest fit
Paper pick listPrinted list; operator finds each locationHands busy with paperNoneLow volume, simple layouts
Handheld RF scannerScreen directs and scan verifiesOne hand occupied by scannerBarcode labelsLarge, changing SKU ranges
Voice pickingSpoken instructions through a headsetHands and eyes freeNoneLarge areas, mobile picking
Pick-to-lightLight and display at the exact locationHands free except button pressDisplay and button at each locationHigh-velocity SKUs in defined zones
Put-to-lightLight shows destination for each itemHands free except button pressDisplay and button at each destinationSorting by order, store, or customer
Where pick-to-light excels
  • Short training time for new or seasonal operators
  • Clear visual confirmation at every pick
  • Works well in dense, fast-moving pick zones
  • Expandable as features and volume grow
Where to be careful
  • Hardware is needed at each storage location, so cost scales with location count
  • Layout changes mean moving or reprogramming displays
  • Less economical for slow-moving, very large SKU ranges
  • Display visibility must be checked against ambient lighting

Engineering and Design Considerations

The light modules get the attention, but the structure that carries them determines whether the system stays accurate and serviceable. These are the factors to settle early in design.

Measure what the system is supposed to improve

Track the same metrics before and after installation so the benefit is visible, not assumed.

Pick rate = order lines picked ÷ labor hours
Pick accuracy (%) = (order lines picked correctly ÷ total order lines) × 100
Travel share = time spent walking ÷ total picking time

Zone layout and flow

Since pick-to-light is usually organized by existing work zones, lay out zones so high-velocity items sit together and orders pass through the fewest zones possible. This is what keeps walking, and therefore idle time, low. Where one operator needs to cover many zones, consider mounting the system on a caster-based cart or alongside a conveyor.

Structure and mounting

Frames built from aluminum extrusion make it simple to reposition display brackets as the layout changes, and posts and struts, gussets and angle plates, and machined sheet metal help keep shelving square and rigid. A rigid frame protects display alignment and button feel over repeated cycles.

Visibility and signaling

Confirm that display brightness and viewing angle work for your aisle lighting and the distance operators typically stand from the shelf. Warning and signaling lights and stack lights can add zone-level status, such as order complete or attention needed, on top of the per-location display.

Safety: When pick-to-light stations are built next to conveyors, moving carts, or other automated equipment, guard pinch points and moving parts according to your site’s safety assessment. A MISUMI extrusion protective guard is one way to build guarding into an aluminum frame.

Commonly Used Components for Pick-to-Light Warehouse Automation Systems

The mechanical and electrical hardware around the lights matters as much as the lights themselves. These warehouse automation component categories are commonly used in pick-to-light builds.

Structure and framing

M1503Factory Frames

Primary framework for pick stations, shelving, and carts.

M1501Aluminum Extrusion

Adjustable profiles for racks and display mounting.

M1505Machined Sheet Metals

Brackets and plates, including machined sheet metal plates.

M1506Gussets, Angle Plates, Welded Steel Stands

Reinforcement and support for frames and stands.

M1509Posts and Struts

Vertical and bracing members for shelving structures.

MaterialMetal Materials

Stock material for custom brackets and fixtures.

Material handling and motion

M1113Conveyors

Move containers between zones so orders follow the operator path.

M1105Rollers

Gravity-fed and roller surfaces for carton flow.

M1606Casters

Mobile carts that carry the system through many zones.

M0117Slide Rails

Pull-out drawers and trays at storage locations.

M0102Shaft Supports

Mounting and support for shafts and guide elements.

M0107Bushings

Low-friction bearing surfaces for sliding and pivoting parts.

Sensing and signaling

WireSensors / Switches

Presence detection and button or switch inputs.

E1115Warning & Signaling Lights

Visual status indication at zones and stations.

E1116Stack Lights

Multi-color zone status visible from a distance.

E1108Timers

Timing control for sequencing and delays.

Blickle caster wheel for mobile pick-to-light carts
Blickle caster wheel
Slide rails for pull-out trays at pick locations
Slide rails
Bushing used in sliding and pivoting mechanisms
Bushings

Tip: Design your own frames and carts faster with the free FRAMES tool, and download 3D models from the inCAD Library to check fit before you order. Need a full design? Try RAPiD Design.

Use Cases by Industry

E-commerce and 3PL

Multi-line, multi-zone order fulfillment where accuracy and fast onboarding of seasonal staff matter most.

Distribution centers

Zone picking with orders passing through multiple work zones, supported by carts or conveyors.

Retail replenishment

Put-to-light sorting of incoming goods into store or customer orders.

Healthcare and pharma

Accuracy-critical picking of small items where confirmation at every pick supports quality processes.

Manufacturing kitting

Guided collection of components into kits for assembly lines, with lighted bins at the line side.

Automotive and spare parts

High-velocity service parts picked from dense shelving with fast operator turnover.

How to Choose a Pick-to-Light Approach

Use these three profiles as a starting point. Your own order profile, SKU velocity, and budget should drive the final decision.

Simple standalone

Choose when: you have a single zone, a small number of locations, and no host-system requirement.

Build with: an aluminum extrusion frame and simple shelving.

Integrated multi-zone

Choose when: orders cross several zones and you need pick-rate reporting through a WMS or ERP.

Build with: factory frames, conveyors, and sensors.

Mobile cart

Choose when: one operator should fulfill a whole order across many zones.

Build with: casters, frames, and slide rails.

Plan for growth: Pick-to-light systems can be simple or very evolved depending on budget and requirements, and you can add features as the technology evolves. Choosing modular, reconfigurable framing early makes later expansion far easier.

Frequently Asked Questions

Q
What is a pick-to-light system?

A pick-to-light system is a paperless order-fulfillment technology that uses alphanumeric displays and confirm buttons mounted at storage locations to guide operators through manual picking. The display lights up at the correct location, shows the quantity to pick, and the operator presses a button to confirm. This reduces search time and picking errors compared with paper pick lists.

Q
How does a pick-to-light system work?

An operator scans a container barcode, the system lights the display at each required storage location and shows the quantity, the operator picks the items into the container and presses the confirm button, and the system moves on to the next location until the order is complete. Advanced systems add digital readouts and extra instructions.

Q
What is the difference between pick-to-light and put-to-light?

Pick-to-light directs an operator to take items from storage locations to fill an order. Put-to-light reverses the flow: the system directs the operator to place incoming goods into the right location, such as a store order, customer order, or another grouping. Both use lighted displays and confirm buttons.

Q
How long does it take to train operators on pick-to-light?

With an efficient pick-to-light system, operator training can be reduced to about 30 to 45 minutes. Traditional picking can take hours or more to learn, depending on the size and complexity of the warehouse, because operators must learn locations and read pick lists.

Q
Can pick-to-light integrate with a WMS or ERP?

Yes. A pick-to-light system can run standalone or integrate with a warehouse management system (WMS), enterprise resource planning (ERP), supply chain management, or other host systems. Integrated systems can also produce pick-rate reports, analyze productivity, and adjust work-zone sizes to match labor to order volume.

Q
What mechanical components are used to build a pick-to-light system?

Common components include factory frames, aluminum extrusion, rollers, slide rails, conveyors, casters, posts and struts, gussets and angle plates, machined sheet metal, shaft supports, bushings, and metal materials, plus electrical parts such as sensors, switches, warning and signaling lights, stack lights, and timers.

Q
What are the main benefits of pick-to-light systems?

The main benefits are faster operator training, higher picking accuracy, less walking and idle time, paperless record keeping, optional integration with WMS and ERP systems, and lower labor cost per order. Because they follow existing work zones, they are also easy to expand as the business grows.

Up next in the series: Warehouse Automation Part 2: Automatic Guided Vehicles & Autonomous Mobile Robots. As you grow, MISUMI hopes to grow with you.

Ready to build your pick-to-light station?

Shop Warehouse Automation Components Browse All Mechanical Components
Share this article: LinkedIn Twitter Facebook

Get More Articles Like This

Weekly engineering insights delivered to your inbox. No spam.

Written by

Carlicia Layosa

Carlicia is the Marketing Automation Manager at MISUMI. She holds a bachelor's degree in Mechanical Engineering and a master's degree in Energy Engineering from the University of Illinois at Chicago. She is a Certified SOLIDWORKS Associate, Marketo Certified Expert, and is passionate about education and training.

← Previous Locating Pin Alignment: How to Prevent Part Binding in Jigs and Fixtures (Video) Next → Shoulder Screws: What They Are, How They Work, and Common Applications