A combination wrench is one of the most common hand tools used for tightening and loosening hex nuts and bolts. Its design is simple: one end is open, while the other is closed in a box shape, giving the user two ways to grip the same size fastener. That makes it useful for everything from general maintenance and equipment assembly to automotive work and industrial repair. Understanding how a combination wrench works, where it is most useful, and how it compares to other wrench types can help make tool selection a lot more practical.
Browse Combination WrenchesHow a Combination Wrench Works
A combination wrench works by giving the user two different ways to turn the same nut or bolt. One end of the tool is open, which allows it to slide onto the sides of a fastener from the side. This is useful when there is not enough clearance to place a tool directly over the top, or when the fastener needs to be engaged and repositioned quickly. The open end is often used for starting a fastener loose or making quick turns in tighter spaces.
The other end is a box end, which fits over the entire head of the nut or bolt. Because it contacts more of the fastener’s sides, it provides a more secure grip and reduces the chance of slipping when more torque is needed. In many cases, the box end is the better choice for breaking a fastener loose or tightening it more firmly.
Since both ends are made for the same size, the user can switch between them depending on the situation. A common approach is to use the box end when a stronger, more controlled grip is needed, then switch to the open end for faster turning once the fastener moves more freely.

Common Types and Variations of Combination Wrenches
- Standard combination wrench
The most common type. It has an open end on one side and a box end on the other, both sized for the same fastener. It is used for general tightening and loosening work. - Offset combination wrench
Many combination wrenches have a slight offset in the box end. This helps create hand clearance above flat surfaces and can make the tool easier to turn in tighter spaces. - Ratcheting combination wrench
This version has a ratcheting box end that allows the fastener to be turned without removing and repositioning the wrench after each turn. It is useful for repetitive work and areas with limited swing room. - Stubby combination wrench
A shorter version made for tight spaces where a full-length wrench will not fit. It offers less leverage, but it can be helpful in compact assemblies or crowded equipment layouts. - Long-pattern combination wrench
This type has a longer handle, which gives the user more leverage. It is often useful for loosening tighter fasteners or reaching into deeper spaces. - Flex-head combination wrench
This variation has a box end that pivots or flexes. It can help reach fasteners at awkward angles or in locations where a straight wrench is hard to position. - Metric combination wrench
Designed for metric fasteners. These are commonly used in many industrial, automotive, and imported equipment applications. - SAE combination wrench
Designed for SAE, or inch-based, fasteners. These are still common in many older systems, maintenance environments, and certain equipment applications. - Polished or chrome-plated combination wrench
Some wrenches differ by finish as well as shape. A polished or chrome-plated surface can help resist corrosion and make the tool easier to clean after use. - Heavy-duty combination wrench
Built for tougher service conditions, often with thicker construction or stronger materials. These are used where higher torque and repeated industrial use are expected.
Adantages of Combination Wrenches
The open end can be useful for quickly engaging a fastener from the side, especially when there is not enough clearance to fit over the top. The box end, on the other hand, surrounds the fastener more completely and provides a firmer hold. This gives the user the option to choose the end that best fits the situation.
Combination wrenches are also valued for their simplicity. They do not rely on moving parts in their basic form, which makes them durable and easy to maintain. In many work environments, that straightforward design is an advantage because the tool can be used repeatedly without much concern for mechanical failure.
Another benefit is control. The box end helps reduce the chance of slipping compared with tools that contact fewer sides of the fastener. That can make it easier to apply torque with more confidence, especially when loosening tight bolts or making final tightening adjustments.
They are also convenient in areas where socket tools may not fit well. In confined spaces, around obstructions, or on exposed fasteners where there is limited room above the bolt head, a combination wrench can often be easier to position and use. This makes it a common choice for field service, machinery work, and general shop use.
Parting Thoughts
MISUMI USA carries a wide range of Box End Wrenches & Ratchets, including – combination, double ended box, spanner, and more. If you have any questions about fastening concerns for your next project or fix, please feel free to contact our product experts, and engineers. For more insights about combination wrenches, and other manufacturing related articles be sure to check out our blog, and articles like – 7 Quick Facts About Combination Wrenches, 6 Tips on Using a Combination, Wrench Conversion Chart, and more.
Author: Scott Bredemann | Updated: 4/7/2026
Disclaimer:
The content on this webpage is for informational purposes only. MISUMI makes no guarantees, expressed or implied, regarding the accuracy, completeness, or validity of the information. Performance parameters, tolerances, designs, materials, or processes should not be assumed to reflect third-party suppliers’ or manufacturers’ deliverables within MISUMI’s network. Buyers are responsible for specifying their part requirements.