Tin Chemical Symbol SN

What Is Tin? Properties, Uses, and Applications in Industry

Author: Scott Bredemann

Updated: 07/14/2025 | Read Time: 7mins

Tin is one of those materials that tends to fly under the radar, yet it’s been quietly supporting human progress for thousands of years. From early bronze tools to modern electronics and food-safe coatings, tin’s versatility has kept it relevant across generations. Today, it shows up in places most people don’t think about—inside soldered electrical connections, lining steel cans, or used in metal alloys that enhance strength and corrosion resistance in industrial parts. Despite its low profile, tin remains essential in both everyday products and specialized manufacturing processes.

Tin Defined

What is Tin? Tin is a chemical element with the symbol Sn, derived from its Latin name stannum. It sits at atomic number 50 on the periodic table and is classified as a post-transition metal. In its pure form, tin is soft, silvery-white, and easy to bend—so much so that it can be shaped by hand. When it bends, it produces a distinctive crackling sound known as “tin cry,” caused by the movement of its crystal structure.

What makes tin particularly useful is its natural resistance to corrosion. Unlike iron or steel, tin doesn’t rust easily, which makes it ideal for protective coatings. It also has a relatively low melting point—about 232°C (450°F)—which has made it a go-to material for soldering applications, especially in electronics where reliable joints are critical.

Where is Tin Found?

Tin is usually found in nature as cassiterite, a tin oxide mineral. Most of the world’s tin is mined in Southeast Asia, with major producers including China, Indonesia, and Myanmar. While tin itself isn’t rare, it’s typically found in low concentrations, which means extracting and refining it requires significant processing.

Physical Properties of Tin vs. Other Common Metals

This section takes a closer look at the physical properties of tin—such as density, melting point, and conductivity—and how they stack up against other commonly used metals like aluminum, copper, and Iron.

Metal Properties Comparison
Property Tin (Sn) Aluminum (Al) Copper (Cu) Iron (Fe) Lead (Pb)
Appearance Silvery-white Silvery-gray Reddish-brown Gray, lustrous Dull gray, bluish tint
Density (g/cm³) 7.31 2.70 8.96 7.87 11.34
Melting Point (°C) 231.93 660.3 1,084.62 1,538 327.46
Boiling Point (°C) 2,602 2,519 2,562 2,862 1,749
Hardness (Mohs) 1.5 2.75 3 4 1.5
Thermal Conductivity 66.8 W/m·K 237 W/m·K 401 W/m·K 80.4 W/m·K 35.3 W/m·K
Electrical Conductivity 8.7 × 10⁶ S/m 3.77 × 10⁷ S/m 5.96 × 10⁷ S/m 1.00 × 10⁷ S/m 4.55 × 10⁶ S/m
Malleability High Very High Very High Medium High
Ductility Moderate High Very High High Low
Magnetic? No No No Yes No

Mechanical Properties of Tin vs. Other Common Metals

In this section, we compare the mechanical properties of tin—such as hardness, strength, and ductility—to those of more robust metals like lead, aluminum, and copper.

Metal Mechanical Properties Comparison
Property Tin (Sn) Aluminum (Al) Copper (Cu) Iron (Fe) Lead (Pb)
Tensile Strength (MPa) 14 – 28 90 – 400 (varies by alloy) 210 – 370 370 – 540 12 – 18
Yield Strength (MPa) ~15 35 – 300 33 – 250 250 – 460 ~18
Hardness (Brinell, HB) ~15 15 – 150 35 – 110 120 – 190 5 – 15
Elastic Modulus (GPa) 50 69 110 200 14
Elongation at Break (%) ~50 (high ductility) 10 – 50 20 – 60 10 – 40 ~50
Poisson’s Ratio 0.36 0.33 0.34 0.27 0.44
Fatigue Strength (MPa) Low Moderate to high Moderate High Very low
Impact Resistance Low Moderate Moderate High Very low

Chemical Properties of Tin vs. Other Common Metals

Metal Chemical Properties Comparison
Property Tin (Sn) Aluminum (Al) Copper (Cu) Iron (Fe) Lead (Pb)
Common Oxidation States +2, +4 +3 +1, +2 +2, +3 +2, +4
Standard Electrode Potential (V) −0.14 (Sn²⁺/Sn) −1.66 (Al³⁺/Al) +0.34 (Cu²⁺/Cu) −0.44 (Fe²⁺/Fe) −0.13 (Pb²⁺/Pb)
Reactivity Moderate; resistant to corrosion Highly reactive; forms oxide layer Low to moderate; resists corrosion Reactive; rusts easily in moist air Low to moderate; tarnishes but slow to corrode
Corrosion Resistance Good; forms protective oxide Excellent; self-healing oxide layer Good; develops patina Poor; rusts (iron oxide forms) Moderate; forms protective oxide but can corrode in acids
Reaction with Acids Reacts slowly with dilute acids Reacts rapidly with acids Reacts with strong acids Reacts readily with acids Reacts slowly with acids
Tarnish Formation Tin oxide (SnO₂) Aluminum oxide (Al₂O₃) Copper oxide, green patina (CuCO₃) Iron oxide (rust) Lead oxide (PbO)
Toxicity Low toxicity Low toxicity Low toxicity Low to moderate (iron salts generally safe) Toxic in high amounts
Uses in Alloys Tin-copper (bronze), tin-lead Aluminum alloys (various) Brass (copper-zinc), bronze Steel (iron-carbon), cast iron Lead alloys, solder alloys

Applications of Tin in Manufacturing

Common applications include tin plating to protect other metals from rust, soldering in electronics due to its low melting point, and use in bronze alloys for bearings and bushings. This section explores the key ways tin is used across various industries.

Industry Application of Tin
Automotive Used in solders for wiring and electronic components; tin-plated parts for corrosion resistance.
Construction Tin alloys used in pipes, solders, and roofing materials; tin plating protects structural elements.
Machinery Tin-based babbitt metal used in bearings to reduce friction; tin solders used in control systems.
Appliances Found in circuit boards and connectors for household appliances due to its reliable conductivity.
Tools Tin coatings improve tool life by reducing corrosion; used in specialty soldering tools.
Shipbuilding Tin-alloy bearings used in engines and propeller shafts; tin coatings help resist saltwater corrosion.
Aerospace Used in high-reliability solders for avionics and navigation systems; also found in anti-corrosion alloys.
Infrastructure Tin coatings and solders used in electronics, lighting, and water delivery systems; supports longevity.
Energy Tin-based materials used in solar panels and battery technologies, including lithium-ion anodes.
Packaging Tin-plated steel (tinplate) widely used in food and beverage containers for corrosion resistance and safety.

Parting Thoughts

Understanding the properties and applications of metals like tin is essential across industries such as electronics, packaging, precision manufacturing, and materials science. Whether you’re working on corrosion-resistant coatings, choosing the right alloy for soldering, or developing components that require stable performance over time, knowing the characteristics of tin can inform better design and material choices. Here are a few examples of tin coated, and tin metal products that MISUMI USA carries:

Thread Solder

Protective Braided Tubing

Bind Head Phillips Drive Screw

MISUMI USA provides a broad selection of metal materials and components—both standard and configurable—including rods, plates, and blocks in various metals. If you’re unsure which material best fits your design requirements, our technical support team can assist. For more detailed resources, be sure to check out our other materials-focused guides and engineering tables.

⚙ Browse MISUMI Metal Products