Dynamic bearing systems are, at their most basic level, an engineered hole/shaft interface that is designed to allow for relative rotation between the components. Typically one of the parts is completely fixed while the other part rotates against it. Bearing system designs can range from very simple to very complicated, with many moving parts and components employed to transmit motion across the system.
Bushings and bearings are two of the most common components used to reduce friction between moving parts, yet they work in different ways and are suited for different applications. While both serve the same basic purpose, supporting motion and minimizing wear, their design, materials, and performance characteristics vary significantly.
This article explores the key differences between bushings and bearings, their advantages, and when one might be a better choice than the other.
What are Bearings?
A bearing allows parts to move smoothly by reducing friction between surfaces that would otherwise grind against each other. Instead of relying on direct sliding contact, most bearings use rolling elements, such as balls, rollers, or needles, housed between inner and outer rings to support loads and guide motion with minimal resistance.
This design makes them ideal for applications requiring high rotational speeds, precise alignment, and efficient energy transfer, such as motors, gear assemblies, and heavy industrial equipment. By distributing loads evenly and minimizing wear, bearings help ensure reliable performance and longer service life for machinery.
What are Bushings?
A bushing is a simple yet effective component designed to reduce friction and wear between two surfaces that slide against each other. Unlike bearings, which rely on rolling elements, bushings provide a smooth, stationary sleeve (often made of bronze, plastic, or composite materials) through which a shaft or other moving part passes.
They are commonly used in applications where movement is slower, loads are heavier, or space is limited, such as hinges, pivot points, or machinery subject to vibration. By absorbing impact and distributing forces, bushings help protect both the moving parts and the housing, contributing to longer service life and reliable operation.
Physical Properties: Bearings vs. Bushings Table

| Feature | Bushings | Bearings |
|---|---|---|
| Type of Motion | Sliding motion between surfaces | Rolling motion via balls, rollers, or needles |
| Friction | Higher friction compared to bearings, but often self-lubricating | Lower friction due to rolling elements |
| Load Capacity | Handles heavier static loads well | Excels at supporting dynamic loads and high-speed rotation |
| Precision | Suitable for applications with less critical alignment | Ideal for applications requiring precise alignment and smooth motion |
| Maintenance | Often low-maintenance; some types are self-lubricating | May require lubrication and periodic inspection |
| Common Materials | Bronze, plastic, composite, graphite, PTFE | Steel, stainless steel, ceramic, hybrid combinations |
| Typical Applications | Hinges, pivot points, agricultural equipment, heavy machinery | Motors, gearboxes, conveyors, robotics, precision instruments |
Plain Bearings (Bushing/Shaft)
The simplest kind of bearing goes by a number of different names, such as plain bearing, journal bearing, or bushing bearing. This type of bearing system is simply an engineered running clearance fit that is typically constructed from a bushing and a shaft. This simple hole/shaft interface is designed to facilitate rotational motion of the journal within the bearing hole typically with an external lubricating compound designed to fill in the clearance spaces between the shaft and hole.
In this way, there are no intermediary rolling or sliding elements that allow motion. Journal bearings are typically built nowadays by leveraging advanced materials technologies such as oil impregnated bushings in order to build a joint that has a low rolling/sliding resistance friction associated with it.
These bearings are simple to construct, but they are almost always employed alongside a comprehensive, reliable, active lubrication system. There are purely “dry” (no lubrication) journal bearings that can be specified for low-load, low-speed applications. These types of bearing systems typically employ polymer bushings that can be specified, but most industrial applications that use journal bearings are fully lubricated shaft/bushing systems.
These systems must be located in areas of the machine that are reasonably accessible for preventative maintenance or repair if needed. The successful operation of these journal bearing systems are highly contingent on the presence of saturating lubrication at every single rotation of the shaft within the bushing. A failure of the lubrication system typically leads to fast, catastrophic failure of the entire machine.
If an active lubrication system is not feasible for a particular application that must sustain high speeds, as well as variable dynamic loading, it is recommended that a rolling contact bearing system design be considered.
Rolling(Ball)Bearings
A bearing is a mechanical component that usually possesses a rolling or sliding component that further reduces the friction between the moving shaft and the stationary hole or reference point. The most common and easily identifiable type of bearing is probably the ball or roller bearing.
These types of bearings are comprised of an inner raceway that is usually directly (press) fitted to the inner shaft. The rolling elements (balls, or conical rollers) then roll along the opposite side of the inner raceway, and they are all contained within one unit by the outer raceway. It’s not difficult to visualize how this system allows relative motion between the inner and outer raceways, via the relative rolling of the rolling elements.
The rolling elements in the bearing cartridge can be lubricated and sealed completely in between the inner and outer raceways of the bearing in order to prevent any exposure from environmental contaminants.
The rolling elements of the ball bearing can be fabricated from a hardened tool steel alloys, and they can even be specified with additional coatings (such as Chrome) in order to further increase the wear resistance and corrosion resistance of the ball bearing.
Stainless steel ball bearing systems can also easily be obtained if corrosion or degradation is a concern in the particular application. If significant thrust loads must be sustained, whereas a journal bearing would be almost useless, a cylindrical or needle rolling bearing system is the ideal bearing for the job and can readily be specified to meet a wide range of applications.
For lower cost applications where the bearing can be readily accessible for lubrication and maintenance, a journal bearing may be a perfectly suitable design and can be employed in many types of applications. However, if accessibility to the bearing would be impossible, and/or the bearing system must sustain radial high loads or thrust loads, the design engineer should proceed and begin exploring the wide world of rolling contact bearings.
Either way, the odds are very good that a suitable bearing is out there waiting to be unearthed for each and every variant of mechanical application.
Coefficient of Friction: Bearings vs. Bushings Table
Coefficient of Friction Comparison
| Type & Material | Coefficient of Friction (μ) | Application Notes | Operating Conditions |
|---|---|---|---|
| BEARINGS | |||
| Ball Bearing (Steel on Steel) | 0.001 – 0.0015 | High-speed applications, precision machinery | Clean, lubricated conditions |
| Roller Bearing (Steel) | 0.0015 – 0.002 | Heavy load applications, automotive | Proper lubrication required |
| Ceramic Ball Bearing | 0.0008 – 0.0012 | High-temperature, corrosive environments | Minimal lubrication needed |
| Needle Bearing | 0.002 – 0.004 | Space-constrained applications | Light to medium loads |
| Thrust Bearing | 0.0015 – 0.003 | Axial load applications | Controlled lubrication |
| BUSHINGS | |||
| Bronze Bushing | 0.08 – 0.15 | Marine applications, pumps | Water or oil lubricated |
| PTFE (Teflon) Bushing | 0.04 – 0.08 | Food grade, chemical resistant | Dry running capability |
| Nylon Bushing | 0.15 – 0.25 | Light duty, quiet operation | Dry or lightly lubricated |
| Graphite Impregnated | 0.05 – 0.12 | High-temperature applications | Self-lubricating properties |
| Rubber Bushing | 0.6 – 1.2 | Vibration dampening, automotive | Designed for compliance, not rotation |
| Steel Bushing (Dry) | 0.4 – 0.6 | Heavy duty, temporary applications | Requires regular lubrication |
| Composite Bushing | 0.08 – 0.18 | Maintenance-free applications | Self-lubricating, various environments |
Bearings vs Bushings: Advantages and Disadvantages
When selecting components for guiding and supporting moving parts in mechanical systems, two common options are bearings and bushings. Both play bearings and bushings play a crucial role in reducing friction and supporting loads, yet they differ significantly in design, performance, and ideal applications. Understanding the strengths and limitations can help you choose the right solution for efficiency, durability, and cost-effectiveness in their machinery.
Bearings are valued for their ability to reduce friction to very low levels, allowing machinery to operate smoothly and efficiently, even at high speeds. They also offer precise alignment for rotating parts and can handle dynamic loads well, which helps extend equipment life. However, bearings can be more expensive due to their intricate design and may require regular lubrication or maintenance. They are also more sensitive to contamination from dust or debris, which can shorten their lifespan if not properly sealed or maintained.
Bushings, on the other hand, are simpler in design and generally more cost-effective. They excel at handling heavy static loads and absorbing shock or vibration, making them a reliable choice for slower-moving or high-impact applications. Many bushings are made from self-lubricating materials, which minimizes upkeep. The trade-off is that they typically have higher friction levels than bearings, making them less suitable for high-speed or precision applications. In systems with continuous motion, bushings may wear out faster and require more frequent replacement.
Find Bushings and Bearings at MISUMI
MISUMI USA carries a large offering of bushings, and bearings, including: plain, self-lubricating, flanged, ball, roller, and more. If you have questions about selecting between the right bushing or bearing for your next project or repair, our product experts and engineers are ready to help.
Explore more from The MechLab Blog for additional articles on bushings, including All About Bushings, Bronze vs. Brass: Differences, Advantages, and Disadvantages, and more.