Author: Scott Bredemann
Updated: 03/17/2025 | Read Time: 6mins
Bronze and brass are often mistaken for one another, but these two copper-based alloys have distinct properties that make them suited for different applications. Whether you’re working in manufacturing, construction, or even the arts, choosing the right material can make a significant difference in performance, durability, and cost.
In this article, we’ll break down the composition, properties, and applications of bronze and brass, giving you a clear guide on when to use each alloy.
What is Bronze?
Bronze is a durable, copper-based alloy known for its strength, wear resistance, and excellent corrosion resistance—especially in marine environments. It’s primarily made from copper and tin, though other elements like aluminum, silicon, phosphorus, or manganese are often added to enhance specific properties.
Types of Bronze:
- Phosphor Bronze- contains phosphorus, making it stronger and more wear-resistant. It’s commonly used in electrical components and bearings.
- Aluminum Bronze – has aluminum added for extra strength and superior corrosion resistance, making it ideal for marine and industrial applications.
- Silicon Bronze – includes silicon, improving corrosion resistance and weldability. It’s often used in sculptures and industrial hardware.
The process of making bronze starts with melting copper in a furnace. Once it reaches the right temperature, alloying elements like tin or aluminum are added in precise amounts. Next, the molten metal is thoroughly mixed to ensure consistency. It’s then poured into molds to form ingots, billets, or finished parts, depending on the intended use. Some bronze components go through additional shaping, like rolling or forging, to refine their form. In some cases, heat treatment is used to improve strength or hardness.
What is Brass?
Like Bronze, brass is a copper-based alloy – it is primarily composed of copper and zinc. It is known for its bright gold-like appearance, excellent machinability, and resistance to corrosion. The amount of zinc in brass can vary, altering its strength, hardness, and color. Because of its versatility, brass is widely used in applications ranging from plumbing and electrical components to musical instruments and decorative fixtures.
Types of Brass:
- Red Brass (High Copper Brass): Contains a higher percentage of copper (85–95%) with less zinc, offering better corrosion resistance and a reddish color.
- Yellow Brass: Has a balanced copper-to-zinc ratio (around 60/40), making it strong, ductile, and easy to machine.
- Leaded Brass: Small amounts of lead (1–3%) are added to improve machinability, making it ideal for precision components like gears and valve parts.
- Admiralty Brass: Contains tin in addition to copper and zinc, enhancing its resistance to seawater corrosion,
Again, like with bronze, the manufacturing process of brass starts with melting copper in a furnace. But, unlike with bronze, zinc is then added in carefully measured amounts to achieve the desired alloy composition. If additional elements like lead or tin are needed, they are introduced at this stage. The produced billets or ingots are later processed through rolling, extrusion, or casting to form sheets, rods, or custom shapes. Some brass alloys undergo annealing, a heat treatment process that softens the metal and enhances its formability.

Differences in Mechanical Properties of Bronze and Brass
| Property | Bronze | Brass |
| Composition | Copper with tin (and sometimes aluminum, silicon, or phosphorus) | Copper with zinc (sometimes with lead or tin) |
| Hardness | Generally harder and more wear-resistant | Softer and more malleable |
| Strength | Higher tensile strength, making it more durable under load | Lower tensile strength but still strong for structural use |
| Machinability | More difficult to machine due to hardness | Easier to machine and shape |
| Corrosion Resistance | Excellent, especially in marine environments | Good, but more prone to corrosion in saltwater |
| Electrical Conductivity | Lower conductivity than brass | Higher conductivity, often used in electrical applications |
| Thermal Conductivity | Lower, making it better for applications requiring heat resistance | Higher, meaning it transfers heat more efficiently |
| Workability | Less ductile and more brittle | More ductile and easier to bend or form |
| Wear Resistance | Superior wear resistance, ideal for bearings and bushings | Less wear-resistant but still durable for many applications |
Differences in Chemical Properties of Bronze and Brass
| Property | Bronze | Brass |
| Primary Elements | Copper (80–90%) and Tin (5–12%), with possible additions of aluminum, silicon, or phosphorus | Copper (55–95%) and Zinc (5–45%), sometimes with lead or tin |
| Oxidation Reaction | Forms a protective oxide layer (patina) that prevents further corrosion | Tarnishes and may develop a greenish patina (verdigris) over time |
| Corrosion Resistance | Excellent, especially in marine and industrial environments | Good, but more susceptible to dezincification in aggressive environments |
| Reaction to Acids | More resistant to acid corrosion than brass | More prone to acid corrosion, especially in strong acids |
| Reaction to Saltwater | Highly resistant, making it ideal for marine applications | Can corrode in saltwater due to dezincification |
| Conductivity (Electrical & Thermal) | Lower electrical and thermal conductivity compared to brass | Higher conductivity, making it more suitable for electrical applications |
| Magnetism | Non-magnetic | Non-magnetic, but can become slightly magnetic if lead is present |
| Toxicity | Generally non-toxic; some alloys are used in food and medical applications | Some leaded brasses can pose health concerns in drinking water applications |
The 3 Most Common Applications for Bronze and Brass
Bronze Applications:
- Bearings and Bushings – Due to its high wear resistance and low friction, bronze is widely used in heavy machinery and industrial equipment.
- Marine Hardware – Its excellent corrosion resistance makes it ideal for ship fittings, propellers, and underwater components.
- Sculptures and Monuments – Artists and architects favor bronze for its durability and ability to develop a protective patina over time.
Brass Applications:
- Plumbing and Fittings – Brass is commonly used for pipes, valves, and faucets due to its corrosion resistance and ease of machining.
- Electrical Connectors – Brass’s high conductivity and durability make it a popular choice for electrical terminals and connectors.
- Musical Instruments – Its excellent acoustic properties make it ideal for instruments like trumpets, saxophones, and trombones.
We hope you found this article helpful and of value – If you have any questions about using bronze, or brass within your projects to meet your manufacturing goals, please feel free to reach out to our team of product experts and engineers. MISUMI USA, also has a vast array of products in stock and ready to ship to meet your bronze and brass fitting and parts needs, including: