Author: Scott Bredemann
Updated: 08/22/2024 | Read Time: 7mins
Brass is a material most of us recognize, whether it’s from connecting a garden hose or fastening the buttons on a classic 1990s denim jacket. This versatile, golden-hued alloy has been shaping industries and crafting everyday essentials since the days of the Roman Empire. In this article, we’ll explore everything manufacturers need to know about brass—its composition, applications, strengths, and unique properties. Whether you’re a seasoned industrial expert or a curious manufacturer looking to learn more, we’ll dive into what makes brass an indispensable material and its endless potential in manufacturing.
What is Brass?
Brass, often referred to as the “metal of the gods,” is an alloy primarily composed of copper and zinc – though, its composition can vary widely depending on the desired properties and applications. By blending these elements in different proportions, manufacturers can tailor brass to meet specific requirements, whether it’s for hardware (think doorknobs, hinges, cabinet hardware), plumbing fixtures, or electrical functions ( think connectors, terminals, and components).
Key Components of Brass
Below, you’ll find a graph illustrating the typical composition of brass, showcasing the proportions of its primary elements, such as copper and zinc. Additionally, we’ve included a detailed table that highlights how each element contributes to the unique properties of brass, from improving machinability to enhancing corrosion resistance.

| Elements in Brass | Value |
| Copper | Main component, provides good electrical conductivity and workability |
| Zinc | Increases strength and machinability, lowers melting point |
| Lead | Improves machinability but can be detrimental to health (use with caution) |
| Tin | Improves corrosion resistance and castability |
| Iron | May improve strength and machinability in small quantities |
| Aluminum | Can improve deoxidation and grain refinement |
| Silicon | Can improve strength and wear resistance |
| Other | Trace amounts of other elements like nickel, arsenic, antimony, etc. may be present depending on the specific brass alloy |
Types of Brass
Brass comes in a bunch of different varieties, each tailored to suit specific applications and industries. From admiralty brass used in marine environments to free-machining brass favored in precision engineering, the versatility of this alloy knows no bounds. Whether it’s architectural fittings, automotive components, or musical instruments, there’s a type of brass suited for every task and challenge.
- Alpha Brass: Contains less than 37% zinc and is primarily composed of copper. It’s relatively soft and malleable, making it suitable for decorative purposes, musical instruments, and plumbing fixtures.
- Alpha-Beta Brass: Contains between 37% to 45% zinc. This type of brass has higher strength and hardness compared to alpha brass. It’s used in applications requiring more durability such as valve stems, gears, and marine fittings.
- Beta Brass: Contains more than 45% zinc. It has even higher strength and hardness but is less ductile compared to alpha brass. Beta brass is used in applications requiring high strength and corrosion resistance, such as locks, keys, and fittings.
- Cartridge Brass (70/30 Brass): Composed of 70% copper and 30% zinc, this type of brass is widely used in the manufacturing of ammunition casings, plumbing fittings, and architectural trim due to its good combination of strength, ductility, and corrosion resistance.
- Naval Brass: Contains around 60% copper, 39% zinc, and a small amount of tin. It offers excellent corrosion resistance in seawater and is used in marine hardware, propeller shafts, and fittings aboard ships.
- Free Cutting Brass: Contains added elements such as lead, sulfur, or selenium to improve machinability. It’s used in applications where intricate machining is required, such as electrical connectors, plumbing components, and automotive fittings.
- Red Brass: Also known as 85/15 brass, it consists of 85% copper and 15% zinc. Red brass offers good corrosion resistance and is commonly used in water supply fittings, pump parts, and plumbing fixtures.
- Yellow Brass: Typically contains around 67% copper and 33% zinc. It’s used in various decorative applications, musical instruments, costume jewelry, and architectural trim due to its attractive golden color and ease of fabrication.
- DZR Brass (Dezincification Resistant Brass): Contains small amounts of arsenic or other elements to resist dezincification, a form of corrosion that can occur in brass fittings exposed to certain environments such as high temperatures and acidic water. DZR brass is commonly used in plumbing fittings and valves.
Where is Brass Manufactured?
Brass production can be considered a bit of a global endeavor, with manufacturers spanning continents to meet the growing demand for this invaluable alloy. And, though China is one of its leading suppliers – essentially where ever copper and zinc are found, There are traditional foundries in Europe to state-of-the-art facilities in Asia. Major producer locations:
- China: The leading producer of brass, accounting for a significant portion of the global market.
- India: A rapidly growing producer of brass, known for its competitive pricing and vast manufacturing capabilities.
- North America and Europe: These regions house established brass producers known for their high-quality products and adherence to strict environmental regulations.

The Applications of Brass
Brass is a testament to its versatility and adaptability. From household fixtures and electronic connectors to industrial valves and architectural accents, brass plays a vital role in ton of applications. Its aesthetic appeal, combined with its durability and reliability, makes brass the material of choice for designers, engineers, and craftsmen alike, ensuring its enduring presence in our modern world.
- Bearings and Bushings: Brass alloys are used in bearings and bushings due to their self-lubricating properties and resistance to wear and corrosion.
- Valves and Fittings: Brass valves, fittings, and couplings are common in industrial settings due to their corrosion resistance and ease of fabrication.
- Pumps and Pump Components: Brass impellers, casings, and fittings are used in pumps due to their corrosion resistance and ability to withstand high pressures.
- Springs and Fasteners: Brass springs and fasteners are employed in various industrial applications where corrosion resistance and electrical conductivity are important.
- Heat Exchangers: Brass tubes and fins are used in heat exchangers due to their excellent thermal conductivity, making them efficient for transferring heat.
- Instrumentation: Brass components are used in industrial instruments, sensors, and gauges due to their electrical conductivity and machinability.
- Decorative Surfaces: Brass plating is applied to industrial products to enhance their appearance and provide corrosion resistance.
- Machined Components: Brass is widely used for precision machining in industrial manufacturing due to its ease of machining and dimensional stability.
- Sprinkler Systems: Brass components are used in fire sprinkler systems due to their corrosion resistance and reliability in high-pressure environments.
- Electrical Connectors and Terminals: Brass is utilized in electrical connectors and terminals in industrial equipment due to its excellent electrical conductivity and durability.

How Strong is Brass? Comparing it to Other Materials
While brass may not rival steel in sheer strength, its unique combination of properties makes it a formidable contender in many applications. By understanding its tensile strength, yield strength, and hardness, engineers can leverage brass’s strengths to optimize performance and efficiency. Whether it’s in structural components or precision instruments, brass proves itself time and time again.
| Property | Brass | Steel | Aluminum |
| Strength | Moderate (varies by alloy) | High (varies by type and grade) | Moderate to High (alloy dependent) |
| Durability | Corrosion-resistant, tarnishes | Corrosion-resistant with coatings | Corrosion-resistant, oxidizes |
| Malleability | Highly malleable | Moderate to High | Highly malleable |
| Cost | Moderate to High | Moderate | Moderate to Low |
The Maximum Operating Temperature of Brass
Temperature plays a crucial role in the performance and longevity of brass components, especially in high-temperature environments. By understanding the maximum operating temperature of brass alloys, engineers can ensure that they remain within safe limits, preventing premature failure and degradation. Through careful design and material selection, brass can withstand the rigors of extreme heat, delivering reliable performance when it matters most.
| Brass Alloy | Maximum Operating Temperature (°F) | Solidus Melting Point (°F) | Liquidus Melting Point (°F) |
| C26000 | 482 – 572 | 1654 | 1700 |
| C27000 | 482 – 572 | 1654 | 1700 |
| C28000 | 482 – 572 | 1654 | 1700 |
| C33000 | 482 – 527 | 1652 | 1690 |
| C36000 | 482 – 527 | 1654 | 1700 |
| C44300 | 482 – 527 | 1654 | 1700 |
| C46400 | 482 – 527 | 1648 | 1697 |
Brass vs. Copper vs. Bronze
Brass, copper, and bronze are often used interchangeably, but each has its own distinct properties and applications. While brass boasts superior machinability and corrosion resistance, copper excels in electrical conductivity and heat transfer. Bronze, on the other hand, offers exceptional strength and wear resistance, making it ideal for bearings and bushings. By understanding the differences between these alloys, manufacturers can choose the right material for their specific needs, maximizing performance and efficiency.
| Material | Strength | Durability | Cost |
| Brass | Moderate | High | Moderate |
| Copper | High | High | High |
| Bronze | High | High | High |
Mechanical Properties of Popular Brass Alloys
This table provides an overview of some popular brass alloys, their corresponding alloy numbers, and their mechanical properties, including tensile strength, yield strength, and hardness. By understanding these variations, manufacturers can select the most appropriate brass alloy for their specific application, ensuring optimal performance and cost-effectiveness.
| Brass Alloy | Alloy Number | Tensile Strength (MPa) | Yield Strength (MPa) | Hardness (HB) |
| Admiralty | C44300 | 240-310 | 110-180 | 65-100 |
| Alpha | C68700 | 290-380 | 120-230 | 80-150 |
| Cartridge | C26000 | 380-550 | 170-310 | 60-100 |
| Commercial | C21000 | 205-345 | 80-140 | 40-95 |
| Gilding | C21000 | 205-345 | 80-140 | 40-95 |
| Muntz | C28000 | 290-460 | 130-310 | 55-95 |
| Naval | C46400 | 290-440 | 120-280 | 60-100 |
| Red | C23000 | 240-380 | 90-200 | 30-80 |
| Yellow | C26800 | 270-390 | 140-320 | 60-95 |
Conclusion:
We really hope you enjoyed learning all about the different aspects of brass on the MechLab Blog, and found the answers to any questions you may have had (or not had) about this interesting metal alloy. To learn more, or if you have any further questions, please visit/contact us at our website.
And, be sure to check out a small portion of MISUMI products that are created with brass:
Standoffs:
https://us.misumi-ec.com/vona2/mech/M1500000000/M1509000000/M1509010000/
Hex Nuts:
https://us.misumi-ec.com/vona2/mech_screw/M3303000000/M3303010000/
Ball Valves:
https://us.misumi-ec.com/vona2/mech/M2000000000/M2007000000/M2007010000/
Threaded Inserts: