Author: Scott Bredemann
Updated: 02/17/2025
Zinc is a bluish-white metal that plays a fundamental role in modern industry, valued for its corrosion resistance, versatility, and ease of processing. As the 24th most abundant element in the Earth’s crust, it is commonly extracted from ores like sphalerite and refined for use in a wide range of applications. Engineers and manufacturers depend on zinc for galvanization, die casting, and alloy production, where its properties enhance durability and performance. In this article, we’ll take a closer look at what zinc is, its key properties, and why it remains a cornerstone material in manufacturing.
What is Zinc?
Zinc (Zn) is a metallic element with atomic number 30, it is found primarily in the mineral sphalerite (zinc sulfide), zinc is extracted through a combination of mining and refining processes, such as roasting and electrolysis.
One of zinc’s defining characteristics is its ability to form a protective patina when exposed to the atmosphere. This natural oxidation layer prevents further corrosion, making zinc an ideal material for coatings, particularly in galvanization. It also has a relatively low melting point (419.5°C or 787.1°F), which makes it well-suited for die casting and alloy production.
In addition to its industrial uses, zinc is an essential trace element in biological systems. It plays a critical role in enzyme function, immune response, and cellular processes, making it a key nutrient for humans, animals, and plants alike. This dual importance—both as an engineering material and a biological necessity—sets zinc apart as a uniquely valuable element in modern applications.
History of Zn
German chemist Andreas Marggraf is often credited with the independent discovery of pure zinc in 1746, refining it through a controlled smelting process. By the 19th century, large-scale zinc production took off, particularly in Europe and the United States. Zinc became a critical material for galvanization—coating iron and steel to prevent rust—which played a major role in infrastructure, transportation, and industrial manufacturing.

Where is it found
Zinc is mined globally, with some of the largest producers being:
- China – The world’s top producer, responsible for nearly one-third of global zinc output.
- Peru – A major supplier, with extensive zinc deposits in the Andes.
- Australia – Home to significant zinc mines, including those in Queensland and the Northern Territory.
- United States – Key mining states include Alaska, Missouri, and Idaho.
- India & Kazakhstan – Both have rich zinc deposits and well-established mining operations.
Interestingly, zinc is also widely recovered through recycling. Scrap metals, galvanized steel, and discarded batteries serve as valuable secondary sources, making zinc one of the most recyclable industrial metals.
Physical Properties of Zinc
| Property | Description |
| Appearance | Bluish-white, metallic luster |
| Density | 7.14 g/cm³ |
| Melting Point | 419.5°C (787.1°F) |
| Boiling Point | 907°C (1665°F) |
| Thermal Conductivity | 116 W/(m·K) at 25°C |
| Electrical Conductivity | Moderate, about 28% that of copper |
| Malleability & Ductility | Brittle at room temperature, but malleable when heated between 100-150°C |
| Corrosion Resistance | Forms a protective oxide layer to prevent further oxidation |
Chemical Properties
| Property | Description |
| Atomic Number | 30 |
| Atomic Mass | 65.38 u |
| Reactivity | Moderately reactive, reacts with acids and bases |
| Reaction with Air | Forms a thin protective zinc oxide (ZnO) layer |
| Reaction with Acids | Dissolves in strong acids, releasing hydrogen gas (e.g., Zn + HCl → ZnCl₂ + H₂) |
| Reaction with Bases | Reacts with strong alkalis to form zincates (e.g., Zn + NaOH → Na₂ZnO₂ + H₂) |
| Alloying Ability | Easily forms alloys with copper, aluminum, and magnesium |
| Toxicity | Non-toxic in small amounts, essential for biological functions, but toxic in excess |
Mechanical Properties
| Property | Description |
| Tensile Strength | 110–200 MPa (varies based on purity and processing) |
| Yield Strength | 10–50 MPa (depends on alloy composition) |
| Hardness | 2.5 Mohs (pure zinc), ~80–120 Brinell (cast zinc) |
| Elastic Modulus | ~108 GPa |
| Poisson’s Ratio | 0.25–0.30 |
| Impact Resistance | Brittle at room temperature but improves when heated to 100–150°C |
| Machinability | Good; easily cut and shaped in die-casting applications |
| Wear Resistance | Moderate; improves when alloyed with other metals |
| Creep Resistance | Low; deforms under long-term stress at high temperatures |

Types of Zinc Metal and Their Uses
- Pure Zinc – High-purity zinc (99.99%) used in industrial applications such as galvanization, chemical production, and die casting.
- Galvanized Zinc – A protective zinc coating applied to steel or iron to prevent rust and corrosion, commonly used in automotive bodies, construction materials, pipelines, and outdoor structures.
- Zinc Alloys – Combinations of zinc with other metals to enhance strength, durability, and machinability, used in die-casting, bearings, and automotive parts.
- Zamak Alloys (Zamak 2, 3, 5, 7) – Zinc-aluminum-magnesium-copper alloys designed for precision casting, found in automotive parts, household hardware, and electronic enclosures.
- Brass (Zinc-Copper Alloy) – A strong, corrosion-resistant copper-zinc alloy used in plumbing fixtures, musical instruments, and electrical connectors.
- Zinc-Aluminum (ZA) Alloys – High-strength alloys with a greater aluminum content, used in die-casting, gears, and structural components.
- Rolled Zinc – Sheets, strips, and plates of zinc used in applications like roofing, batteries, and decorative elements.
- Zinc Powder & Dust – Fine zinc particles used in chemical processes, such as paints, coatings, anti-corrosion treatments, and batteries.
- Zinc Oxide (ZnO) – A white powder form of zinc with industrial and chemical uses, including rubber production, sunscreens, pharmaceuticals, and ceramics.
- Zinc Sulfate (ZnSO₄) – A water-soluble zinc compound used in agriculture and medicine, commonly found in fertilizers, animal feed, and dietary supplements.
We hope this deep dive into zinc has given you valuable insights into its properties, applications, and importance in manufacturing. At MISUMI USA, we offer a wide range of standard and customizable zinc and zinc-coated components to meet your needs: 🔗 Browse Zinc-Coated Screws & Fasteners 🔗 Explore Zinc-Plated Bolts 🔗 Check Out Zinc-Plated Nuts Looking for more insights on industrial metals? Explore our other articles covering steel, titanium, copper, aluminum, and more. Stay ahead with the right materials for your next project!