Author: Scott Bredemann
Updated: 02/24/2025
Steel is one of the most widely used materials in the world, but it has one major weakness—rust. That’s where galvanized steel comes in. Galvanized steel is regular steel that has been coated with a protective layer of zinc to prevent corrosion and extend its lifespan. This process makes it a popular choice in industries like construction, automotive manufacturing, and industrial equipment production. In this article, we’ll break down what galvanized steel is, how it’s made, and why it’s such a reliable material for so many applications. Here we will explore this material more indepth.
What is Galvanized Steel?
Galvanized steel is steel that has been coated with a layer of zinc to protect it from rust and corrosion. This process helps extend the lifespan of the metal, making it more durable and reliable for long-term use. The zinc coating acts as a barrier, preventing moisture and oxygen from reaching the steel underneath. Even if the coating gets scratched or damaged, the zinc still provides some level of protection by corroding first, a process known as sacrificial protection.
Because of its ability to resist rust, galvanized steel is commonly used in outdoor structures, construction materials, and industrial equipment. It is also found in everyday products like fencing, roofing, and even certain household appliances. The combination of strength, affordability, and low maintenance makes galvanized steel one of the most widely used materials in both industrial and consumer applications.
Methods of Galvanizing Steel
- Hot-Dip Galvanizing – The steel is submerged in a bath of molten zinc, creating a thick, durable coating that offers excellent corrosion resistance.
- Electro-Galvanizing – A thin layer of zinc is applied to the steel using an electric current, resulting in a smooth and uniform coating, often used in automotive and appliance industries.
- Galvannealing – A combination of hot-dip galvanizing and heat treatment, this process creates a matte, paintable surface with enhanced adhesion properties, commonly used in automotive and construction applications.
- Sherardizing – Also known as dry galvanizing, this method involves heating steel with zinc powder in a rotating drum, forming a strong, diffusion-bonded coating suitable for small parts and fasteners.
- Mechanical Plating – Zinc powder is applied to steel using tumbling and impact energy, creating a uniform coating ideal for small components like nails and bolts.

Physical Properties
| Property | Description |
| Density | ~7.85 g/cm³ (same as regular steel) |
| Melting Point | ~1,370–1,530°C (steel core); Zinc layer melts at ~419°C |
| Tensile Strength | Varies based on base steel, typically 250–550 MPa |
| Hardness | Depends on steel grade and coating thickness; Zinc coating hardness: ~50–150 HV |
| Thermal Conductivity | ~45–60 W/m·K (lower than pure steel due to zinc layer) |
| Electrical Conductivity | Lower than plain steel due to zinc coating |
| Corrosion Resistance | High resistance due to zinc barrier and sacrificial protection |
| Surface Appearance | Matte to shiny, depending on the galvanization method |
Chemical Properties
| Property | Description |
| Primary Elements | Iron (Fe) and Zinc (Zn) |
| Zinc Coating Composition | Primarily zinc (Zn), may contain small amounts of aluminum (Al) or lead (Pb) depending on the process |
| Reactivity with Acids | Reacts with strong acids (e.g., hydrochloric acid), dissolving the zinc layer and exposing the steel |
| Reactivity with Alkalis | Resistant to mild alkalis but can corrode in highly alkaline environments |
| Oxidation Resistance | High due to zinc layer, which forms a protective zinc oxide (ZnO) or zinc carbonate (ZnCO₃) film in atmospheric conditions |
| Galvanic Protection | Zinc acts as a sacrificial anode, corroding before the steel and preventing rust formation |
| Environmental Resistance | Performs well in most atmospheric conditions but can degrade in highly acidic or marine environments |
| Coating Stability | Zinc layer remains stable in normal conditions but can wear off over time due to mechanical abrasion or exposure to harsh chemicals |
Top Benefits
- Corrosion Resistance – The zinc coating protects steel from rust and oxidation, even in harsh environments.
- Durability – Galvanized steel has a long lifespan, often lasting 50+ years in regular conditions and 20–25 years in highly exposed environments.
- Cost-Effective – Compared to stainless steel or other coatings, galvanizing is an affordable way to extend the life of steel with minimal maintenance.
- Low Maintenance – Once applied, the zinc coating requires little to no upkeep, reducing long-term maintenance costs.
- Sacrificial Protection – Even if the coating is scratched, the zinc will corrode before the steel, preventing rust from spreading.

Common Uses in Industrial Manufacturing
| Industry | Common Applications |
| Construction | Structural beams, roofing, support frameworks, fences, handrails |
| Automotive | Vehicle frames, body panels, undercarriage components, exhaust systems |
| Industrial Machinery | Conveyor systems, storage racks, ductwork, processing equipment |
| Infrastructure | Bridges, guardrails, utility poles, pipelines |
| Fasteners & Hardware | Bolts, nuts, screws, nails, brackets |
| Electrical Equipment | Cable trays, electrical enclosures, metal conduits |
Parting Thoughts
At MISUMI USA, we hope this article has provided valuable insights into the benefits and applications of galvanized steel in industrial manufacturing. If you’re interested in learning more about other essential metals used in manufacturing, be sure to check out our articles on aluminum, aluminum alloys, copper, lead, and more.
Looking for high-quality galvanized steel components? Explore our product offerings here:
If you have any questions about selecting the right materials for your next project—including galvanized steel—our product experts are here to help. Contact us today!