If you think a caster wheel’s material doesn’t have much significance, think again. Caster wheel material influences the performance, durability, and safety of the caster wheel and its application.
Each material option, whether it be polyurethane, rubber, nylon, or metal, presents a unique set of advantages and limitations requiring careful consideration to ensure optimal functionality and longevity in usage.
Additionally, there are certain environments, floor conditions, and other factors that should be considered when choosing the right caster wheel material.
This article covers the different types of caster wheel materials, and the different environmental settings to consider.
Caster Wheel Materials: A High-Level Comparison
The type of caster wheel material you choose depends on different factors. A great place to start is to familiarize yourself with the features and strengths of each material, including load capacity, wear, and common application uses.
| METAL | RUBBER | POLYURETHANE | NYLON/PLASTIC | PNEUMATIC/SOLID/SEMI | |
| KEY FEATURES: | – High load capacity – High heat tolerance | Long-wearing | – Long-wearing – Higher loads than rubber | Chemical-resistant | – Rough or uneven surface – Great for outdoor applications |
Metal
With the highest capacity and tensile strength, metal, including steel and cast iron, is a popular choice for high heat applications.
Metal is also a great option for applications that require a high load capacity. Keep in mind that, despite rolling ease, metal caster wheels don’t offer floor protection on soft flooring.
Rubber
Another popular choice is rubber. Rubber is long-wearing and is often used on industrial equipment.
Rubber can also be molded on iron, aluminum, or plastic centers. This technique is referred to as “mold-in rubber,” and provides the soft tread of rubber with the hard backing of the wheel center.
Polyurethane
Polyurethane takes a liquid form and is casted onto centers made of cast iron, aluminum, or forged steel.
Polyurethane is also long-wearing, but it can also carry higher loads than rubber. It also offers protection from floor damage and is quiet when gliding on the floor.
Nylon/Plastic
Nylon/plastic materials, such as nylon, phenolic, or polyolefin, offer a wide range of advantages, including easy rolling, chemical resistance, and high load capacity.
Pneumatic/Solid/Semi
These types of caster wheel materials are often used on rough or uneven surfaces, as they allow for push and pull with ease.
This type of material can accommodate for larger wheel diameters for easier rolling, making it a great option for outdoor applications, such as grass.
Choosing the Right Material: 3 of Factors to Consider
Once you understand the key benefits of each caster wheel material, the second thing to consider is the caster wheel’s environment before making a final choice.
Understanding the operational context for selecting the most suitable caster ensures optimal performance and longevity.
Below are some common environments and settings where wheels are extensively utilized.
1. Industrial Settings
In industrial environments, caster wheels are subjected to heavy loads, rough surfaces, and often harsh operating conditions. They are utilized in material handling equipment such as carts, dollies, and platform trucks for transporting goods within warehouses, manufacturing facilities, and distribution centers.
These environments require caster wheels with high load-bearing capacities, excellent durability, and resistance to abrasion, chemicals, and extreme temperatures.
Steel material caster wheels can be a strong consideration for such an environment. However, if there are chemicals present in the facility, nylon can be considered for its chemical resistant properties.
2. Commercial Spaces
Caster wheels are integral to the smooth functioning of equipment in commercial spaces such as hotels, restaurants, hospitals, and retail stores.
They are used in service carts, medical equipment, display racks, and furniture, facilitating easy mobility and maneuverability.
Caster wheels in these settings offer quiet operations, non-marking properties, and are compatible with various flooring types to maintain aesthetics and prevent damage.
Polyurethane would be one of the best material choices for such commercial settings.
3. Outdoor Environments
Caster wheels are not limited to indoor use and are frequently employed in outdoor settings, such as construction sites, parks, and landscaping projects.
Outdoor caster wheels must withstand exposure to elements like moisture, UV radiation, and rough and uneven terrain conditions while maintaining reliable functionality.
Weather-resistant materials and robust construction are imperative to ensure longevity and performance in such environments.
One of the best choices to consider would be the pneumatic for its good handling on uneven surfaces, while providing some cushioning for many bumps along those types of roads.
Benefits of Caster Wheel Configuration
Caster wheels serve as indispensable components in a multitude of environments, facilitating mobility, and functionality across various sectors.
Finding the right material is a key step in selecting a caster wheel to ensure optimal performance and longevity while enhancing operational productivity and safety.
With many materials to choose from, like steel for heavy loads, polyurethane for softer surfaces, pneumatic for outdoor terrain, and many others, almost all scenarios are considered for your caster and wheel needs.
MISUMU is a great source for casters and wheels, with access to brands like Pegasus, Payson, and Blickle to meet your needs.
To learn more, explore MISUMI’S catalog of wheels and casters.