Coefficient of Friction for Metals and Materials | Table & Calculator

Understanding the coefficient of friction can help greatly when selecting materials for mechanical design, whether you’re working with metals, plastics, or composites. Engineers often reference a friction coefficient chart or a coefficient of friction table to determine how different surfaces interact under load. For example, the coefficient of friction steel on steel can vary depending on surface finish and lubrication, making accurate data critical in design calculations.

This guide provides a practical overview of friction values for common materials, along with a calculator to help simplify your project planning.

Friction Force Calculator

Friction Force Calculator
Formula Used:
F = μ × m × g

Coefficient of Friction Table

Coefficient of Friction Table

Common Material Combinations (Dry Conditions at Room Temperature)

Material Combination Static (μₛ) Kinetic (μₖ) Notes
Rubber on Dry Concrete — 0.6-0.85 Tire applications, high grip
Rubber on Wet Concrete — 0.45-0.75 Reduced friction when wet
Rubber on Dry Asphalt 0.9 0.5-0.8 Car tires, temperature dependent
Rubber on Wet Asphalt — 0.25-0.75 Significant reduction when wet
Rubber on Rubber 1.16 — Very high static friction
Steel on Steel (Clean) 0.5-0.8 0.42 Dry, clean surfaces
Steel on Steel (Grease) 0.16 — Lubricated surfaces
Steel on Steel (Oil) 0.11-0.23 0.081-0.084 Various oil types (castor, mineral, lard)
Aluminum on Aluminum (Clean) 1.05-1.35 0.4 High friction when clean
Aluminum on Aluminum (Lubricated) 0.3 — Significantly reduced with lubrication
Aluminum on Mild Steel 0.61 0.47 Common engineering combination
Cast Iron on Cast Iron 1.1 0.15 High static, low kinetic friction
Cast Iron on Cast Iron (Grease) — 0.07 Machine tool applications
Cast Iron on Steel 0.4 0.23 Common in machinery
Copper on Copper 1.6 — Extremely high static friction
Copper on Copper (Grease) 0.08 — Lubricated copper surfaces
Copper on Steel 0.53 0.36 Electrical contacts, bearings
Copper on Cast Iron 1.05 0.29 High static friction combination
Copper on Glass 0.68 0.53 Metal on glass interface
Brass on Steel (Clean) 0.51 0.44 Bearing applications
Brass on Steel (Lubricated) 0.11-0.19 — With grease or castor oil
Glass on Glass (Clean) 0.9-1.0 0.4 Clean, dry surfaces
Glass on Glass (Grease) 0.1-0.6 0.09-0.12 Lubricated glass surfaces
Glass on Metal 0.5-0.7 — Clean surfaces
Glass on Metal (Grease) 0.2-0.3 — Lubricated interfaces
Iron on Iron 1.0 — Pure iron surfaces
Iron on Iron (Grease) 0.15-0.20 — Lubricated iron surfaces
Nickel on Nickel 0.7-1.1 0.53 Clean nickel surfaces
Nickel on Nickel (Grease) 0.28 0.12 Lubricated nickel surfaces
Silver on Silver 1.4 — Clean precious metal surfaces
Silver on Silver (Grease) 0.55 — Lubricated silver contacts
Platinum on Platinum 1.2 — Precious metal contacts
Platinum on Platinum (Grease) 0.25 — Lubricated platinum surfaces
Wood on Wood (Clean) 0.25-0.5 — Varies with grain direction
Wood on Wood (Wet) 0.2 — Moisture reduces friction
Oak on Oak (Parallel grain) 0.62 0.48 Wood grain parallel
Oak on Oak (Cross grain) 0.54 0.32 Wood grain perpendicular
Wood on Clean Metal 0.2-0.6 — Construction applications
Wood on Wet Metal 0.2 — Moisture present
Wood on Concrete 0.62 — Construction interface
Wood on Brick 0.6 — Building materials
Leather on Oak 0.61 0.52 Belt drive applications
Leather on Metal 0.4-0.6 — Belt drives, brake applications
Leather on Cast Iron 0.6 0.56 Industrial belt systems
Ice on Ice (0°C) 0.1 0.02 Forms water film
Ice on Ice (-12°C) 0.3 0.035 Temperature dependent
Ice on Ice (-80°C) 0.5 0.09 Very cold conditions
Ice on Wood 0.05 — Very low friction
Ice on Steel 0.03 — Extremely low friction
PTFE on PTFE 0.04 0.04 Teflon on Teflon
PTFE on Steel 0.05-0.2 — Non-stick coating applications
Waxed Wood on Snow (Wet 0°C) 0.14 0.1 Skiing conditions
Waxed Wood on Snow (Dry) — 0.04 Optimal skiing conditions
Ski Wax on Snow (Wet 0°C) 0.1 — Wet snow conditions
Ski Wax on Snow (Dry 0°C) 0.04 — Dry powder snow
Ski Wax on Snow (Dry -10°C) 0.2 — Cold, dry snow
Nylon on Nylon 0.15-0.25 — Plastic on plastic
Nylon on Steel 0.4 — Plastic bearing applications
Polyethylene on Polyethylene 0.2 — Low friction plastic
Polyethylene on Steel 0.2 — Consistent with/without grease
Polystyrene on Polystyrene 0.5 — Consistent with/without grease
Polystyrene on Steel 0.3-0.35 — Plastic on metal interface
Plexiglas on Plexiglas 0.8 — Acrylic plastic surfaces
Plexiglas on Steel 0.4-0.5 — Consistent with/without grease
Graphite on Steel 0.1 — Solid lubricant
Graphite on Graphite 0.1 — Self-lubricating material
Graphite on Graphite (Vacuum) 0.5-0.8 — Higher friction without air/moisture
Tungsten Carbide on Steel 0.4-0.6 — Hard material applications
Friction Level Guide:
Low Friction (μ < 0.3)
Medium Friction (0.3 ≤ μ < 0.7)
High Friction (μ ≥ 0.7)


Note: Values are approximate and can vary significantly based on surface conditions, temperature, humidity, load, and material quality. Always consult specific material data for critical applications.

Coefficient of Friction Equation/Formula

The coefficient of friction (μ) is a dimensionless value that describes the resistance to sliding between two surfaces. It is calculated using a simple formula:

μ = Fₓ / Fₙ

Where:

  • μ = coefficient of friction
  • Fₓ = frictional force (in newtons or pounds)
  • Fₙ = normal force (the force perpendicular to the surfaces in contact)

The frictional force is the force resisting motion between surfaces, while the normal force is typically the object’s weight or any force pressing the surfaces together. By dividing the frictional force by the normal force, this equation gives you a value that helps predict how difficult it will be to slide one material across another.

There are two types of friction coefficients commonly used:

  • Static coefficient of friction (μₛ): Used when the object is at rest and just about to start moving.
  • Kinetic coefficient of friction (μₖ): Used once the object is already in motion.

Example:
If it takes 10 N of force to start moving an object that weighs 20 N, then:
μ = 10 / 20 = 0.5

Parting Thoughts

If you have questions about selecting the right materials or tackling a specific design challenge, our team of product experts and engineers is here to help. MISUMI USA offers a wide range of industrial and automation components—including aluminum extrusions, linear shafts, and metal materials—to support your manufacturing needs. Be sure to explore our extensive catalog, and don’t forget to visit the MechLab Blog for more helpful resources. You’ll find data-driven tools like our Linear Thermal Expansion Coefficient Chart, Metal Melting Points Chart, and other technical calculators to support your next project.

Author: Scott Bredemann | Updated: 8/15/2025

Disclaimer:
The content on this webpage is for informational purposes only. MISUMI makes no guarantees, expressed or implied, regarding the accuracy, completeness, or validity of the information. Performance parameters, tolerances, designs, materials, or processes should not be assumed to reflect third-party suppliers’ or manufacturers’ deliverables within MISUMI’s network. Buyers are responsible for specifying their part requirements