The choice between a collaborative robot (cobot) and an industrial robot depends on the needs of your application, including factors like safety, flexibility, complexity, and the operational environment.
This article showcases and compares the benefits of each.
Benefits of Collaborative Robots

Cobots have benefits over a traditional industrial robot, from human-robot collaboration to costs.
Human-Robot Collaboration
Cobots are designed to work safely alongside humans without the need for safety cages or barriers (when following safety protocols).
If your application involves close cooperation between humans and robots, a cobot is ideal. Cobots are more common in the packaging and warehouse automation industries for this reason. For example, in warehousing, a cobot can assist a worker with lifting or assembly tasks.
Flexibility and Adaptability
Cobot teaching software is generally more flexible and easier to reprogram or reconfigure for different tasks. If you need a robot that can quickly adapt to new production needs or tasks, a cobot is a good choice.
In addition, the software is often built-in, whereas an industrial robot would generally require programming or specialized knowledge on how to teach the robot.
Flexibility and adaptability of floor space should also be considered as industrial robots require fencing and safety infrastructure. If your process is quickly changing or floor plans are updated frequently, an anchored industrial robot and safety fencing take more time to move, as well as reprogram.
Small batch manufacturing companies and smaller packaging and assembly startups are starting to use more cobots. This is especially true if the company is without dedicated robotics engineers who need a robot that operators can easily program and deploy.
Smaller and Limited Floor Space
Small-scale operations or environments with limited floor space make a cobot an ideal choice.
Cobots are often smaller and lighter than industrial robots, making them easier to move and deploy in various workspaces. If you have limited space or need to deploy a single robot in multiple locations frequently, cobots are a good option.
Costs
Cobots tend to be less expensive than industrial robots, both in terms of initial cost and maintenance. For smaller companies or those with a limited budget, cobots provide an affordable solution.
When considering the programming and software costs and the safety infrastructure required of an industrial robot, the numbers lean even more in favor of cobots.
Benefits of Industrial Robots

With so many advantages of cobots, that’s not to say industrial robots are going away.
Industrial robots have their place in the automation space and have consistently shown their value across industries.
Here are the benefits of industrial robots.
High-Speed, High-Precision, or High-Volume Production
Industrial robots are generally faster, more precise, and better suited for high-volume, repetitive tasks.
If your application requires high performance in terms of speed and accuracy, an industrial robot is the better choice. Cobots by design are not going to have the rigidity, precision, or throughput of an industrial robot.
Heavy Payloads
Industrial robots are designed to handle larger payloads and are capable of lifting heavier objects. If you need a robot to handle large parts or materials, industrial robots can typically handle much greater weight than cobots.
High-Duty Cycles
Industrial robots are designed to work on a single task flawlessly without error. They are also built to continuously endure long hours of high-intensity operation at a single task.
If your production process requires a robot to run for long periods without interruption, an industrial robot will be more durable and suited for the task.
Special Environments
Industrial robots are great at precision tasks in special environments such as extreme temperatures, contamination risks, or high-pollution areas. They are often used in processes that require robust durability and safety features.
Industrial robots are more often found in food packaging where robots need to be NSF-rated and subject to harsh chemicals in washdown.
As of right now, cobots are generally not rated to handle washdown environments without third-party additions such as coatings or paint to the cobot. If a person doesn’t need to be there, such as in a welding, painting or hazardous material environment you lose out on the main advantage that a cobot offers.
Cobots Provides Flexibility, While Industrial Robots Are Designed for High Performance
To sum it up, use a cobot when you need human interaction, flexibility, ease of programming, and smaller-scale or less precise tasks. Use an industrial robot when you need high performance: speed, precision, heavy payload handling, and long-duty cycles.
Ultimately, the decision comes down to the balance between automation requirements, safety, environment, flexibility, and cost.
MISUMI offers a number of components for end-of-arm tooling, aluminum extrusion for safety fencing, light curtains, sensors, stop buttons, and brackets and plates for mounting and installing your robot.