Laser welding metal up close

All About Laser Welding

Author: Scott Bredemann

Updated: 03/6/2025 | Read Time: 4mins

Unlike traditional welding techniques, laser welding uses a focused beam of light to fuse materials together, allowing for incredibly precise welds with minimal impact on surrounding areas. This makes it ideal for delicate components, intricate assemblies, and high-speed production lines.In this guide, we’ll break down everything you need to know about laser welding—how it works, the different types, its advantages and limitations, and where it’s used.

What is Laser Welding?

Laser welding generates intense heat in a very concentrated area, allowing for deep penetration and minimal heat distortion. It works by directing a high-energy laser beam at the materials being joined. The heat from the laser melts the surfaces, and as they cool, they fuse together to create a strong, seamless bond. Because the laser is so precise, it’s ideal for applications where traditional welding might cause warping or excessive heat damage, especially in delicate components or thin materials.

There are several types of lasers used in welding, each suited for different applications. Fiber lasers, CO₂ lasers, and Nd:YAG lasers are some of the most common, with fiber lasers becoming the industry standard due to their efficiency and ability to work with a wide range of metals. Laser welds are quite often used in automotive manufacturing, medical device production, or microelectronics, due to speed and accuracy compared to conventional welding techniques.

Laser Welding Gun

Types of Laser Welding

The table below highlights the most common types of laser welding, listed by popularity and industrial use:

Type of Laser WeldingDescriptionBest For
Fiber Laser WeldingUses a fiber-optic cable to deliver a highly efficient and precise laser beam.High-speed manufacturing, automation, and a wide range of metals
Keyhole Laser WeldingCreates a deep, narrow weld by vaporizing material and forming a keyhole.Deep penetration welding, high-strength structural joints
Conduction WeldingUses lower laser power to create shallow, smooth welds without keyhole formation.Thin materials, aesthetic welds
Deep Penetration WeldingUses a high-energy laser to achieve strong, deep welds in thick materials.Heavy-duty applications, structural components
Nd:YAG Laser WeldingUses a neodymium-doped yttrium aluminum garnet (Nd:YAG) crystal as the laser medium.Precision welding, medical devices, aerospace components
Laser-Hybrid WeldingCombines laser welding with another welding process (e.g., MIG) for enhanced strength and efficiency.Thick materials, high-speed production in automotive and shipbuilding
CO₂ Laser WeldingUses a gas-based laser to generate a high-energy beam, but is being replaced by fiber lasers.Non-metal materials, some legacy industrial applications
Table of Laser Welding Types

Steps to Perform Laser Welding

Here’s a basic step-by-step guide to the process:

  1. Choose the Right Laser Type – Select the appropriate laser (fiber, CO₂, Nd:YAG, etc.) based on the material, thickness, and application.
  2. Prepare the Materials – Clean the surfaces to remove any dirt, oxidation, or contaminants that could weaken the weld.
  3. Secure the Workpieces – Use clamps or fixtures to hold the materials in place to ensure precision and avoid misalignment.
  4. Adjust Welding Parameters – Set the correct laser power, speed, focal point, and shielding gas based on the material and weld type.
  5. Use Proper Shielding Gas – Apply gases like argon or nitrogen to protect the weld from oxidation and ensure a clean joint.
  6. Initiate the Laser Beam – Activate the laser and begin the welding process, either manually or through an automated system.
  7. Monitor the Weld – Observe the weld pool to ensure proper penetration and fusion; adjust settings if needed.
  8. Allow the Weld to Cool – Let the welded joint solidify naturally or use controlled cooling for stress reduction.
  9. Inspect the Weld – Check for defects such as cracks, porosity, or incomplete fusion using visual inspection or non-destructive testing methods.
  10. Post-Weld Cleaning & Finishing – Remove any excess material or oxidation if necessary for cosmetic or functional purposes.
Laser Welding System Diagram

Laser Welding vs. Other Types of Welding

Welding MethodPrecisionHeat InputSpeedLimitations
Laser WeldingVery HighLowVery FastHigh equipment cost, requires precise joint preparation
TIG (GTAW) WeldingHighMediumSlowSlow process, requires skilled operator
MIG (GMAW) WeldingMediumHighFastMore heat input, potential for spatter
Stick (SMAW) WeldingLowHighMediumProduces slag, not ideal for thin materials
Resistance Spot WeldingMediumLowVery FastLimited to lap joints, not for thick materials
Plasma Arc WeldingVery HighLow-MediumFastComplex setup, expensive
Table of Laser Welding vs. Other Types

Parting Thoughts

We hope you found this article informative and valuable as you continue to expand your laser welding knowledge. At MISUMI USA, we are committed to providing you with resources to support your business and projects. Be sure to explore our other articles for more insights into the manufacturing world. Additionally, take a look at MISUMI USA’s extensive online catalog of standard and configurable parts designed to meet your welding needs. Examples include:

Welding Supplies

Electric Welders

Welding Rods

If you have any questions about laser welding or other industrial manufacturing needs, don’t hesitate to reach out to our product experts for assistance.