Metals and nonmetals make up most of the materials we use every day, and they behave very differently. Some bend easily and conduct electricity, while others are brittle or act as good insulators. These differences come from basic traits in how the elements are structured. Understanding what sets metals and nonmetals apart gives you a better sense of why certain materials are chosen for tools, wiring, containers, machinery, and countless other uses.
What are Metal Elements?
Taking a look at Metal elements – they make up most of the periodic table, stretching across the center and left side. These elements share a set of practical traits: they conduct heat and electricity well, can be shaped or bent without breaking, and often have a natural shine. Because of these properties, metals are used for wiring, machinery, structural parts, and countless everyday items. Their behavior on the periodic table is consistent too—most metals react by giving up electrons, which helps explain how they bond and why they’re so useful in manufacturing and engineering. Familiar examples include iron, copper, and aluminum.
What are NonMetals?
Nonmetal elements appear mostly on the right side of the periodic table, with a few exceptions like hydrogen. They tend to behave very differently from metals. Most nonmetals do not conduct heat or electricity well, and many are brittle if they’re solid. They also lack the shine and flexibility associated with metals. In chemical reactions, nonmetals typically gain or share electrons, which influences how they form compounds. These elements play essential roles in everyday materials and processes—carbon forms the basis of plastics and living organisms, oxygen supports combustion and respiration, and nitrogen makes up most of the air we breathe.
Differences Between Metals and Nonmetal Elements
Metals and nonmetals differ in several ways that are easy to see both in the periodic table and in real-world use. Metals, which dominate the left and center of the table, are usually good conductors of heat and electricity, can be shaped without breaking, and often have a reflective shine. Nonmetals, found mainly on the right side, tend to be poor conductors, dull in appearance, and brittle when solid. Their chemical behavior is different as well—metals typically give up electrons during reactions, while nonmetals usually gain or share them. These contrasting traits explain why metals are often chosen for structural and electrical applications, and why nonmetals are common in gases, insulators, and many types of chemical compounds.
Real World Applications of Each
Metals and nonmetals are used in different ways because their properties lend themselves to specific jobs. Metals are strong, durable, and good at carrying heat and electricity, which makes them well-suited for structural frames, automotive parts, machine components, electrical wiring, cookware, and tools. Aluminum, for example, is common in transportation and packaging, while copper is relied on for electrical systems.
Nonmetals play a different role. Many act as insulators, react in controlled ways, or form the basis of everyday materials. Carbon is essential for plastics, composites, and biological systems. Oxygen supports combustion and is used in medical and industrial settings. Nitrogen is important in fertilizers and forms the bulk of the air. Sulfur, chlorine, and other nonmetals appear in water treatment, pharmaceuticals, and chemical manufacturing. These uses reflect how nonmetals contribute in areas where flexibility, reactivity, or stability matter more than strength or conductivity.
Parting Thoughts
MISUMI USA carries a wide range of industrial manufacturing components – including metal screws, and plastic screws – for your next project or machine fix. If you have any questions about materials (metals or non-metals), feel free to connect with our product experts, and engineers. Also, if you are looking for more insights be sure to check out our other blog articles, including: What are Metalloids, Aluminum in Manufacturing, What is Mild Steel?, and more.
Author: Scott Bredemann | Updated: 12/4/2025
Disclaimer:
The content on this webpage is for informational purposes only. MISUMI makes no guarantees, expressed or implied, regarding the accuracy, completeness, or validity of the information. Performance parameters, tolerances, designs, materials, or processes should not be assumed to reflect third-party suppliers’ or manufacturers’ deliverables within MISUMI’s network. Buyers are responsible for specifying their part requirements