MISUMI hardness scale guide

Understanding Shore Hardness Scales: Shore A, Asker C, & Asker F Explained

Published on
December 18, 2024

2 min read

Polyurethanes and rubbers can come in many different types. Each type will have its own unique properties, but one thing that they have in common is how their hardness is measured.

The most common type of measurement for the hardness of urethanes and rubbers is the Shore A scale, which is the hardness measured by using a type-A durometer. A durometer is the instrument used to measure the hardness of a material.

This measures the resistance of rubbers or urethanes toward indentation. Hardness of materials softer than urethane and rubber is measured by Asker type C/E, and even softer than that can be measured by the Asker F scale.

What are the Shore Hardness Scales?

The Shore A hardness scale is a way to measure the hardness of rubbers and polyurethanes. The same type of rubber with a different Shore hardness could have different properties, such as tensile strength, specific gravity, temperature resistance, and elongation. A general guideline is that if the hardness value is higher, the tensile strength will increase and elongation percentage will decrease.

The Asker C hardness scale can be used to measure materials softer than standard polyurethanes or rubbers. The hardness is measured using a spring-type hardness tester. This scale is commonly used for softer sponge/foam materials. The higher the value on the Shore A scale and Asker C scale, the harder the material is.

The Asker F hardness scale is used when materials are even softer than sponge or foam materials. This is commonly used to measure shock-absorbing gels, with the characteristic of recovering their original shape after compression.

Note: The Shore D scale is commonly used to measure the hardness of plastics, though the resin materials manufactured by MISUMI do not have a Shore D hardness associated with them.

Benefits of Using the Scales

Materials have different properties at different hardnesses, so the different hardness scales can be used to determine which is best for the application.

  • Shore A Hardness: Rubber/Urethane
  • Asker C Hardness: Sponge/Foam
  • Asker F Hardness: Softer gel-like materials
Hardness scale chart by MISUMI

The Shore A scale is used for its wide range of hardness values. Within the products sold by MISUMI, the highest hardness value on the scale is A95, equivalent to a golf ball hardness. The lowest hardness value can be as low as A15, which is slightly softer than a rubber band.

Sponges on the Asker C scale commonly range from C1 to C35, which would only be around A1-A15 on the Shore A scale. The wider range on the Asker C scale allows you to choose a more precise hardness for these materials compared to the Shore A scale.

The Asker F scale is used when materials are softer than either the Shore A or Asker C scales can be used for. Materials measured with Asker F are typically found on products that are used for their shock absorption properties.

Using a Durometer to Measure Shore Hardness

A durometer is used to measure the hardness of a material by measuring the height that the needle part on the durometer indents the material. The more the needle pushes into the material, the lower the hardness. A number between 0-100 will be displayed on the durometer, which corresponds to the Shore hardness scale.

Configurable Polyurethanes and Rubbers

MISUMI offers a wide range of polyurethane and rubber products at many different Shore A hardness values. Links to some of these products can be found below.

About the Author

Brian Hettinger

Brian Hettinger is a product engineer at MISUMI. He started on the Custom Components team in 2018 as his first role out of college and assisted with the launch of meviy. He now supports the growth of MISUMI’s standard made-to-order products.

You may also like these