Lead screws are used in machines and assemblies where rotary motion needs to be converted into controlled linear movement. A motor, handwheel, or other rotating input turns the screw, and the mating nut moves along the threads to push, pull, lift, or position a load. This makes lead screws useful in everything from manual adjustment mechanisms to automated positioning systems. Unlike some linear motion components that are built mainly for speed or high efficiency (think ball screws), lead screws are often selected because they are simple, durable, and relatively easy to integrate.
This article covers how lead screws work, the main types used in mechanical design, and their key advantages,
What Are Lead Screws?
A lead screw is a threaded shaft used to produce straight-line motion in a mechanical assembly. It works with a matching nut, carriage, or threaded component that follows the screw’s thread path. As one part rotates, the other part moves along the screw’s axis, creating linear travel that can be used for positioning, lifting, clamping, opening, closing, or adjusting a machine element.
The term “lead screw” usually refers to a screw designed for motion rather than fastening. Unlike a standard bolt, which is mainly used to hold parts together, a lead screw is intended to move a load over a controlled distance. The thread geometry, screw diameter, lead, nut material, and support method all affect how much force the screw can handle, how quickly it moves, and how accurately it can position a component.
Common Types of Lead Screws
Lead screws can be grouped by thread shape, lead, number of starts, material, and accuracy. Each type affects motion differently, including speed, load capacity, friction, wear, backlash, and maintenance needs.
Acme Lead Screws
- One of the most common lead screw types used in industrial equipment.
- Uses a trapezoidal thread form with a broad crest and root.
- Offers good thread strength and wear resistance.
- Easier to manufacture than square threads.
- Often used in machine slides, clamps, linear actuators, vises, lift mechanisms, and manual adjustment systems.
- A practical choice when the application needs reliable motion but does not require the high efficiency of a ball screw.
Trapezoidal Lead Screws
- Similar to Acme lead screws but based on metric thread standards.
- Uses a trapezoidal thread profile with metric dimensions and geometry.
- Common in machinery, automation equipment, and positioning systems.
- Often selected when the rest of the machine design uses metric components.
- Provides strong, guided linear motion with a simple screw-and-nut arrangement.
Square Thread Lead Screws
- Uses a thread profile with nearly square-shaped flanks.
- Can be more efficient than Acme or trapezoidal threads because it reduces radial force between the screw and nut.
- Converts more input torque into useful linear force.
- More difficult and expensive to manufacture.
- Less common in standard machine components.
- Usually used when efficiency is important enough to justify the added manufacturing complexity.
Buttress Thread Lead Screws
- Use an asymmetric thread profile designed to carry high force in one primary direction.
- Common in presses, clamps, jacks, lifting mechanisms, and heavy-duty actuators.
- Useful when axial load is mostly one-directional.
- Less suitable when the application needs equal performance in both directions.
- Thread direction must match the direction of the applied load.
Lead Screws vs. Ball Screws
A lead screw may be the better choice when the application needs controlled movement at a lower cost, especially if the duty cycle is intermittent or the speed is relatively low. A ball screw is usually the better choice when the system needs high efficiency, frequent cycling, faster travel, or tighter positioning control over time.
| Factor | Lead Screws | Ball Screws |
|---|---|---|
| Contact Method | Use sliding contact between the screw and nut. | Use rolling contact through recirculating ball bearings. |
| Efficiency | Lower efficiency because of higher sliding friction. | Higher efficiency because rolling friction is much lower. |
| Cost | Typically lower cost and simpler to integrate. | Usually higher cost due to more complex construction. |
| Speed | Better suited for slow to moderate-speed movement. | Better suited for faster linear motion and frequent cycling. |
| Input Torque | Generally require more torque to move the same load. | Can move loads with less input torque. |
| Back-Driving | May resist back-driving depending on lead angle, friction, lubrication, and load. | More likely to back-drive because of low friction. |
| Maintenance | Can be simple to maintain, especially in lower-duty applications. | Often require careful lubrication and protection from contamination. |
| Precision | Suitable for moderate positioning needs, but backlash should be considered. | Commonly used where high repeatability and low backlash are required. |
| Common Uses | Manual adjustments, clamps, fixtures, lifts, guards, and simple actuators. | CNC machines, robotics, automated equipment, and high-duty positioning systems. |
| Best Fit | Cost-sensitive applications that need controlled motion at moderate speed. | Applications that need high efficiency, speed, repeatability, or frequent motion. |
Conclusion
Lead screws are a practical option for converting rotary motion into controlled linear movement, especially in applications where simplicity, mechanical advantage, cost, and positioning control are important. The right selection depends on how the screw will be used, including load direction, speed, travel length, duty cycle, backlash requirements, mounting support, lubrication, and the operating environment. In many designs, the best performance comes from choosing the proper screw type and pairing it with the right nut material, guides, bearings, and drive method.
Browse Lead ScrewsMISUMI USA carries a wide range of linear motion parts and components including linear shafts, linear actuators, ball screws, and more. If you have any questions about linear motion concerns for your next project or fix, please feel free to contact our product experts and engineers. For more insights about lead screws and other manufacturing-related articles, be sure to check out Lead Screw Applications: Examples and Use Cases and lead screws on the MISUMI Mech Lab blog.