How to Select the Right Bearing Part 5

Published on
October 5, 2021

7 min read

Bearing Preload and Rigidity

This post is a continuation of the Koyo Bearings series, you can find the original post on their website here.

In Part 4, we explained about bearing limiting speed, running accuracy, and fits.

To catch up on the previous Bearing Selection blog posts, read each one below:

How to Select the Right Bearing Part 1: The Order of Priority for Selecting Bearings and the Types of Bearings

How to Select the Right Bearing Part 2: Selecting Bearing Arrangement

How to Select the Right Bearing Part 3: Bearing Dimensions and Service Life

How to Select the Right Bearing Part 4: Bearing limiting speed, running accuracy, and fits

In Part 5, we will explain bearing preload and rigidity as measures for whether the bearing type you chose was appropriate.

Generally, bearings are operated with a certain amount of proper clearance allowed. For some applications, however, bearings are mounted with axial load of such magnitude that the internal clearance will be slightly negative. This axial load is referred to as “preload”.

In this part, we will introduce you to information relating to preload and rigidity.

Table 1: Bearing Selection Check List

2. Amount of displacement of the shaft center and the contact condition of the bearing rolling elements caused by preload

The contact condition between the rolling elements and the bearing rings (or the races) differs depending on whether there is internal clearance in the bearing or preload is applied to the bearing. Allow us to explain the contact condition using radial bearings as an example.

1) If there is internal clearance in the bearing

If there is internal clearance in the bearing, the largest load will be placed on the rolling elements located nearest the direction of the load.
This load induces a slight elastic deformation at the point where the rolling elements come in contact with the bearing rings. When the load is removed, it returns to normal and the elastic deformation disappears (see Figure 1).

Fig. 1: Where elastic deformation is induced

However, at the rolling elements located on the opposite side of the load direction, no load is applied and no elastic deformation occurs (see Figure 2).

Fig. 2: Where no elastic deformation is induced

Because of this difference in elastic deformation due to the position of the rolling elements, the position of the shaft center (i.e. bearing center) changes slightly (see Figure 3a).
If the direction of the load changes, the shaft center moves in other direction, causing vibration.

2) If preload is applied to the bearing

Applying preload causes the bearing’s internal clearance to become slightly negative, causing a greater number of rolling elements to come in contact with the inner and outer rings. The difference of the elastic deformation among rolling elements contacting with the rings becomes smaller.
As a result, the amount of displacement in the bearing shaft center position decreases (see Figure 3b).

Fig. 3: Amount of displacement in shaft center position

Applying preload to the bearing and decreasing the amount of displacement in the shaft center position in this manner is called increasing shaft rigidity.

Furthermore, with roller bearings, the amount of elastic deformation caused by the load is smaller than with ball bearings.

3. Method of preloading

Preloading can be done by either position preloading or constant pressure preloading (see Table 3).

AdvantagesDisadvantages
1.Position preloadingWith the same amount of preload, the displacement is smaller, relative to the load, than constant pressure preloadingThe amount of preload changes under the influence of assembly conditions, the centrifugal force during rotation, and a rise in temperature
2.Constant pressure preloadingThere is little fluctuation in the amount of preload during rotation, and a stable amount of preload is maintainedWith the same amount of preload, the displacement is bigger, relative to the load, than position preloading
Table 2: Position preloading and constant pressure preloading

The structures of the two different preload methods are shown below (see Figures 4 and 5).

Fig. 4: Position preloading structure
Fig. 5: Constant pressure preloading structure

4. Bearing arrangement

Arrangement methods of angular contact ball bearings and tapered roller bearings

With angular contact ball bearings and tapered roller bearings, an axial load is applied for the preloading.


In this situation, back-to-back arrangement is most often used (see Figure 6).


This is because with back-to-back arrangement the load center position dimensions become larger and the amount of displacement in the bearing shaft center position decreases (the rigidity increases).

Fig. 6: Bearing (tapered roller bearing) arrangement and load center position

5. The relationship between preload and rigidity

The load being applied on a bearing induces the elastic deformation to occur at the point where the rolling elements come in contact with the bearing rings. For this reason, the amount of displacement of the bearing increases along with the increase in the applied load.


For angular contact ball bearings and tapered roller bearings, the relationship between the axial load (preload) and the amount of displacement in the axial direction (rigidity) is used to apply an axial load needed for the preloading (see Figure 7).

Fig. 7: The relationship between axial load (preload) and amount of displacement in the axial direction (rigidity)

See the following for a detailed explanation:
Preload and rigidity – Ball & Roller Bearings Catalog
Rigidity and preload of bearings – Precision Ball & Roller Bearings for Machine Tools

6. Amount of preload

1) Points to note when setting the amount of preload

It is important to set the amount of preload appropriately in consideration of factors such as the rotational speed and lubrication conditions.
If you increase the amount of preload, the rigidity of the bearing will be raised, but it will have a significant impact on the bearing service life, the increase in temperature, and so on.

2) Preload amount of a bearing for a machine tool spindle (example)

As for high-precision matched pair angular contact ball bearings for use in machine tool spindles, JTEKT provides these ready-matched (see Figure 8).

Fig. 8: A matched pair angular contact ball bearing

With these high-precision matched pair angular contact ball bearings, so that you can freely select the amount of preload best suited to your application, JTEKT endorses four types of standard preload: slight preload (S), light preload (L), medium preload (M), and heavy preload (H). (See Table 4.)

Table 4: Standard preload of high-precision matched pair angular contact ball bearings

Amount of preload – Ball & Roller Bearings Catalog

Conclusion

To increase running accuracy or raise rigidity, it is possible to apply preload to the bearing.

  1. The preload method can be position preloading or constant pressure preloading, depending on the application.
  2. With angular contact ball bearings and tapered roller bearings in back-to-back arrangement, the relationship between the axial load (preload) and amount of displacement in the axial direction (rigidity) is used to apply the appropriate rigidity.
  3. The amount of preload should be set at such a level as not to negatively impact the service life, temperature increase, etc. Applying more preload causes a larger increase in temperature and can potentially cause a bearing failure (seizure). This means that selecting the appropriate preload is very important.

Explore Koyo Bearings’ line of products at this link.

Works Cited
Koyo Bearings. (2020, May 29). Bearing Trivia. Retrieved from Koyo Bearings: https://koyo.jtekt.co.jp/en/2020/05/column02-05.html

About the Author

Carlicia Layosa

Carlicia is the Marketing Automation Manager at MISUMI. She holds a bachelor's degree in Mechanical Engineering and a master's degree in Energy Engineering from the University of Illinois at Chicago. She is a Certified SOLIDWORKS Associate, Marketo Certified Expert, and is passionate about education and training.

You may also like these