Browse Topic

piezo stage misumi

Piezo Stages: Your (Not So) Secret Weapon for High Resolution Imaging 

January 6, 2026 · Andrew Barendregt

Discover how piezo stages achieve nanometer precision, fast focus changes, and superior imaging accuracy.

Direct Drive Linear Motor - Blog Post

5 Semiconductor Applications Where Direct Drive Linear Motor Stages Excel

January 30, 2025 · Andrew Barendregt

Learn why direct drive linear motor stages are preferred over leadscrew-driven motors in the semiconductor industry.

The Laser’s Edge for Semiconductor Fabrication

April 23, 2024 · Andrew Barendregt

Enhancing Semiconductor Manufacturing Precision with Smart LAC Laser Autocollimators There are no smartphones, tablets, or modern appliances without…

The Optics of Flow Cytometry

March 12, 2024 · Andrew Barendregt

Flow cytometry, a powerful technique in cell biology and medical diagnostics, intricately combines fluidics, optics, and electronics to…

Manual and Motorized Drive Stages

July 26, 2022 · Andrew Barendregt

Positioning stages are differentiated by the means used to control the position of the stage platform, either by…

Measuring Parallelism with a Smart Laser Autocollimator

November 23, 2021 · Andrew Barendregt

Laser Autocollimators are useful for measuring flatness and parallelism between two planes.  This is often an easy application,…

Guide Mechanisms for Precision Positioning Stages

December 4, 2019 · Andrew Barendregt

Most stages employ three primary types of guide mechanism for their precision positioning stages. Dovetail, Linear Ball, and…

Setting the Stage: Four Steps in Stage Selection

November 13, 2019 · Andrew Barendregt

Selecting the right stage for your application can seem like a daunting task, especially with the variety available.…

A customer-modified MISUMI High Precision Stage

Q&A: How To Reverse the 5 Stage Stepper Motor on a MISUMI High Precision Stage

January 20, 2015 · Andrew Barendregt

Question: Dear MISUMI Engineering Team: Hi, we purchased a MISUMI single axis high precision stage, but then needed…