Piezo stages are an actuation technology that has revolutionized high-resolution imaging but remains underrated. Instead of your typical “move – stop-image” motion, piezo stages work by moving continuously while imaging with nanometer accuracy.
The way they allow extremely fast and precise focus changes is why they are commonly used in optics, microscopy, scientific, and semiconductor applications.
This article breaks down why piezo stages can be your “secret weapon” for achieving unparalleled imaging precision.
What Are Piezo Stages?
Also known as “piezoelectric” or “nano-positioning” stages, piezo stages are precision motion devices driven by piezoelectric actuators to move objects with nanometer to sub-nanometer resolution.
The piezoelectric actuator is sometimes called a “piezo motor” because it converts electrical energy to mechanical energy like a motor does. However, it isn’t a traditional motor that consists of a rotor and stator; it’s a material (often a ceramic or crystal) that changes size or shape when voltage is applied to it. This is referred to as the “inverse piezoelectric effect.”
These minuscule movements need to be directed into a motion we can use in the laboratory, or in our production process. Mechanical elements like flexures are designed to direct such movement into this desired motion. The result is a high precision positioner that gives us unparalleled capabilities for imaging, and other applications.
Common High-Resolution Imaging Applications
Due to nanometer-scale resolution, repeatability, and fast response time capability, piezo stages are commonly used in the following applications when precision imaging matters.
Microscopy Applications
Piezo stages allow for motion control at the same scale as to what is being imaged, which is why they are common in microscopy applications.
Modern microscopes are so powerful that a tiny shift can throw the image out of focus, undetected vibrations can blur the picture, and a slight drift over time can ruin a long-form experiment.
Piezo stages solve this by enabling us to make extremely gentle, smooth, and fast movements to nullify these factors. It can adjust focus in milliseconds and move through many focus levels quickly and accurately.
Here is a high-level breakdown of how piezo stages are used in different microscopy applications:
| Microscopy Application | Piezo Stage Use Case |
| AFM / STM | Atomic-scale scanning and feedback |
| Optical Microscopy | Fast, vibration-free focusing and Z-stacking |
| Super-Resolution Imaging | Sub-diffraction positioning and drift control |
Industrial and Scientific Applications
Piezo stages are also used in applications where precision, speed, and stability are critical, especially in industrial and scientific applications.
In precision manufacturing, misalignment of micro-scale parts, maintaining tight tolerances, and minimizing vibration during assembly or inspection are common challenges.
Piezo stages help solve these challenges by achieving fine alignment of components, nanometer-scale positioning during inspection, and active compensation for thermal drift. That’s why industries like semiconductor manufacturing, photonics and optics assembly, and MEMS fabrication rely on piezo stages.
In research labs, piezo stages are used when researchers need controlled, repeatable motion at nanometer or sub-nanometer scales while simultaneously measuring a signal.
For example, a typical experimental setup might include:
- A sample mounted on a stage
- Sensors measuring forces, light, current, or displacement
- A feedback loop adjusting position in real time.
The piezo stage would sit inside this loop and instead of “moving here and stopping,” the stage is constantly making tiny, continuous corrections based on sensor feedback (e.g., if a material expands due to temperature changes, the piezo stage will compensate for this).
Other applications include laser processing and beam steering, offering real-time fine positioning and stable, high-precision optical alignment.
Top Advantages of Piezo Stages for Imaging
To summarize the main benefits of piezo stages for imaging, it all comes down to precision and speed, versatility, and reliability and control.
Precision and Speed
High dynamic performance and millisecond, or even microsecond, step and settle times give piezo stages a clear advantage over traditional motorized stages allowing for faster data acquisition, high-throughput scanning, and precise capture of objects.
Versatility
Piezo stages offer versatility due to their sub-nanometer precision, high speed, and rapid response capabilities. They offer precision motion across multiple axes (X, Y, Z, rotation) for nanoscale positioning, with configurations for vacuum, non-magnetic needs, or heavy loads, making them adaptable for a wide range of microscopy applications, semiconductor manufacturing, and scientific lab needs.
Reliability and Control
Piezo stages offer excellent long-term stability and high repeatability with backlash-free motion, ensuring that specific points of interest can be revisited for quantitative analysis or time-lapse studies.
Piezo Stage Challenges to Consider
Okay, now some downsides. Important considerations when choosing to implement a piezo stage include:
- Cost
- Complexity
- Support and Maintenance
Upfront & System Cost
Piezo stages are much more expensive than traditional motorized stages. In fact, a piezo stage that moves only 100-300 microns can cost as much as a motorized stage with tens or hundreds of millimeters of travel.
And the stage itself is only part of the expense. You’ll also have to consider the cost of piezo amplifiers/drives, feedback sensors, controllers, and cabling.
Integration Complexity
Piezo stages can require high-voltage amplifiers, closed-loop control for precision work, and careful tuning. Adoption of a piezo stage requires not only mechanical expertise but also control expertise to ensure smooth integration.
Support and Maintenance
Piezo systems are highly integrated, so you’ll want to choose a supplier that can provide technical support, integration guidance, and quality documentation.
Fortunately, piezo stages offer low mechanical wear. However, they can age slightly over time, and certain factors can play into temperature changes, humidity, and electrical noise.
Market Adoption in the US
According to a recent report, the piezo stage market is expected to grow over $1,500 million by 2035. The overall grow rate is expected to be 5.9% for the next 10 years.
Ongoing technological advances in piezoelectric materials and miniaturization techniques may hopefully improve affordability, which is one of the major challenges in implementing piezo technology.
Overall, the demand for piezo stages is rapidly growing in both North America and Asia-Pacific regions, specifically in manufacturing and scientific laboratories.
Adopting Piezo Stage Technology
Piezo stages enable motion control at the same scale as the object or event being measured or processed, making them indispensable in advanced microscopy, precision manufacturing, and high-end optical systems.

MISUMI offers Motion Solution’s nPFOCUS Piezo Stage with 100 µm, 250 µm, and 400 µm range, fitted with a strain gauge. Paired with the LC.400 series controller and objective lens thread adapters. A capacitive sensor for closed-loop feedback is available upon request.