Browse Topic

UPDATE MAKEiT, Inc: Project Bigfoot

September 6, 2017 · Carlicia Layosa

This week we catch up with our friends at MAKEiT, Inc on their project Bigfoot as well as…

Surface Finishes: Hard Chrome Plating

August 29, 2017 · Carlicia Layosa

The most common and long-established method of decorative plating on steel is copper-nickel-chrome plating also known as ‘chrome…

Surface Finishes: Heat Treatments

August 22, 2017 · Carlicia Layosa

Heat treatment is a type of surface treatment that includes hardening and thermal diffusion. Both use heating to…

Surfaces Finishes: Electroless Plating

August 15, 2017 · Carlicia Layosa

Electroless plating is a chemical plating technique used to deposit a layer of metal plating without using an…

Surface Finishes: Anodizing

August 8, 2017 · Carlicia Layosa

“Anodizing is an electrochemical process that converts the metal surface into a decorative, durable, corrosion-resistant, anodic oxide finish.”…

The Technique of Losing Weight: Part Two

August 1, 2017 · Carlicia Layosa

Strength and Shape Design Considerations After looking at ways to use different plastics instead of metal in last…

The Technique of Losing Weight: Part One

July 25, 2017 · Carlicia Layosa

In response to concerns about global warming and depletion of subterranean resources such as petroleum oil, the automobile…

One for All: Universal Design

July 18, 2017 · Carlicia Layosa

“Universal design is the design of products and environments to be usable by all people, to the greatest…

Belt Driven Actuators: Loads and Speeds

July 11, 2017 · Carlicia Layosa

Actuators are systems used to control or drive a load. There are pneumatic, hydraulic and electric actuators, all…

You Can with Cantilever Shafts!

June 27, 2017 · Carlicia Layosa

Back during your engineering school days, most of us took a strength of materials course and learned about…

1 … 17 18 19 … 31